powered by CADENAS

Manual

Manual

4.8.8.  Tabbed page Assembly

The Assembly tabbed page shows up only for project type Assembly configuration and Assembly template.

Basically, a distinction must be made between Assembly configuration and Assembly template . Configuration relates to an assembly project which is set up step by step in PARTdataManager and which can also be influenced individually in its composition. By contrast, a template is set up fully and automatically when open, like a template.

The distinction between these two assembly types is also clearly shown by the various symbols in the directory tree.

When you Create and Save an assembly in the Configurator, *.prj and *.asy or *.sbl files are created automatically in PARTproject's directory tree.

Assembly-Type

Symbol

Configuration

Template

Assembly file:

The field is automatically assigned the corresponding file name after being created.

Data directories:

The data directory is determined within 23d-libs and is entered in the field of the same name.

Dimensioning views:

Files indicating assembly dimensioning must be specified in the Dimensioning views field.