powered by CADENAS

Social Share

Amazon

Guitar pedalboard (2296 views - Music)

A guitar pedalboard is a flat board or panel which serves as a container, patch bay and power supply for effects pedals for the electric guitar. Some pedalboards contain their own transformer and power cables, in order to power a number of different pedals. Pedalboards assist the player in managing multiple pedals. The entire pedalboard can be packed up and transported to the next location without the need for disassembly. Pedalboards often have a cover which protects the effects pedals during transportation. There are many varieties of pedalboard cases, including homemade DIY pedalboard cases, store-bought pedalboard cases, and custom-made pedalboard cases. Hard shell pedalboard-cases have foam padding, reinforced corners, and locking latches which protect the pedals during transport; during onstage performance, with the lid removed, the bottom of the case is a pedalboard. Most pedalboards have a flat surface where pedals and their power supplies are attached using Velcro or other techniques, and they often have a removable lid or padding to protect the pedals when they are not being used. Some pedalboards have handles or wheels to facilitate transportation.
Go to Article

Explanation by Hotspot Model

Youtube


    

Guitar pedalboard

Guitar pedalboard

Guitar pedalboard

A guitar pedalboard is a flat board or panel which serves as a container, patch bay and power supply for effects pedals for the electric guitar. Some pedalboards contain their own transformer and power cables, in order to power a number of different pedals. Pedalboards assist the player in managing multiple pedals. The entire pedalboard can be packed up and transported to the next location without the need for disassembly.

Pedalboards often have a cover which protects the effects pedals during transportation. There are many varieties of pedalboard cases, including homemade DIY pedalboard cases, store-bought pedalboard cases, and custom-made pedalboard cases. Hard shell pedalboard-cases have foam padding, reinforced corners, and locking latches which protect the pedals during transport; during onstage performance, with the lid removed, the bottom of the case is a pedalboard. Most pedalboards have a flat surface where pedals and their power supplies are attached using Velcro or other techniques, and they often have a removable lid or padding to protect the pedals when they are not being used. Some pedalboards have handles or wheels to facilitate transportation.

Pedal power supply

Most effects pedals are powered by varying levels of DC voltage, depending on the manufacturer. Possible voltages include 9V, 12V, 15V, 18V, 24V, and 40V, though 9V is most common. Some effects pedals accept a range of voltages, producing different effects. Guitar players can experiment with varying voltages to generate different sounds.

DC power can be generated by batteries, an AC/DC power supply, or a rechargeable battery. Each has its own advantages and disadvantages. Using individual batteries is fine for occasional players, because they don't have to worry about the cost of replacement batteries or changes in sound as batteries get tired. Battery life varies depending on the pedal's power draw. Professional players normally replace all batteries with new ones before a show.

Using a DC power supply is a good alternative, even though the initial cost is higher. However, one has to pay attention to ground loops and power line hum. Noise gates can help to reduce the noise by suppressing the signal below a certain volume threshold, but this only controls unwanted noise without actually removing it from the signal.

The third approach is to use a powerful rechargeable battery to drive all the pedals, and a battery charger to recharge the battery. This eliminates ground loops because the pedals are grounded at a single point: the amplifier. There are batteries on the market that can power over 20 effects pedals for eight hours on a single charge. The effects pedals are connected to the rechargeable battery via isolated DC-DC converters, which produce the required voltages.

Using a rechargeable effects pedal battery or AC/DC power supply in conjunction with a “pedalboard suitcase” reduces setup time prior to a show.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Music

3d,printed,3dprinting,3dprint,music,song,dvd,dcrom,schellak,top hit