Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution 3.0 (Hannes Grobe (talk)).
安培 | |
---|---|
单位信息 | |
单位制 | 国际单位制 |
物理量名称 | 电流 |
符号 | A |
得名 | 安德烈-马里·安培 |
正式定義 | |
定義 | 當基本電荷 e,以單位 C,即 A·s,表示時,將其固定數值取為1.602176634×10−19來定義安培,其中秒用ΔνCs定義。 |
安培,简称安,是国际单位制中电流强度的单位,符号是A[1][2][3]。同时它也是国际单位制中七个基本单位之一[注 1]。安培是以法国数学家和物理学家安德烈-马里·安培命名的,为了纪念他在经典电磁学方面的贡献。
实际情况中,安培是对单位时间内通过导体横截面的电荷量的度量。1秒内通过横截面的电量为1库仑(6.241×1018个电子的电量)时,电流大小為1安培。[4]
2018年11月16日,第26届国际计量大会决定定义安培为:
“ | 安培,符号 A,SI 的电流单位。当基本电荷 e,以单位 C,即 A·s,表示时,将其固定数值取为1.602176634×10−19来定义安培,其中秒用ΔνCs定义。[5] | ” |
其中ΔνCs是指铯133原子基态的两个超精细能级之间的跃迁辐射频率。新定义使用基本电荷 e 重新定义安培,这样的条件可以在实验室中重现,同时较简单易明,于2019年5月20日生效。
安培最初是被定义为厘米-克-秒制中电流单位绝对安培的十分之一[6]。如此确定它的大小是为了保证从国际单位制中的其他单位推导安培得到的值比较合适。
“国际安培”是一个较早的电流单位,定义为使硝酸银溶液中每秒析出0.001118000克银的电流[7]。之后,更精确地测量发现,这一电流是0.99985 A。
1948年第九届国际计量大会决定定义安培为:
“ | 真空中,截面积可忽略的两根相距1米的无限长平行圆直导线内,通以等量恒定电流时,若导线间相互作用在每米长度上的力为2×10–7牛顿,则每根导线中的电流为一安培。 | ” |
—— [2][8] |
2005年,国际计量委员会同意研究将元电荷电荷量用于安培定义的可能。新的定义在2014年的第25屆国际度量衡委员会上被討論,于2019年5月20日生效。[9][10]
2018年第二十六届国际计量大会通过给予元电荷确定的电荷量,确定了安培的新定义。自2019年5月20日起,元电荷的电荷量被确定为 ,而
。由此,1 安培所代表的电流强度大小由元电荷电荷量和秒确定。[11]
安培这一单位与瓦特平衡(英语:Watt balance)和欧姆定律中的单位伏特、欧姆相联系。而在约瑟夫森效应和量子霍尔效应中也都各自有所应用。[12]
现在,建立一安培的技术已经能够达到107的逼近误差。[12]
|
|
This article uses material from the Wikipedia article "安培", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced