powered by CADENAS

Social Share

Amazon

Aircraft design process (8366 views - Transportation - Air Water Earth)

The aircraft design process is the engineering design process by which aircraft are designed. These depend on many factors such as customer and manufacturer demand, safety protocols, physical and economic constraints etc. For some types of aircraft the design process is regulated by national airworthiness authorities. This article deals with powered aircraft such as airplanes and helicopter designs. Aircraft design is a compromise between many competing factors and constraints and accounts for existing designs and market requirements to produce the best aircraft.
Go to Article

Explanation by Hotspot Model

Youtube


    

Aircraft design process

Aircraft design process

Aircraft design process

The aircraft design process is the engineering design process by which aircraft are designed. These depend on many factors such as customer and manufacturer demand, safety protocols, physical and economic constraints etc. For some types of aircraft the design process is regulated by national airworthiness authorities. This article deals with powered aircraft such as airplanes and helicopter designs.

Aircraft design is a compromise between many competing factors and constraints and accounts for existing designs and market requirements to produce the best aircraft.

Design constraints

Purpose

The design process starts with the aircraft's intended purpose. Commercial airliners are designed for carrying a passenger or cargo payload, long range and greater fuel efficiency where as fighter jets are designed to perform high speed maneuvers and provide close support to ground troops. Some aircraft have specific missions, for instance, amphibious airplanes have a unique design that allows them to operate from both land and water, some fighters, like the Harrier Jump Jet, have VTOL (Vertical Take-off and Landing) ability, helicopters have the ability to hover over an area for a period of time.[1]

The purpose may be to fit a specific requirement, e.g. as in the historical case of a British Air Ministry specification, or fill a perceived "gap in the market"; that is, a class or design of aircraft which does not yet exist, but for which there would be significant demand.

Aircraft regulations

Another important factor that influences the design of the aircraft are the regulations put forth by national airworthiness authorities.[2][3]

Airports may also impose limits on aircraft, for instance, the maximum wingspan allowed for a conventional aircraft is 80 m to prevent collisions between aircraft while taxiing.[4]

Financial factors and market

Budget limitations, market requirements and competition set constraints on the design process and comprise the non-technical influences on aircraft design along with environmental factors. Competition leads to companies striving for better efficiency in the design without compromising performance and incorporating new techniques and technology.[5]

In the 1950s and ’60s, unattainable project goals were regularly set, but then abandoned, whereas today troubled programs like the Boeing 787 and the Lockheed Martin F-35 have proven far more costly and complex to develop than expected. More advanced and integrated design tools have been developed. Model-based systems engineering predicts potentially problematic interactions, while computational analysis and optimization allows designers to explore more options early in the process. Increasing automation in engineering and manufacturing allows faster and cheaper development. Technology advances from materials to manufacturing enable more complex design variations like multifunction parts. Once impossible to design or construct, these can now be 3D printed, but they have yet to prove their utility in applications like the Northrop Grumman B-21 or the re-engined A320neo and 737 MAX. Airbus and Boeing also recognize the economic limits, that the next airliner generation cannot cost more than the previous ones did.[6]

Environmental factors

An increase in the number of aircraft also means greater carbon emissions. Environmental scientists have voiced concern over the main kinds of pollution associated with aircraft, mainly noise and emissions. Aircraft engines have been historically notorious for creating noise pollution and the expansion of airways over already congested and polluted cities have drawn heavy criticism, making it necessary to have environmental policies for aircraft noise.[7][8] Noise also arises from the airframe, where the airflow directions are changed.[9] Improved noise regulations have forced designers to create quieter engines and airframes.[10] Emissions from aircraft include particulates, carbon dioxide (CO2), Sulfur dioxide(SO2), Carbon monoxide (CO), various oxides of nitrates and unburnt hydrocarbons.[11] To combat the pollution, ICAO set recommendations in 1981 to control aircraft emissions.[12] Newer, environmentally friendly fuels have been developed[13] and the use of recyclable materials in manufacturing[14] have helped reduce the ecological impact due to aircraft. Environmental limitations also affect airfield compatibility. Airports around the world have been built to suit the topography of the particular region. Space limitations, pavement design, runway end safety areas and the unique location of airport are some of the airport factors that influence aircraft design. However changes in aircraft design also influence airfield design as well, for instance, the recent introduction of new large aircraft (NLAs) such as the superjumbo Airbus A380, have led to airports worldwide redesigning their facilities to accommodate its large size and service requirements.[15][16]

Safety

The high speeds, fuel tanks, atmospheric conditions at cruise altitudes, natural hazards (thunderstorms, hail and bird strikes) and human error are some of the many hazards that pose a threat to air travel.[17][18][19]

Airworthiness is the standard by which aircraft are determined fit to fly.[20] The responsibility for airworthiness lies with national aviation regulatory bodies, manufacturers, as well as owners and operators.[citation needed]

The International Civil Aviation Organization sets international standards and recommended practices for national authorities to base their regulations on [21][22] The national regulatory authorities set standards for airworthiness, issue certificates to manufacturers and operators and the standards of personnel training.[23] Every country has its own regulatory body such as the Federal Aviation Authority in USA, DGCA (Directorate General of Civil Aviation) in India, etc.

The aircraft manufacturer makes sure that the aircraft meets existing design standards, defines the operating limitations and maintenance schedules and provides support and maintenance throughout the operational life of the aircraft. The aviation operators include the passenger and cargo airliners, air forces and owners of private aircraft. They agree to comply with the regulations set by the regulatory bodies, understand the limitations of the aircraft as specified by the manufacturer, report defects and assist the manufacturers in keeping up the airworthiness standards.[citation needed]

Most of the design criticisms these days are built on crashworthiness. Even with the greatest attention to airworthiness, accidents still occur. Crashworthiness is the qualitative evaluation of how aircraft survive an accident. The main objective is to protect the passengers or valuable cargo from the damage caused by an accident. In the case of airliners the stressed skin of the pressurized fuselage provides this feature, but in the event of a nose or tail impact, large bending moments build all the way through the fuselage, causing fractures in the shell, causing the fuselage to break up into smaller sections.[24] So the passenger aircraft are designed in such a way that seating arrangements are away from areas likely to be intruded in an accident, such as near a propeller, engine nacelle undercarriage etc.[25] The interior of the cabin is also fitted with safety features such as oxygen masks that drop down in the event of loss of cabin pressure, lockable luggage compartments, safety belts, lifejackets, emergency doors and luminous floor strips. Aircraft are sometimes designed with emergency water landing in mind, for instance the Airbus A330 has a 'ditching' switch that closes valves and openings beneath the aircraft slowing the ingress of water.[26]

Design optimization

Aircraft designers normally rough-out the initial design with consideration of all the constraints on their design. Historically design teams used to be small, usually headed by a Chief Designer who knows all the design requirements and objectives and coordinated the team accordingly. As time progressed, the complexity of military and airline aircraft also grew. Modern military and airline design projects are of such a large scale that every design aspect is tackled by different teams and then brought together. In general aviation a large number of light aircraft are designed and built by amateur hobbyists and enthusiasts.[27]

Computer-aided design of aircraft

In the early years of aircraft design, designers generally used analytical theory to do the various engineering calculations that go into the design process along with a lot of experimentation. These calculations were labour-intensive and time-consuming. In the 1940s, several engineers started looking for ways to automate and simplify the calculation process and many relations and semi-empirical formulas were developed. Even after simplification, the calculations continued to be extensive. With the invention of the computer, engineers realized that a majority of the calculations could be automated, but the lack of design visualization and the huge amount of experimentation involved kept the field of aircraft design stagnant. With the rise of programming languages, engineers could now write programs that were tailored to design an aircraft. Originally this was done with mainframe computers and used low-level programming languages that required the user to be fluent in the language and know the architecture of the computer. With the introduction of personal computers, design programs began employing a more user-friendly approach.[28][not in citation given]

Design aspects

The main aspects of aircraft design are:

  1. Aerodynamics
  2. Propulsion
  3. Controls
  4. Mass
  5. Structure

All aircraft designs involve compromises of these factors to achieve the design mission.[29]

Wing design

The wing of a fixed-wing aircraft provides the lift necessary for flight. Wing geometry affects every aspect of an aircraft’s flight. The wing area will usually be dictated by the desired stalling speed but the overall shape of the planform and other detail aspects may be influenced by wing layout factors.[30] The wing can be mounted to the fuselage in high, low and middle positions. The wing design depends on many parameters such as selection of aspect ratio, taper ratio, sweepback angle, thickness ratio, section profile, washout and dihedral.[31] The cross-sectional shape of the wing is its airfoil.[32] The construction of the wing starts with the rib which defines the airfoil shape. Ribs can be made of wood, metal, plastic or even composites.[33]

The wing must be designed and tested to ensure it can withstand the maximum loads imposed by maneuvering, and by atmospheric gusts.

Fuselage

The fuselage is the part of the aircraft that contains the cockpit, passenger cabin or cargo hold.[34]

Propulsion

Aircraft propulsion may be achieved by specially designed aircraft engines, adapted auto, motorcycle or snowmobile engines, electric engines or even human muscle power. The main parameters of engine design are:[citation needed]

  • Maximum engine thrust available
  • Fuel consumption
  • Engine mass
  • Engine geometry

The thrust provided by the engine must balance the drag at cruise speed and be greater than the drag to allow acceleration. The engine requirement varies with the type of aircraft. For instance, commercial airliners spend more time in cruise speed and need more engine efficiency. High-performance fighter jets need very high acceleration and therefore have very high thrust requirements.[35]

Weight

The weight of the aircraft is the common factor that links all aspects of aircraft design such as aerodynamics, structure, and propulsion, all together. An aircraft's weight is derived from various factors such as empty weight, payload, useful load, etc. The various weights are used to then calculate the center of mass of the entire aircraft.[36] The center of mass must fit within the established limits set by the manufacturer.

Structure

The aircraft structure focuses not only on strength, stiffness, durability (fatigue), fracture toughness, stability, but also on fail-safety, corrosion resistance, maintainability and ease of manufacturing. The structure must be able to withstand the stresses caused by cabin pressurization, if fitted, turbulence and engine or rotor vibrations.[37]

Design process and simulation

The design of any aircraft starts out in three phases[38]

Conceptual Design

Aircraft conceptual design involves sketching a variety of possible configurations that meet the required design specifications. By drawing a set of configurations, designers seek to reach the design configuration that satisfactorily meets all requirements as well as go hand in hand with factors such as aerodynamics, propulsion, flight performance, structural and control systems.[39] This is called design optimization. Fundamental aspects such as fuselage shape, wing configuration and location, engine size and type are all determined at this stage. Constraints to design like those mentioned above are all taken into account at this stage as well. The final product is a conceptual layout of the aircraft configuration on paper or computer screen, to be reviewed by engineers and other designers.

Preliminary design phase

The design configuration arrived at in the conceptual design phase is then tweaked and remodeled to fit into the design parameters. In this phase, wind tunnel testing and computational fluid dynamic calculations of the flow field around the aircraft are done. Major structural and control analysis is also carried out in this phase. Aerodynamic flaws and structural instabilities if any are corrected and the final design is drawn and finalized. Then after the finalization of the design lies the key decision with the manufacturer or individual designing it whether to actually go ahead with the production of the aircraft.[40] At this point several designs, though perfectly capable of flight and performance, might have been opted out of production due to their being economically nonviable.

Detail design phase

This phase simply deals with the fabrication aspect of the aircraft to be manufactured. It determines the number, design and location of ribs, spars, sections and other structural elements.[41] All aerodynamic, structural, propulsion, control and performance aspects have already been covered in the preliminary design phase and only the manufacturing remains. Flight simulators for aircraft are also developed at this stage.

Delays

Some commercial aircraft have experienced significant schedule delays and cost overruns in the development phase. Examples of this include the Boeing 787 Dreamliner with a delay of 4 years with massive cost overruns, the Boeing 747-8 with a two year delay, the Airbus A380 with a two year delay and US$6.1 billion in cost overruns, the Airbus A350 with delays and cost overruns, the Bombardier C Series, Global 7000 and 8000, the Comac C919 with a four year delay and the Mitsubishi Regional Jet, which was delayed by four years and ended up with empty weight issues.[42]

Program development

An existing aircraft program can be developed for performance and economy gains by stretching the fuselage, increasing the MTOW, enhancing the aerodynamics, installing new engines, new wings or new avionics. For a 9,100 nmi long range at Mach 0.8/FL360, a 10% lower TSFC saves 13% of fuel, a 10% L/D increase saves 12%, a 10% lower OEW saves 6% and all combined saves 28%.[43]

Re-engine

Jet airliners
Base Previous engines First flight Re-engined New engines First flight
DC-8 Super 60 JT3D May 30, 1958 DC-8 Super 70 CFM56 1982
Boeing 737 Original JT8D Apr 9, 1967 Boeing 737 Classic CFM56 Feb 24, 1984
Fokker F28 Rolls-Royce Spey May 9, 1967 Fokker 100/70 Rolls-Royce Tay Nov 30, 1986
Boeing 747 JT9D/CF6-50/RB211-524 Feb 9, 1969 Boeing 747-400 PW4000/CF6-80/RB211-524G/H Apr 29, 1988
Douglas DC-10 JT9D/CF6-50 Aug 29, 1970 MD-11 PW4000/CF6-80 Jan 10, 1990
Douglas DC-9/MD-80 JT8D Feb 25, 1965 MD-90 V2500 Feb 22, 1993
Boeing 737 Classic CFM56-3 Feb 24, 1984 Boeing 737 NG CFM56-7 Feb 9, 1997
Boeing 747-400 PW4000/CF6/RB211 Apr 29, 1988 Boeing 747-8 GEnx Feb 8, 2010
Airbus A320 CFM56/V2500 Feb 22, 1987 Airbus A320neo CFM LEAP/PW1100G Sep 25, 2014
Boeing 737 NG CFM56 Feb 9, 1997 Boeing 737 MAX CFM LEAP Jan 29, 2016
Embraer E-Jet CF34 Feb 19, 2002 Embraer E-Jet E2 PW1000G May 23, 2016
Airbus A330 CF6/PW4000/Trent 700 Nov 2, 1992 Airbus A330neo Trent 7000 Oct 19, 2017
Boeing 777 GE90/PW4000/Trent 800 Jun 12, 1994 Boeing 777X GE9X plan. Q1 2019

Fuselage stretch

Jet airliners
Base Base length First flight Stretched Stretched length First flight
Boeing 737-100 28.65 m (94.00 ft) Apr 9, 1967 737-200 30.53 m (100 ft 2 in)
737-500/600 31.00-31.24 m (101 ft 9 in - 102 ft 6 in)
737-300/700 33.4-33.63 m (109 ft 7 in - 110 ft 4 in)
737 MAX 7 35.56 m 116 / ft 8 in
737-400 36.40 m / 119 ft 7 in
737-800/MAX 8 39.47 m / 129 ft 6 in
737-900/MAX 9 42.11 m / 138 ft 2 in
737 MAX 10 43.80 m / 143 ft 8 in
Boeing 747-100/200/300/400 70.66 m / 231 ft 10 in Feb 9, 1969 Boeing 747SP 56.3 m / 184 ft 9 in Jul 4, 1975
Boeing 747-8 76.25 m / 250 ft 2 in Feb 8, 2010
Boeing 757 47.3 m / 155 ft 3 in Feb 19, 1982 Boeing 757-300 54.4 m / 178 ft 7 in
Boeing 767-200/ER 48.51m / 159 ft 2in Sep 26, 1981 Boeing 767-300/ER 54.94m / 180 ft 3in
Boeing 767-400ER 61.37m / 201 ft 4in
Boeing 777-200/ER/LR 63.73 m / 209 ft 1 in Jun 12, 1994 Boeing 777X-8 69.8 m / 229 ft
Boeing 777-300/ER 73.86 m / 242 ft 4 in Oct 16, 1997
Boeing 777X-9 76.7 m / 251 ft 9 in plan. Q1 2019
Boeing 787-8 56.72 m (186 ft 1 in) Dec 15, 2009 Boeing 787-9 62.81 m (206 ft 1 in) Sep 17, 2013
Boeing 787-10 68.28 m (224 ft) Mar 31, 2017
Airbus A300 53.61-54.08 m (175.9-177.4 ft) Oct 28, 1972 Airbus A310 46.66 ft (14.22 m) Apr 3, 1982
Airbus A320 (neo) 37.57 m (123 ft 3 in) Feb 22, 1987 Airbus A318 31.44 m (103 ft 2 in) Jan 15, 2002
Airbus A319 (neo) 33.84 m (111 ft 0 in) Aug 25, 1995
Airbus A321 (neo) 44.51 m (146 ft 0 in) Mar 11, 1993
Airbus A330-300/900 63.67 m (208.89 ft) Nov 2, 1992 Airbus A330-200/800 58.82 m (192.98 ft) Aug 13, 1997
Airbus A340-300 63.69 m (208 ft 11 in) Oct 25, 1991 Airbus A340-200 59.40 m (194 ft 11 in) Apr 1, 1992
Airbus A340-500 67.93 m (222 ft 10 in) Feb 11, 2002
Airbus A340-600 75.36 m (247 ft 3 in) Apr 23, 2001
Airbus A350-900 66.61 m / 218.54 ft Jun 14, 2013 A350-1000 73.59 m / 241.44 ft Nov 24, 2016

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht