powered by CADENAS

Social Share

Amazon

Automatic lubrication (5324 views - Mechanical Engineering)

Automatic lubrication (also called autolube or auto-lube) refers to a lubrication system on a two-stroke engine, in which the oil is automatically mixed with fuel and manual oil-fuel pre-mixing is not necessary. The oil is contained in a reservoir that connects to a small oil pump in the engine, which needs to be periodically refilled. This system is commonly used for motorcycles as it eliminates the need of pre-mixing fuel and two-stroke oil. Vespa Sprint is an example where pre-mixing of two-stroke oil is required. Automatic lubrication was introduced for motorcycles by Velocette in 1913.An example of application of automatic lubrication system is Suzuki AX100 motorcycle. The motorcycle has a separate oil reservoir on its right side which supplies the cylinder with two-stroke oil proportional to engine speed.
Go to Article

Explanation by Hotspot Model

Youtube


    

Automatic lubrication

Automatic lubrication


Automatic lubrication (also called autolube or auto-lube) refers to a lubrication system on a two-stroke engine, in which the oil is automatically mixed with fuel and manual oil-fuel pre-mixing is not necessary. The oil is contained in a reservoir that connects to a small oil pump in the engine, which needs to be periodically refilled.


This system is commonly used for motorcycles as it eliminates the need of pre-mixing fuel and two-stroke oil. Vespa Sprint is an example where pre-mixing of two-stroke oil is required. Automatic lubrication was introduced for motorcycles by Velocette in 1913.[1]

An example of application of automatic lubrication system is Suzuki AX100 motorcycle. The motorcycle has a separate oil reservoir on its right side which supplies the cylinder with two-stroke oil proportional to engine speed.

Advantages

  1. Consistent lubrication and oil consumption is reduced greatly
  2. More effective lubrication results because the oil enters the engine in larger size droplets
  3. There is much less unwanted carbon deposited on the spark plugs, cylinder heads, pistons and exhaust system.
  4. There is much less exhaust smoke
  5. Refueling is simplified

Disdvantages

  1. The system is more complicated compared to manual pre-mixing, although it is easier for the end user.
  2. For any reason, if the two-stroke oil pump fails to operate properly, chance of damaging the engine is very high.
  3. The two-stroke oil tank in scooters and motorcycles is usually hidden from direct view of the rider and needs filling up occasionally. Without any indicator to indicate oil level, it is possible for a novice rider to forget to fill up the oil tank. This can end up starving the engine of oil and cause damage.
  1. ^ Mike Waller (September 1986), "Deja vu: British author Mike Waller reminds us that high tech isn't always new tech", American Motorcyclist, American Motorcyclist Association: 15


This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD