powered by CADENAS

Social Share

Amazon

Product design (7150 views - Industrial Markets)

Product design as a verb is to create a new product to be sold by a business to its customers. A very broad coefficient and effective generation and development of ideas through a process that leads to new products. Thus, it is a major aspect of new product development. Due to the absence of a consensually accepted definition that reflects the breadth of the topic sufficiently, two discrete, yet interdependent, definitions are needed: one that explicitly defines product design in reference to the artifact, the other that defines the product design process in relation to this artifact. Product design as a noun: the set of properties of an artifact, consisting of the discrete properties of the form (i.e., the aesthetics of the tangible good and/or service) and the function (i.e. its capabilities) together with the holistic properties of the integrated form and function.Product design process: the set of strategic and tactical activities, from idea generation to commercialization, used to create a product design. In a systematic approach, product designers conceptualize and evaluate ideas, turning them into tangible inventions and products. The product designer's role is to combine art, science, and technology to create new products that people can use. Their evolving role has been facilitated by digital tools that now allow designers to do things that include communicate, visualize, analyze, 3D modeling and actually produce tangible ideas in a way that would have taken greater manpower in the past. Product design is sometimes confused with (and certainly overlaps with) industrial design, and has recently become a broad term inclusive of service, software, and physical product design. Industrial design is concerned with bringing artistic form and usability, usually associated with craft design and ergonomics, together in order to mass-produce goods. Other aspects of product design and industrial design include engineering design, particularly when matters of functionality or utility (e.g. problem-solving) are at issue, though such boundaries are not always clear.
Go to Article

Explanation by Hotspot Model

Youtube


    

Product design

Product design

Product design as a verb is to create a new product to be sold by a business to its customers.[1] A very broad coefficient and effective generation and development of ideas through a process that leads to new products.[2] Thus, it is a major aspect of new product development.

Due to the absence of a consensually accepted definition that reflects the breadth of the topic sufficiently, two discrete, yet interdependent, definitions are needed: one that explicitly defines product design in reference to the artifact, the other that defines the product design process in relation to this artifact.

Product design as a noun: the set of properties of an artifact, consisting of the discrete properties of the form (i.e., the aesthetics of the tangible good and/or service) and the function (i.e. its capabilities) together with the holistic properties of the integrated form and function.[3]

Product design process: the set of strategic and tactical activities, from idea generation to commercialization, used to create a product design. In a systematic approach, product designers conceptualize and evaluate ideas, turning them into tangible inventions and products. The product designer's role is to combine art, science, and technology to create new products that people can use. Their evolving role has been facilitated by digital tools that now allow designers to do things that include communicate, visualize, analyze, 3D modeling and actually produce tangible ideas in a way that would have taken greater manpower in the past.

Product design is sometimes confused with (and certainly overlaps with) industrial design, and has recently become a broad term inclusive of service, software, and physical product design. Industrial design is concerned with bringing artistic form and usability, usually associated with craft design and ergonomics, together in order to mass-produce goods.[4] Other aspects of product design and industrial design include engineering design, particularly when matters of functionality or utility (e.g. problem-solving) are at issue, though such boundaries are not always clear.[5]

Product design process

There are various product design processes, and many focus on different aspects. One example formulation/model of the process is described by Don Koberg and Jim Bagnellin, in "The Seven Universal Stages of Creative Problem-Solving." The process is usually completed by a group of people with different skills and training - e.g. industrial designers, field experts (prospective users), engineers (for engineering design aspects), depending upon the nature and type of product involved. The process often involves figuring out what is required, brainstorming possible ideas, creating mock prototypes, and then generating the product. However, that is not the end. Product designers would still need to execute the idea, making it into an actual product and evaluating its success (seeing if any improvements are necessary).

The product design process has experienced huge leaps in evolution over the last few years with the rise and adoption of 3D printing. New consumer-friendly 3D printers can produce dimensional objects and print upwards with a plastic like substance opposed to traditional printers that spread ink across a page.

The product design process, as expressed by Koberg and Bagnell, typically involves three main aspects:[6]

  • Analysis
  • Concept
  • Synthesis

Depending on the kind of product being designed, the latter two sections are most often revisited (e.g. depending on how often the design needs revision, to improve it or to better fit the criteria). This is a continuous loop, where feedback is the main component.[6] Koberg and Bagnell offer more specifics on the process: In their model, "analysis" consists of two stages, "concept" is only one stage, and "synthesis" encompasses the other four. (These terms notably vary in usage in different design frameworks. Here, they are used in the way they're used by Koberg and Bagnell.)

Analysis

  • Accept Situation: Here, the designers decide on committing to the project and finding a solution to the problem. They pool their resources into figuring out how to solve the task most efficiently.[6]
  • Analyze: In this stage, everyone in the team begins research. They gather general and specific materials which will help to figure out how their problem might be solved. This can range from statistics, questionnaires, and articles, among many other sources.[6]

Concept

  • Define: This is where the key issue of the matter is defined. The conditions of the problem become objectives, and restraints on the situation become the parameters within which the new design must be constructed.[6]

Synthesis

  • Ideate: The designers here brainstorm different ideas, solutions for their design problem. The ideal brainstorming session does not involve any bias or judgment, but instead builds on original ideas.[6]
  • Select: By now, the designers have narrowed down their ideas to a select few, which can be guaranteed successes and from there they can outline their plan to make the product.[6]
  • Implement: This is where the prototypes are built, the plan outlined in the previous step is realized and the product starts to become an actual object.[6]
  • Evaluate: In the last stage, the product is tested, and from there, improvements are made. Although this is the last stage, it does not mean that the process is over. The finished prototype may not work as well as hoped so new ideas need to be brainstormed.[6]

Demand-pull innovation and invention-push innovation

Most product designs fall under one of two categories: demand-pull innovation or invention-push innovation.[7]

Demand-pull happens when there is an opportunity in the market to be explored by the design of a product.[7] This product design attempts to solve a design problem. The design solution may be the development of a new product or developing a product that's already on the market, such as developing an existing invention for another purpose.[7]

Invention-push innovation happens when there is an advancement in intelligence. This can occur through research or it can occur when the product designer comes up with a new product design idea.[7]

Product design expression

Design expression comes from the combined effect of all elements in a product. Colour tone, shape and size should direct a person's thoughts towards buying the product.[8] Therefore, it is in the product designer's best interest to consider the audiences who are most likely to be the product's end consumers. Keeping in mind how consumers will perceive the product during the design process will direct towards the product’s success in the market.[9] However, even within a specific audience, it is challenging to cater to each possible personality within that group.

The solution to that is to create a product that, in its designed appearance and function, expresses a personality or tells a story.[8] Products that carry such attributes are more likely to give off a stronger expression that will attract more consumers. On that note it is important to keep in mind that design expression does not only concern the appearance of a product, but also its function.[8] For example, as humans our appearance as well as our actions are subject to people's judgment when they are making a first impression of us. People usually do not appreciate a rude person even if they are good looking. Similarly, a product can have an attractive appearance but if its function does not follow through it will most likely drop in regards to consumer interest. In this sense, designers are like communicators, they use the language of different elements in the product to express something.[10]

Product design considerations

Product design is not an easy task.[11] The stakeholders involved all demand something different from the product designer and from the design process.[11]

  • The manufacturer is concerned with production cost; in the end, the manufacturer wants an economically produced product.[11]
  • The purchaser looks at price, appearance, and prestige value.[11]
  • The end user is concerned with usability and functionality of the final product.[11]
  • The maintenance and repair department focuses on how well the final product can be maintained: is the product easily reassembled, disassembled, diagnosed, and serviced?[11]

Stakeholders' needs vary from one another and it is the product designer's job to incorporate those needs into their design.

Trends in product design

Product designers need to consider all of the details: the ways people use and abuse objects, faulty products, errors made in the design process, and the desirable ways in which people wish they could use objects.[12] Many new designs will fail and many won't even make it to market.[12] Some designs eventually become obsolete. The design process itself can be quite frustrating usually taking 5 or 6 tries to get the product design right.[12] A product that fails in the marketplace the first time may be re-introduced to the market 2 more times.[12] If it continues to fail, the product is then considered to be dead because the market believes it to be a failure.[12] Most new products fail, even if it's a great idea.[12]

All types of product design are clearly linked to the economic health of manufacturing sectors. Innovation provides much of the competitive impetus for the development of new products, with new technology often requiring a new design interpretation. It only takes one manufacturer to create a new product paradigm to force the rest of the industry to catch up - fueling further innovation.[13] Products designed to benefit people of all ages and abilities—without penalty to any group—accommodate our swelling aging population by extending independence and supporting the changing physical and sensory needs we all encounter as we grow older.[14]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Industrial Markets

3D - 3D CAD - 3D Models - 3D Library - Mechanical Engineering - Maschinenbau , Architecture Engineering - Architektur - BIM, Electrical Engineering - Elektrotechnik, Mechatronic - Mechatronik, Plant Design - Anlagenbau, Marine - Offshore Onshore - Food Service - Interior Architecture Innenarchitektur - Furnitures Möbel - Automotive - IoT Internet Of Things Industry 4.0 Industrie 4.0 Digital Twin Manufacturing 2025 - Chemistry - Food Service - Landscape Architecture - Exterior Architecture