powered by CADENAS

Social Share

Amazon

Stationary steam engine (8880 views - Mechanism & Kinematics)

Stationary steam engines are fixed steam engines used for pumping or driving mills and factories, and for power generation. They are distinct from locomotive engines used on railways, traction engines for heavy steam haulage on roads, steam cars (and other motor vehicles), agricultural engines used for ploughing or threshing, marine engines, and the steam turbines used as the mechanism of power generation for most nuclear power plants. They were introduced during the 18th century and widely made for the whole of the 19th century and most of the first half of the 20th century, only declining as electricity supply and the internal combustion engine became more widespread.
Go to Article

Explanation by Hotspot Model

Youtube


    

Stationary steam engine

Stationary steam engine

Stationary steam engine

Stationary steam engines are fixed steam engines used for pumping or driving mills and factories, and for power generation. They are distinct from locomotive engines used on railways, traction engines for heavy steam haulage on roads, steam cars (and other motor vehicles), agricultural engines used for ploughing or threshing, marine engines, and the steam turbines used as the mechanism of power generation for most nuclear power plants.

They were introduced during the 18th century and widely made for the whole of the 19th century and most of the first half of the 20th century, only declining as electricity supply and the internal combustion engine became more widespread.

Types of stationary steam engine

There are different patterns of stationary steam engines, distinguished by the layout of the cylinders and crankshaft:

  • Beam engines have a rocking beam providing the connection between the vertical cylinder and crankshaft.
  • Table engines have the crosshead above the vertical cylinder and the crankshaft below.
  • Horizontal engines have a horizontal cylinder.
  • Vertical engines have a vertical cylinder.
  • Inclined engines have an inclined cylinder.

Stationary engines may be classified by secondary characteristics as well:

When stationary engines had multiple cylinders, they could be classified as:

  • Simple engines, with multiple identical cylinders operating on a common crankshaft.
  • Compound engines which use the exhaust from high-pressure cylinders to power low-pressure cylinders.

An engine could be run in simple or condensing mode:

  • Simple mode meant the exhaust gas left the cylinder and passed straight into the atmosphere
  • In condensing mode, the steam was cooled in a separate cylinder, and changed from vapour to liquid water, creating a vacuum that assisted with the motion. This could be done with a water-cooled plate that acted as a heat sink, or pumping-in a spray of water.

Stationary engines may also be classified by their application:

Stationary engines could be classified by the manufacturer

History

In order of evolution:

[1]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanism & Kinematics

3D,Geneva double,mechanism,kinematics,rotation,translation