powered by CADENAS

Social Share

Amazon

Monocoque (4856 views - Transportation - Air Water Earth)

Monocoque (), also structural skin, is a structural system where loads are supported through an object's external skin, similar to an egg shell. The word monocoque is a French term for "single shell" or (of boats) "single hull". First used in boats, a true monocoque carries both tensile and compressive forces within the skin and can be recognised by the absence of a load-carrying internal frame. Few metal aircraft can strictly be regarded as pure monocoques, as they use a metal shell or sheeting reinforced with frames riveted to the skin, but most of the wooden aircraft are described as monocoques, even though they also incorporate frames. By contrast, a semi-monocoque is a hybrid combining a tensile stressed skin and a compressive structure made up of longerons and ribs or frames. Other semi-monocoques, not to be confused with true monocoques, include vehicle unibodies, which tend to be composites, and inflatable shells or balloon tanks, both of which are pressure stabilised. The term is frequently misused, particularly as a marketing term for structures built up from hollow components.
Go to Article

Explanation by Hotspot Model

Youtube


    

Monocoque

Monocoque

Monocoque (/ˈmɒnəˌkɒk, -ˌkk/), also structural skin, is a structural system where loads are supported through an object's external skin, similar to an egg shell. The word monocoque is a French term for "single shell" or (of boats) "single hull".[1] First used in boats,[2] a true monocoque carries both tensile and compressive forces within the skin and can be recognised by the absence of a load-carrying internal frame.

Few metal aircraft can strictly be regarded as pure monocoques, as they use a metal shell or sheeting reinforced with frames riveted to the skin, but most of the wooden aircraft are described as monocoques, even though they also incorporate frames.

By contrast, a semi-monocoque is a hybrid combining a tensile stressed skin and a compressive structure made up of longerons and ribs or frames.[3] Other semi-monocoques, not to be confused with true monocoques, include vehicle unibodies, which tend to be composites, and inflatable shells or balloon tanks, both of which are pressure stabilised. The term is frequently misused, particularly as a marketing term for structures built up from hollow components.

Aircraft

Early aircraft were constructed using frames, typically of wood or steel tubing, which could then be covered (or skinned) with fabric[4] such as Irish linen or cotton.[5] The fabric made a minor structural contribution in tension but none in compression and was there for aerodynamic reasons only. By considering the structure as a whole and not just the sum of its parts, monocoque construction integrated the skin and frame into a single load-bearing shell with significant improvements to strength and weight.

To make the shell, thin strips of wood were laminated into a three dimensional shape; a technique adopted from boat hull construction. One of the earliest examples was the Deperdussin Monocoque racer in 1912, which used a laminated fuselage made up of three layers of glued poplar veneer, which provided both the external skin and the main load-bearing structure.[6] This also produced a smoother surface and reduced drag so effectively that it was able to win most of the races it was entered into.[6]

This style of construction was further developed in Germany by LFG Roland using the patented Wickelrumpf (wrapped body) form later licensed by them to Pfalz Flugzeugwerke who used it on several fighter aircraft. Each half of the fuselage shell was formed over a male mold using two layers of plywood strips with fabric wrapping between them. The early plywood used was prone to damage from moisture and delamination.[7]

While all-metal aircraft such as the Junkers J 1 had appeared as early as 1915, these were not monocoques but added a metal skin to an underlying framework.

The first metal monocoques were built by Claudius Dornier, while working for Zeppelin-Lindau.[8] He had to overcome a number of problems, not least was the quality of aluminium alloys strong enough to use as structural materials, which frequently formed layers instead of presenting a uniform material.[8] After failed attempts with several large flying boats in which a few components were monocoques, he built the Zeppelin-Lindau V1 to test out a monocoque fuselage. Although it crashed, he learned a lot from its construction. The Dornier-Zeppelin D.I was built in 1918 and although too late for operational service during the war was the first all metal monocoque aircraft to enter production.[8][9]

In parallel to Dornier, Zeppelin also employed Adolf Rohrbach, who built the Zeppelin-Staaken E-4/20, which when it flew in 1920[10] became the first multi-engined monocoque airliner, before being destroyed under orders of the Inter-Allied Commission. At the end of WWI, the Inter-Allied Technical Commission published details of the last Zeppelin-Lindau flying boat showing its monocoque construction. In the UK, Oswald Short built a number of experimental aircraft with metal monocoque fuselages starting with the 1920 Short Silver Streak in an attempt to convince the air ministry of its superiority over wood. Despite advantages, aluminium alloy monocoques would not become common until the mid 1930s as a result of a number of factors, including design conservatism and production setup costs. Short would eventually prove the merits of the construction method with a series of flying boats, whose metal hulls didn't absorb water as the wooden hulls did, greatly improving performance. In the United States, Northrop was a major pioneer, introducing techniques used by his own company and Douglas with the Northrop Alpha.

Road vehicles

In motor racing, the safety of the driver depends on the car body which must meet stringent regulations and only a few cars have been built with monocoque structures.[11][12] An aluminum alloy monocoque chassis was first used in the 1962 Lotus 25 Formula 1 race car and McLaren was the first to use carbon-fiber-reinforced polymers to construct the monocoque of the 1981 McLaren MP4/1. In 1992 the McLaren F1 became the first production car with a carbon-fiber monocoque.[13]

The term monocoque is frequently misapplied to unibody cars. Commercial car bodies are almost never true monocoques but instead use the unibody system (also referred to as unitary construction, unitary body-chassis or body frame integral construction),[14] which uses box sections, bulkheads and tubes to provide most of the strength of the vehicle, while the skin adds relatively little strength or stiffness. [15]

Armoured vehicles

Some armoured fighting vehicles use a monocoque structure with a body shell built up from armour plates, rather than attaching them to a frame. This reduces weight for a given amount of armour. Examples include the German TPz Fuchs and RG-33.

Two-wheeled vehicles

French industrialist and engineer Georges Roy attempted in the 1920s to improve on the bicycle-inspired motorcycle frames of the day, which lacked rigidity. This limited their handling and therefore performance. He applied for a patent in 1926, and at the 1929 Paris Automotive Show unveiled his new motorcycle, the Art-Deco styled 1930 Majestic. Its new type of monocoque body solved the problems he had addressed, and along with better rigidity it did double-duty, as frame and bodywork provided some protection from the elements. Strictly considered, it was more of a semi-monocoque, as it used a box-section, pressed-steel frame with twin side rails riveted together via crossmembers, along with floor pans and rear and front bulkheads.[2]

A monocoque-framed motorcycle was developed by the Spanish motorcycle manufacturer, Ossa, for the 1967 Grand Prix motorcycle racing season.[16]Although the single-cylinder Ossa had 20 horsepower (15 kW) less than its rivals, it was 45 pounds (20 kg) lighter and its monocoque frame was much stiffer than conventional motorcycle frames, giving it superior agility on the racetrack.[16] Ossa won four Grand Prix races with the monocoque bike before their rider was killed during the 1970 Isle of Man TT, causing the Ossa factory to withdraw from Grand Prix competition.[16]

Notable designers such as Eric Offenstadt and Dan Hanebrink created unique monocoque designs for racing in the early 1970s.[17] The 1973 Isle of Man TT was won by Peter Williams on the monocoque-framed Norton John Player Special that he helped design.[18] Honda also experimented with a monocoque Grand Prix racing motorcycle named the NR500 in 1979.[19] The bike had other innovative features, including an engine with oval shaped cylinders, and eventually succumbed to the problems associated with attempting to develop too many new technologies at once. In 1987 John Britten developed the Aero-D One, featuring a composite monocoque chassis that weighed only 12 kg (26 lb).[20]

An aluminium monocoque frame was used for the first time on a mass-produced motorcycle from 2000 on Kawasaki's ZX-12R,[21] their flagship production sportbike aimed at being the fastest production motorcycle.

Single-piece carbon fiber bicycle frames are sometimes described as monocoques; however as most use components to form a frame structure (even if molded in a single piece),[22] these are frames not monocoques, and the pedal-cycle industry continues to refer to them as framesets.

Rockets

Various rockets have used pressure-stabilized monocoque designs, such as Atlas[23] and Falcon 1.[24] The Atlas was very light since a major portion of its structural support was provided by its single-wall steel balloon fuel tanks, which hold their shape while under acceleration by internal pressure. Balloon tanks are not true monocoques but act in the same way as inflatable shells. A balloon tank skin only handles tensile forces while compression is resisted by internal liquid pressure in a way similar to semi-monocoques braced by a solid frame. This becomes obvious when internal pressure is lost and the structure collapses.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht