powered by CADENAS

Social Share

Amazon

容器 (4454 views - Consumer products)

容器是一種基礎工具。泛指任何可以用於容納其它物品的工具,可以部份或完全封閉,被用於容納、儲存、運輸物品。物體可以被放置在容器中,而容器則可以保護內容物。
Go to Article

Explanation by Hotspot Model

容器

容器

容器是一種基礎工具[1][2]。泛指任何可以用於容納其它物品的工具,可以部份或完全封閉,被用於容納、儲存、運輸物品[3]。物體可以被放置在容器中,而容器則可以保護內容物。

歷史

人類使用容器的歷史至少有十萬年,甚至可能有數百萬年的歷史[4]。第一個容器可能是用於儲存食物[4][5] ,這讓食物能保存更長的時間,也能便於攜帶,還能免受其它動物的侵擾。儲存食物的容器對人類社會的發展具有重大的意義,這在靈長類動物之中是一種獨有的行為.[6]。最早的容器可能是自然界中原有的物體,例如在塔魯族[7]夏威夷族[8] 的文化中,有使用空心葫蘆的案例[9]。在這之後,出現了籃、木器和陶器。

隨著人類的技術不斷演進,新的材料、新的生產方式接連誕生,容器的形式也不斷改變[10]。最早的玻璃瓶是在腓尼基生產的,在賽普勒斯羅得島一帶挖掘出腓尼基人所生產的透明玻璃瓶,長度自3英吋至6英吋不等[11]。這些腓尼基人在西元前創作的作品被推測用於裝載香水及其他物品[12],古羅馬人從腓尼基人那兒學到了玻璃的製作方法,並且製造了很多精細的玻璃瓶,大小相對較小。到了18世紀初,玻璃瓶的尺寸已經有公定的標準[13]

1810年,法國人Philippe de Girard法语Philippe de Girard造訪倫敦,他找上英國商人彼得·杜蘭英语Peter Durand作為自己的代理人以推銷自己的嶄新想法——錫罐[14]。而罐頭這個概念是源自法國廚師尼古拉·阿佩爾,阿佩爾之家成為了世界上第一家商業罐頭工廠。

大規模運輸作業一直是一個大難題,主要是因為20世紀時使用的木製貨櫃容易破損,這也讓海關官員在檢查貨物進口時缺乏標準程序[13]。現代的標準貨櫃起源於1950年代,且很快就普及至各地。電腦輔助設計讓容器的設計變得更專業化、產品也更為精準[15]

現代特色

在設計容器時,有幾種必須考慮的要點:

光是具有防震、防潮的功能,可不能算得上一個好的容器。精心設計的容器必須是易於使用的,也就是說、使用者必須要能很輕易地開啟或關閉容器,放入或取出內容物,即使在運輸時也不減損其功能。此外、良好的容器必須要有清晰而便利的標示,形狀要有利於堆放和儲存,在使用壽命將至時,必須要能便於回收。[16]

容器的類型

以下列舉數種常見的容器:

  • - 指口部比腹部窄小、頸長的容器。
  • - 指那些開口較大、一般為近圓筒形的器皿。
  • - 通常是立方體或圓柱體。形狀固定。
  • - 以條狀物編織而成。
  • - 一種圓柱形的容器。
  • - 柔性材料製成的容器,形狀會受內容物而變化。
  • - 通常是指陶製,口小肚大的容器。
  • - 用來盛載食物的容器。
  • - 指一個由盒組成的傢俱。
  • 日语 - 用於裝載刀刃的容器。

参考文献

引用

  1. ^ David P. Braun, "Pots as Tools", in J. A. Moore and A. S. Keene, eds., Archaeological Hammers and Theories (1983), pp. 108-134.
  2. ^ Karen Gayle Harry, Stephanie Michelle Whittlesey, Trixi Bubemyre, Pots, Potters, And Models: Archaeological Investigations at the SRI Locus of the West Branch Site, Tucson, Arizona (2005), p. 283: "The perspective taken in this chapter is that ceramic containers are tools (Braun 1983) and, as a crucial part of the technological repertoire, can provide considerable information about activity organization, production technology, food-preparation and storage technology, settlement function, and economic organization".
  3. ^ Soroka, W. Illustrated Glossary of Packaging Terms. Institute of Packaging Professionals. 2008: 51. ISBN 1-930268-27-0. 
  4. ^ 4.0 4.1 Clive Gamble, Origins and Revolutions: Human Identity in Earliest Prehistory (2007), p. 204.
  5. ^ David A. Munro, A Place For Everything (1968), p. 92.
  6. ^ Bernard Grant Campbell, Human Evolution: An Introduction to Mans Adaptations (2009), p. 306.
  7. ^ Sameera Maiti, The Tharu: Their Arts and Crafts (2004), p. 178.
  8. ^ Irving Jenkins, The Hawaiian Calabash (1989), p. 5.
  9. ^ Chuck Groth, Exploring Package Design (2005), p. 3.
  10. ^ Lewandowski, Krzysztof. Growth in the Size of Unit Loads and Shipping Containers from Antique to WWI.. Packaging Technology and Science. 2016, 29 (8-9): 451–478. ISSN 1099-1522. 
  11. ^ Perrot and Chipiez, Histoire de l'art, v iii, 734-744
  12. ^ George Rawlinson, History of Phoenicia, 1889, Green Longmans publisher, 583 pages
  13. ^ 13.0 13.1 Warren Belasco, Roger Horowitz, Food Chains: From Farmyard to Shopping Cart, p. 98-99.
  14. ^ Geoghegan, Tom. BBC News – The story of how the tin can nearly wasn't. Bbc.co.uk. 2013-04-21 [2013-06-04]. 
  15. ^ Geoff A. Giles, Design and Technology of Packaging Decoration for the Consumer Market (2000), p. 82: "Container designers also found that shrink sleeves gave them new-found freedom to design containers that until then had been viewed as impossible to decorate".
  16. ^ Anthony F. Buono, Henri Savall, Socio-economic Interventions in Organizations (2007), p. 231.

來源

书籍

外部連結



This article uses material from the Wikipedia article "容器", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Consumer products

.max, Maya, Challenge, Competition, Rendering, 3D, Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D, 3D library