Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Industry | Automotive |
---|---|
Founded | Facel SA 1939 |
Defunct | 1964 |
Headquarters | Paris, France |
Key people | Jean Daninos |
Products | Automobiles from 1954 |
Website | www |
Facel S.A. was a French manufacturer of steel furniture and pressed steel components, later complete automobiles to their own design, founded in 1939 to make components for Bronzavia's military aircraft. In 1945 in conjunction with Métallon Facel began to make short-run special bodies, coupés or cabriolets, for Simca, Ford, Panhard and Delahaye.
Unitary bodies without a chassis became general for mass-produced cars and Facel lost their big customers. French niche manufacturers ended production. Métallon left the partnership in 1953. Facel set about designing and making their own complete cars using engines made by Chrysler, Volvo and Austin. Their first design named Vega was shown to the public in 1954.
Though initially successful Facel closed its factory in October, 1964. Their Facellia model, introduced in 1959, was under-developed and losses brought about by its warranty problems became impossible to recoup. Prior to closure Facel had been placed under the control of Sud Aviation subsidiary SFERMA.
Facel, Forges et Ateliers de Constructions d'Eure-et-Loir, was founded 20 December, 1939 by Bronzavia, a French manufacturer of military aircraft to make special components. Jean Daninos, technical director of Bronzavia, had begun his career with Citroen where he assisted in the design of the Traction coupés and cabriolets. He moved to Morane-Saulnier then to Bronzavia. During WW II he worked with General Aircraft in USA who were using Bronzavia patents but he returned in 1945 and took charge of Facel. Facel merged with Metallon, a tie maintained until January, 1953.[1]
Daninos put Facel to the manufacture of short-run and special complete finished bodies for the major French brands. In conjunction with l'Aluminium Français Facel designed the all-aluminium alloy Panhard Dyna X and then built around 45,000 examples for Panhard.[1]
A luxury car division was established in 1948. It made various models of Simca Sport and drew publicity by designing with Farina and then building a special body on a Bentley Mark VI chassis. The car was named Bentley Cresta. The exercise was repeated in 1951 and named Cresta II. September 1951 saw the introduction of their Ford Comète. Production of the Comète ended in 1955 when Simca took over Ford France. The styling of the Crestas and Comètes was developed into the shape of the first Vega.[1]
During the same period Facel-Metallon pressed out body panels for: Delahaye's army jeeps (painted and upholstered) ; Simca, Delahaye and Somua's trucks (painted and upholstered); scooters by Vespa, Piaggio and Motobécane; tractors by Massey-Ferguson and stainless-steel bumpers, hubcaps and grilles for Simca and Ford and for Renault.[1]
In conjunction with Hispano-Suiza Facel-Metallon and Facel also turned out for Rolls-Royce combustion chambers in special metals for their jet engines.[1]
The marque Facel Vega was created in 1954 by Jean Daninos (brother of the humorist Pierre Daninos, who wrote Les Carnets du Major Thompson), although the Facel company had been established by the Bronzavia Company in 1939 as a subcontracting company for the aviation industry. FACEL (Forges et Ateliers de Construction d'Eure-et-Loir, in English: forge and construction workshop of the department of Eure-et-Loir) was initially a metal-stamping company but decided to expand into car manufacturing in the early 1950s.[2] Facel entered the automobile business as a supplier of special bodies for Panhard, Delahaye and Simca.
The Vega production cars (FV, later and more famously the HK500) appeared in 1954 using Chrysler V8 engines, at first a 276 cu in (4.5 L) DeSoto Hemi engine; the overall engineering was straightforward, with a tubular chassis, double wishbone suspension at the front and a live axle at the back, as in standard American practice. They were also as heavy as American cars, at about 1,800 kg (3,968 lb). Performance was brisk, with a top speed of around 190 km/h (118 mph) and 0 to 100 km/h (62 mph) in just under 10 seconds.
Most cars were two-door hardtops with no centre pillar, but a few convertibles were built. Fully 77% of production was exported, due to the punitive Tax horsepower system in France.[2]
The 1956 model was improved with a bigger 331 cu in (5.4 L) Chrysler engine and updated transmission and other mechanicals. In the same year production began of a four-door model, the Excellence, with rear-hinged doors (suicide doors) at the back and no centre pillar. The pillarless design unfortunately made it less rigid and the handling was thus poorer than that of the two-door cars, and surviving examples are rare.
1959 models had even bigger engines, a 5.8 L (354 cu in) and later a 6.28 L (383 cu in)[citation needed] Chrysler V8, and were quite a bit faster despite their extra weight. The final evolution of the V8 models came in 1962 with the Facel Vega II, which was lighter, with sleeker, more modern lines, substantially faster still, and famously elegant.
In 1960, Facel entered the sports car market with the Facellia, a small car similar in size to the then popular Mercedes 190SL. Facellias were advertised in three body styles: cabriolet, 2+2 coupé and 4-seat coupé — all with the same mechanical parts and a 2,450 mm (96.5 in) wheelbase. Styling was similar to the Facel HK500, but with rather elegant (though fingernail-breaking) flush door handles. Following Facel Vega's demise several of M Daninos's styling cues were "borrowed" by Mercedes-Benz.[citation needed] Prices were roughly US$4,000 for the Facellia, US$5,500 for the Facel III and US$6,000 for the Facel 6.[3]
With the idea of creating a mass-produced all-French sports car competing with the Alfa Romeos, Facel moved away from American engines. The Facellia had a 4-cylinder 1.6 L DOHC engine built in France by Paul Cavallier of the Pont-à-Mousson company (which already provided manual gear boxes for the company's larger models). The engine had only two bearings supporting each camshaft, using special steels, as opposed to the usual four or five. Despite the metallurgical experience of Pont-à-Mousson, this resulted in excessive flex, timing problems and frequent failures. Famed engineers Charles Deutsch and Jean Bertin were called in to solve the issues, but it was not enough and the engine was pronounced a disaster and the Facellia with it.[4] Company president, Jean Daninos having been obliged to resign in August 1961 in response to the company's financial problems, the new boss, a former oil company executive called André Belin, gave strict instructions to the after-sales department to respond to customer complaints about broken Facellia engines by replacing the units free of charge without creating "difficulties".[5] The strategy was intended to restore confidence among the company's customer base.[5] It would certainly have created a large hole in the income statement under the "warranty costs" heading, but it may have been too late for customer confidence.
The troublesome engine was replaced with a Volvo B18 powerplant in the Facel III, but the damage was done. Production was stopped in 1963 and despite the vision of it being a "volume" car, only 1,100 were produced - still enough to make this Facel's highest production number. Facel lost money on every car they built, with the luxury car side of the company being supported entirely by the other work done by Facel Metallon.[citation needed]
The small Facellia met with little success and the losses from this, due to strong competition at the luxury end of the market, killed off the business which closed its doors at the end of October, 1964. What was, according to some, the best small Facel, the Facel 6, which used an Austin-Healey 2.8-litre engine, came too late to save the company with fewer than 30 having been produced when the financial guarantors withdrew their support.
Prominent owners of Facel Vegas (mainly of Facel IIs) included Pablo Picasso, Ava Gardner, Christian Dior, Herb Alpert, Joan Collins, Ringo Starr, Max Factor Jr, Joan Fontaine, Stirling Moss, Tony Curtis, several Saudi princes, Dean Martin, Fred Astaire, Danny Kaye, Louis Malle, The President of Mexico, François Truffaut, Robert Wagner, Anthony Quinn, Hassan II, King of Morocco, Debbie Reynolds, the Shah of Persia, Frank Sinatra, Maurice Trintignant, Brian Rix, Joe Hepworth and French Embassies around the world.[6][7][8] Race-car driver Stirling Moss would drive his HK500 from event to event rather than fly.
French writer Albert Camus died in a Facel Vega FV3B driven by his publisher, Michel Gallimard.[9] At the time of his death, Camus had planned to travel by train, with his wife and children, but at the last minute accepted his publisher's proposal to travel with him.[10]
In the 1989 film "Dealers", Paul McGann, as Daniel Pascoe, drives a Facel ll.
A Facel Vega HK500 appears in computer-animated form in the film Ratatouille (Pixar, 2007), driven by one of the main characters.
A Facel Vega Facellia appeared in the music video for Caravan Palace's Dramophone.[11]
A 1958 Facel Vega HK500 appeared in the 1961 Movie Goodbye Again starring Ingrid Bergman, Yves Montand and Anthony Perkins.[12]
Chief Inspector Swan Laurence drives a wine-red Facel Véga Facellia F2 Coupé in the television series Les Petits Meurtres d'Agatha Christie, season 2 (2013).[13]
Wikimedia Commons has media related to Facel S.A.. |
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer