powered by CADENAS

Social Share

Amazon

Industrial processes (5682 views - Mechanical Engineering)

Industrial processes are procedures involving chemical, physical, electrical or mechanical steps to aid in the manufacturing of an item or items, usually carried out on a very large scale. Industrial processes are the key components of heavy industry.
Go to Article

Explanation by Hotspot Model

Youtube


    

Industrial processes

Industrial processes

Industrial processes are procedures involving chemical, physical, electrical or mechanical steps to aid in the manufacturing of an item or items, usually carried out on a very large scale. Industrial processes are the key components of heavy industry.

General processes

These may be applied on their own, or as part of a larger process.

Chemical processes

  • Haber process – chemically binding gaseous nitrogen from the atmosphere to make ammonia
  • Smelting – chemically enhancing metals
  • Disinfection – chemical treatment to kill bacteria and viruses
  • Pyroprocessing – using heat to chemically combine materials, such as in cement.

Heat processes

  • Flash smelting – a refinement on smelting, for sulfur-containing ores (produces copper, nickel and lead)

Electrolysis

The availability of electricity and its effect on materials gave rise to several processes for plating or separating metals.

Cutting

Physical processes

There are several physical processes for reshaping a material by cutting, folding, joining or polishing, developed on a large scale from workshop techniques.

Moulding

The physical shaping of materials by forming their liquid form using a mould.

Separation

Many materials exist in an impure form, purification, or separation provides a usable product.

Distillation

Additive

Iron and steel

Early production of iron was from meteorites, or as a by-product of copper refining.

Petroleum and organic compounds

The nature of an organic molecule means it can be transformed at the molecular level to create a range of products.

Others

Organized by product:

A list by process:

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD