powered by CADENAS

Social Share

V-block (6671 views - Tooling)

V-Blocks are precision metalworking jigs typically used to hold round metal rods or pipes for performing drilling or milling operations. They consist of a rectangular steel or cast iron block with a 90-degree channel rotated 45-degrees from the sides, forming a V-shaped channel in the top. A small groove is cut in the bottom of the "V". They often come with screw clamps to hold the work. There are also versions with internal magnets for magnetic work-holding. V-blocks are usually sold in pairs.
Go to Article

Explanation by Hotspot Model

V-block

V-block

V-Blocks are precision metalworking jigs typically used to hold round metal rods or pipes for performing drilling or milling operations. They consist of a rectangular steel or cast iron block with a 90-degree channel rotated 45-degrees from the sides, forming a V-shaped channel in the top. A small groove is cut in the bottom of the "V". They often come with screw clamps to hold the work. There are also versions with internal magnets for magnetic work-holding. V-blocks are usually sold in pairs.

The inventor of an improved magnetic V-block was Harold Arlington Spanker http://patentimages.storage.googleapis.com/pdfs/US2449255.pdf



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing