powered by CADENAS

Social Share

DiMarzio (6652 views - Brands)

DiMarzio, Inc. (original name: DiMarzio Musical Instrument Pickups, Inc.) is a United States manufacturer best known for its direct-replacement guitar pickups. The company also produces miscellaneous guitar accessories, such as cables, straps and hardware. DiMarzio became known for its Super Distortion model, which was the first after-market replacement guitar pickup. It was introduced in 1972 and is still one of the most popular models. The Super Distortion pickup produced a higher electrical output than the pickups normally fitted as standard to guitars at the time. It has around twice the output of a PAF-type pickup, and stronger ceramic magnets. This drove the input stage of guitar amplifiers with roughly twice as much voltage as a PAF pickup, so that an overdriven distorted sound was easier to obtain. Two of the technologies that they are known for are: their Dual-Resonance design which uses two asymmetrical coils tuned to different frequencies to produce unique sounds. their Airbucker™ design which reduces string pull and increases sensitivity and sustain.
Go to Article

Explanation by Hotspot Model

DiMarzio

DiMarzio

DiMarzio Inc.
Private
Products Guitar pickups
Website DiMarzio.com

DiMarzio, Inc. (original name: DiMarzio Musical Instrument Pickups, Inc.) is a United States manufacturer best known for its direct-replacement guitar pickups.[1] The company also produces miscellaneous guitar accessories, such as cables, straps and hardware.

DiMarzio became known for its Super Distortion model, which was the first after-market replacement guitar pickup. It was introduced in 1972 [2] and is still one of the most popular models.

The Super Distortion pickup produced a higher electrical output than the pickups normally fitted as standard to guitars at the time. It has around twice the output of a PAF-type pickup, and stronger ceramic magnets. This drove the input stage of guitar amplifiers with roughly twice as much voltage as a PAF pickup, so that an overdriven distorted sound was easier to obtain.

Two of the technologies that they are known for are:

  • their Dual-Resonance design which uses two asymmetrical coils tuned to different frequencies to produce unique sounds.
  • their Airbucker™ design which reduces string pull and increases sensitivity and sustain.

Notable users past and present

Patents

Lawrence P. DiMarzio holds following US patents:

  • US patent 4133243, DiMarzio, Lawrence P., "Electric pickup", issued 1979-01-09 
  • US patent 4227434, DiMarzio, Lawrence P., "Adjustable soundhole mount for a musical pickup", issued 1980-10-14 
  • US patent 4320829, DiMarzio, Lawrence P.; Altilio, Daniel, "Merchandise display container", issued 1982-03-23  — a special container for merchandising pickups.
  • US patent 4442749, DiMarzio, Lawrence P.; Blucher, Steven L., "Electrical pickup for a stringed instrument having ferromagnetic strings", issued 1984-04-17 
  1. ^ Guitar World Magazine May 1994
  2. ^ DiMarzio Super Distortion Specifications
  3. ^ "DiMarzio Twang King Neck & The Chopper T Bridge Pickups for Richie Kotzen | DiMarzio". www.dimarzio.com. 2014-01-10. Retrieved 2017-05-11. 
  4. ^ "FUGAZI: A guitar gear summary (Guest Post)". Effects Bay. 2010. Retrieved 1 June 2014. 

Further reading

  • Guitar World Magazine, "The 100 Most Important People In Guitar", San Francisco, CA, May 1994.


This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Brands

3D,brand,good,trademark,company,copyright,good