powered by CADENAS

Social Share

Gittler guitar (8619 views - Music)

A Gittler Guitar is an experimental designed guitar created by Allan Gittler (1928–2002). Gittler felt that sentimental design references to acoustic guitars are unnecessary in an electronically amplified guitar, and designed his instrument with the objective of reducing the electric guitar to the most minimal functional form possible.
Go to Article

Explanation by Hotspot Model

Gittler guitar

Gittler guitar

Gittler guitar

Licensed under Creative Commons Attribution 2.0 (Frank Kovalchek from Anchorage, Alaska, USA).

A Gittler Guitar is an experimental designed guitar created by Allan Gittler (1928–2002).[1] Gittler felt that sentimental design references to acoustic guitars are unnecessary in an electronically amplified guitar, and designed his instrument with the objective of reducing the electric guitar to the most minimal functional form possible.

History

He made 60 guitars in New York in the mid-1970s to early 1980s (selling one to Andy Summers, which he plays in The Police's "Synchronicity II" video). In 1982, Gittler emigrated to Israel, settled in Hebron, changed his name to Avraham Bar Rashi, and licensed the design to a local company in Kiryat Bialik called Astron Engineer Enterprises LTD. They computer-machined around 300, Bar Rashi commented later to the effect that he was unhappy with the manufacturing. Astron, however, claims that their instruments are precisely manufactured copies of the original construction, and that the addition of a plastic body containing electronics for simplified handling, while arguably compromising the minimalism of the original idea, had no influence on the sound or the style of playing.

The first 60 are sometimes described as the Fishbone Gittler guitar. Three Gittler basses also exist, made in New York and numbered 1, 2, and 3.

During this period, he also made a portable, battery-powered amplifier, cylindrical in shape, with a long handle that allowed it to be rolled around like a grass-seed-roller. Rolling was necessary to transport it through the street, since it was quite heavy due to the large number of D batteries that powered it. He frequently used this set-up to play his guitar in a street adjoining Astor Place in lower Manhattan, where the reverberation from the surrounding buildings amplified the sound.

The Gittler guitar has six strings. Each string has its own pickup. Later versions have a plastic body. The steel frets, consisting of stainless steel bars pressure fitted into the stainless steel neck, give the instrument a sitar-like feel, as it is possible to bend the strings downward past where a wooden fretboard would prohibit the movement in a conventional guitar. The six individual pickups can be routed to divided outputs via D-sub-9-pin. or be mixed to a 1/4" TS connector. The built in pre-amps are powered by a 9 V battery or via D-sub connector. The New York version came without a pre-amp section; the individual pickups' signals were led into single cables, which could then be plugged into a mixing box or each separately amplified.

The Museum of Modern Art, MOMA has one instrument in its collection, as does the Boston Museum of Fine Arts (which also has a later Bar Rashi wooden electric guitar). Gittler guitars can also be seen in several other museums and collections.

The only left-handed Gittler guitar known to exist was made by Bar Rashi himself in 1995 or 1996. It is a signed minimalist instrument, identical to the one he played in the later period of his life and made to order for a client in Jerusalem. There are only 12 separate parts in total and the frets are one long thread of nylon. This creates a unique sound.

Current Production

After Bar Rashi's passing in 2003, his eldest son, Yonatan, became a partner in Gittler Instruments LLC. The company has returned to manufacturing the Gittler guitar and presently sells the instruments online [2]. Gittler Instruments president Russ Rubman has extended the company's line to include upright basses and violins designed with the same principles of the original Gittler Guitar [3].




This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Music

3d,printed,3dprinting,3dprint,music,song,dvd,dcrom,schellak,top hit