powered by CADENAS

Social Share

Car seat (10328 views - Cars & Motorbikes & Trucks & Buse)

A car seat is the seat used in automobiles. Most car seats are made from inexpensive but durable material in order to withstand prolonged use. The most common material is polyester.
Go to Article

Car seat

Car seat

Car seat

A car seat is the seat used in automobiles. Most car seats are made from inexpensive but durable material in order to withstand prolonged use. The most common material is polyester.[citation needed]

Bucket seat and bench seat

A bucket seat is a separate seat with a contoured platform designed to accommodate one person, distinct from a bench seat that is a flat platform designed to seat up to three people. Individual bucket seats typically have rounded backs and may offer a variety of adjustments to fit different passengers.

Folding seats

Early touring cars featured folding auxiliary seats to offer additional passenger capacity.[1] Some early automobiles were available with an exterior rumble seat that folded open into an upholstered seat for one or two passengers.

Some sedan models offer fold-down rear seats (e.g. Chevrolet Corvair), to gain cargo space when they are not occupied by passengers.

A fold-down front-passenger seat was a feature on the Chrysler PT Cruiser to fit longer items such as a 8-foot (2.4 m) ladder inside the vehicle.[2]

Ergonomy: lumbar and thigh support

The lumbar is the region of the spine between the diaphragm and the pelvis; it supports the most weight and is the most flexible. The adjustable lumbar mechanisms in seats allow the user to change the seat back shape in this region, to make it more comfortable and include adjustable lumbar cushion. Some seats are long enough to support full thigh and follow back curves.

Safety

The National Traffic and Motor Vehicle Safety Act enacted by the U.S. in 1966 established standards of strength for automobile seats. These included requirements for proper anchorage and construction of automobile vehicle seat assemblies.[3] The legal requirements in some jurisdictions for a child to sit up front is 5'0 and they must weigh more than 80 lbs. Some studies have shown that drivers have an aversion towards carrying the full capacity amount of passengers due to concerns over insufficient vision through the back window.[4]

  • An anti-submarine seat is a kind of seat that incorporates specially shaped panels in the forward edge of the seat cushion, reducing the tendency for the occupant to slide beneath the seatbelt in a severe frontal collision. Anti-submarine seating is a safety feature that may be more important for the front seats than the rear seats.[5]
  • A child safety seat or child restraint system is a restraint which is secured to the seat of an automobile equipped with safety harnesses or seat belts, to hold a child in the event of a crash. All 50 states require child seats with specific criteria. Requirements vary based on a child's age, weight and height. The National Child Passenger Safety Board, managed by the National Safety Council, maintains the quality and integrity of the National Child Passenger Safety Certification Training Program. The program is used to train and certify child passenger safety technicians and instructors in order to assist caregivers in safe transportation of children.[6]

Side airbags are often built right into the side of the seat. Seats so equipped should not be covered which impedes the operation of the airbag.[7]

Power seats

Some car seat systems are set up with a battery-powered automatic control to adjust how the seat sits in the car.

In suitably equipped cars, seats and mirrors can be adjusted using electric controls. Some vehicles let the driver(s) save the adjustments in memory (memory seat) for later recall, with the push of a button. Most systems allow users to store more than one set of adjustments. This allows multiple drivers to store their comfort settings, or a single driver to store several different occupant positions. Some vehicles associate memorized settings with a specifically numbered, remotely operated key fob, resetting a seat to the position associated with that fob when the vehicle is unlocked (e.g. key fob #1 sets seats to memory position #1, #2 to #2, etc.).

Covers

Car seat covers are accessories that protect the original seat upholstery from wear and add a custom look to a vehicle's interior. They can help to maintain the resale value of the vehicle and maximize the comfort of the driver and passengers.

Seat construction

Parts

Adjustments

  • Backrest angle
  • Cushion edge
  • Fore-and-aft position
  • Headrest angle
  • Headrest level
  • Lumbar position
  • Seat depth
  • Seat height
  • The upper section of the seat backrest, may be tilted to the front for optimum, individual shoulder support
  • Variable head support at the sides
  • Cushion Tilt
  • Turning Seat

Climate control and ventilation

Some vehicles includes the option of seat climate control (i.e. heating by seat warmers) and ventilation. Ventilation was introduced in 1997 by Saab and heating by Cadillac in 1966.

See also


Alfa Romeo 4CAlfa Romeo GiuliaAll-terrain vehicle阿斯顿·马丁雅士頓馬田DB5Aston Martin DBR1Aston Martin Vantage奥迪A3奥迪R8Audi RS 4Audi Sportback conceptBentley Continental賓利Continental GT自行車Bicycle fork盲點偵測系統小轮车Bowl sink布加迪威龙保险杠公共汽車汽车CarriageCaudron雪佛兰科尔维特Chevrolet Corvette (C2)Chevrolet Corvette C6.RChrysler Hemi engineCoandă-1910PBY卡特琳娜水上飛機Defect detectorDeLorean DMC-12迪羅倫時光機道奇毒蛇Ducati DiavelFarman SportFerrari 250 GT法拉利加利福尼亚Fish-class sloopFokker SpinFord Cortina叉车Fuji FA-200 Aero Subaru直升機吉普汽車JNR Class C62朱诺号Kayak克卜勒太空望遠鏡Lake Renegade蘭博基尼Aventador兰博基尼Huracán林寶堅尼Miura鐵路機車Logging truck迈凯伦MP4-12C梅赛德斯 (消歧义)Mercedes-Benz 300 SL梅赛德斯-奔驰S级梅赛德斯-奔驰SLK级梅赛德斯-奔驰SLS AMG三菱集团摩托車日產汽車越野车欧宝Pagani HuayraPagani Zonda保时捷550保时捷911螺旋槳Rail transport轉轍器火箭Santos-Dumont 14-bisScooterSelf-balancing scooter新幹線Ship雪橇扫雪机车速限制跑车Steamroller方向盘潛艇噴火戰鬥機輪胎Trabant 拖拉机Train自行三轮车载货汽车V8发动机廂型車大众汽车WagonWright Model BYacht前轮驱动賽車場賽車秋千模型车Torque limiter底盘Bucket seatPendulum car車禍Automobile safety座位安全帶Stock car racing斯特林·莫斯Mercedes-Benz 300 SLRFacel Vega豪華旅行車豪華汽車轎跑車公路Ferrari 246 F1凌志ISCompact executive car紧凑型轿车Mid-engine designSport compactKoenigsegg AgeraRenault Twizy电动汽车充电式电动车辆Quadricycle (EU vehicle classification)迷你车法蘭克福車展迈凯伦汽车三級方程式賽車方程式赛车比赛開輪式賽車Auto Union racing car大奖赛赛车Road racing二級方程式賽車Lada NivaFiat 500 (2007)BMW M6BMW 6系列漂浮滑板HovercarMicro kartShow car

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks

Car, Truck,MotorBike, Bicycle, Engine, Racer