powered by CADENAS

Social Share

Zirconium hydride (15267 views - Material Database)

Zirconium hydride describes an alloy made by combining zirconium and hydrogen. Hydrogen acts as a hardening agent, preventing dislocations in the zirconium atom crystal lattice from sliding past one another. Varying the amount of hydrogen and the form of its presence in the zirconium hydride (precipitated phase) controls qualities such as the hardness, ductility, and tensile strength of the resulting zirconium hydride. Zirconium hydride with increased hydrogen content can be made harder and stronger than zirconium, but such zirconium hydride is also less ductile than zirconium.
Go to Article

Zirconium hydride

Zirconium hydride

Zirconium hydride describes an alloy made by combining zirconium and hydrogen. Hydrogen acts as a hardening agent, preventing dislocations in the zirconium atom crystal lattice from sliding past one another. Varying the amount of hydrogen and the form of its presence in the zirconium hydride (precipitated phase) controls qualities such as the hardness, ductility, and tensile strength of the resulting zirconium hydride. Zirconium hydride with increased hydrogen content can be made harder and stronger than zirconium, but such zirconium hydride is also less ductile than zirconium.

Material properties

Zirconium is found in the Earth's crust only in the form of an ore, usually a zirconium silicate, such as zircon. Zirconium is extracted from zirconium ore by removing the oxygen and silica. This process, known as the Kroll process, was first applied to titanium. The Kroll process results in an alloy containing hafnium. The hafnium and other impurities are removed in a subsequent step. Zirconium hydride is created by combining refined zirconium with hydrogen. Like titanium, solid zirconium dissolves hydrogen quite readily.

The density of zirconium hydride varies based the hydrogen and ranges between 5.56 and 6.52 g cm−3.

Even in the narrow range of concentrations which make up zirconium hydride, mixtures of hydrogen and zirconium can form a number of different structures, with very different properties. Understanding such properties is essential to making quality zirconium hydride. At room temperature, the most stable form of zirconium is the hexagonal close-packed (HCP) structure α-zirconium. It is a fairly soft metallic material that can dissolve only a small concentration of hydrogen, no more than 0.069 wt% at 550 °C. If zirconium hydride contains more than 0.069% hydrogen at zirconium hydride making temperatures then it transforms into a body-centred cubic (BCC) structure called β-zirconium. It can dissolve considerably more hydrogen, more than 1.2% hydrogen above 900 °C.

When zirconium hydrides with less than 0.7% hydrogen, known as hypoeutectoid zirconium hydride, are cooled from the β phase the mixture attempts to revert to the α phase, resulting in an excess of hydrogen.

Another polymorphic form is the γ phase, is generally accepted to be a metastable phase.

Approximate formula CAS number Molecular
weight
Density
g/cm3
Symmetry Space group No Pearson symbol
ZrH 13940-37-9 92.232 5.9[1] Orthorhombic[2] Cccm 66 oS8
ZrH1.6 5.66 Cubic[3] Fm3m 225 cF12
ZrH2 7704-99-6 93.240 5.56 Tetragonal[4] I4/mmm 139 tI6
ZrH4 15457-96-2 95.256

Zirconium hydrides are odorless, dark gray to black metallic powders.[5] They behave as usual metals in terms of electrical conductivity and magnetic properties (paramagnetic, unless contaminated with ferromagnetic impurities). Their structure and composition is stable at ambient conditions.[6] Similar to other metal hydrides, different crystalline phases of zirconium hydrides are conventionally labeled with Greek letters, and α is reserved for the metal. The known ZrHx phases are γ (x = 1), δ (x = 1.5–1.65) and ε (x = 1.75–2). Fractional x values often correspond to mixtures, so the compositions with x = 0.8–1.5 usually contain a mixture of α, γ and δ phases, and δ and ε phases coexist for x = 1.65–1.75. As a function of increasing x, the transition between δ-Zr and ε-Zr is observed as a gradual distortion of the face-centered cubic δ (fluorite-type) to face-centered tetragonal ε lattice. This distortion is accompanied by a rapid decrease in Vickers hardness, which is constant at 260 HV for x < 1.6, linearly decreases to 160 HV for 1.6 < x < 1.75 and stabilizes at about 160 HV for 1.75 < x < 2.0.[7] This hardness decrease is accompanied by the decrease in magnetic susceptibility.[3][4] The mass density behaves differently with the increasing hydrogen content: it decreases linearly from 6.52 to 5.66 g/cm3 for x = 0–1.6 and changes little for x = 1.6–2.0.[1]

Preparation and chemical properties

Zirconium hydrides form upon interaction of the metal with hydrogen gas. Whereas this reaction occurs even at room temperature, homogeneous bulk hydrogenation is usually achieved by annealing at temperatures of 400–600 °C for a period between several hours and a few weeks.[3] At room temperature, zirconium hydrides quickly oxidize in air, and even in high vacuum. The formed nanometer-thin layer of oxide stops further oxygen diffusion into the material, and thus the change in composition due to oxidation can usually be neglected. However, the oxidation proceeds deeper into the bulk with increasing temperature.[6]

Zirconium hydrides are soluble in hydrofluoric acid or alcohol; they react violently with water, acids, oxidizers or halogenated compounds.[5]

Applications

Formation of zirconium hydrides is an important factor in the operation of several types of nuclear reactors, such as boiling water reactors Fukushima I and II, which suffered from a series of explosions caused by the 2011 Tōhoku earthquake and tsunami. Their uranium fuel pellets are enclosed in metal rods made from Zircaloy – an alloy of typically about 98.25% zirconium with 1.5% tin and minor amounts of other metals. Zircaloy is used because of its small absorption cross-section for thermal neutrons and superior mechanical and corrosion properties to those of most metals, including zirconium.[8][9][10] The rods are cooled by streaming water which gradually oxidizes zirconium, liberating hydrogen. In Fukushima reactors, the reactor cooling system failed because of the tsunami. The resulting temperature increase accelerated chemical reactions and caused accumulation of significant amounts of hydrogen, which exploded upon reaction with oxygen when the gas was released to the atmosphere.[11]

In regular operation, most hydrogen is safely neutralized in the reactor systems; however, a fraction of 5-20% diffuses into the Zircaloy rods forming zirconium hydrides.[8] This process mechanically weakens the rods because the hydrides have lower hardness and ductility than metal. Only a few percent of hydrogen can dissolve in zirconium. Excess hydrogen forms voids that weaken Zircalloy.[10] Among Zircaloys, Zircaloy-4 is the least susceptible to hydrogen blistering.[8]

It is also used as a neutron moderator in thermal-spectrum nuclear reactors such as the TRIGA research reactor developed by General Atomics or the Soviet TOPAZ nuclear reactors. At neutron energies above 0.14 eV it is as effective at moderating a nuclear reactor as elemental hydrogen (the best known material), but far more dense, and therefore permits compact reactors with high power per unit volume. It has neutron resonances that prevent almost all moderation at energies below 0.14 eV. Zirconium deuteride is superior, because it has a lower neutron absorption cross-section than aneutronic hydrogen, decreasing neutron absorption in a reactor.[12][13][14]

As a pure powder, zirconium hydrides are used as hydrogenation catalysts, in powder metallurgy, and as getters in the vacuum tube industry.[5] In vacuum system, zirconium hydrides help establish a seal between a metal and ceramic. In this method, a hydride powder (particularly ZrH4) is mixed with the sealing metal; heating the mixture results in decomposition of the hydride. The evolving hydrogen cleans up the surrounding area, and the produced metal flows and forms a seal even at temperatures as low as 300 °C.[15]

ZrH2 is used in powder metallurgy, as a hydrogenation catalyst, and as a reducing agent, vacuum tube getter, and a foaming agent in production of metal foams. Other uses include acting as a fuel in pyrotechnic compositions, namely pyrotechnic initiators.

Safety

Powdered zirconium hydrides are flammable and can ignite and explode if exposed to heat, fire, or sparks. When heated above 300 °C, they decompose releasing hydrogen gas, which is also flammable.[5]

  1. ^ a b Atwood, J. D.; Zuckerman, J. J. (1999). Inorganic reactions and methods: Formation of ceramics. John Wiley and Sons. pp. 377–. ISBN 978-0-471-19202-2. Retrieved 16 March 2011. 
  2. ^ Switendick, A. C. (1984). "Electronic structure of γ phase zirconium hydride". Journal of the Less-Common Metals. 103 (2): 309–315. doi:10.1016/0022-5088(84)90254-6. 
  3. ^ a b c Bowman, R.; Craft, B.; Cantrell, J.; Venturini, E. (1985). "Effects of thermal treatments on the lattice properties and electronic structure of ZrHx". Physical Review B. 31 (9): 5604–5615. doi:10.1103/PhysRevB.31.5604. 
  4. ^ a b Niedźwiedź, K.; Nowak, B.; Żogał, O. (1993). "91Zr NMR in non-stoichiometric zirconium hydrides, ZrHx (1.55 ≤ x ≤ 2)". Journal of Alloys and Compounds. 194 (1): 47–51. doi:10.1016/0925-8388(93)90643-2. 
  5. ^ a b c d Occupational Safety and Health Guideline for Zirconium & Compounds Archived July 21, 2011, at the Wayback Machine., Occupational Safety & Health Administration, U.S. Department of Labor
  6. ^ a b Bowman, R.; Venturini, E.; Craft, B.; Attalla, A.; Sullenger, D. (1983). "Electronic structure of zirconium hydride: A proton NMR study". Physical Review B. 27 (3): 1474–1488. doi:10.1103/PhysRevB.27.1474. 
  7. ^ Korn, C. (1983). "NMR study comparing the electronic structures of ZrHx and TiHx". Physical Review B. 28 (1): 95–111. doi:10.1103/PhysRevB.28.95. 
  8. ^ a b c DOE-HDBK-1017/2-93 JANUARY 1993, DOE FUNDAMENTALS HANDBOOK, MATERIAL SCIENCE, Volume 2 of 2, U.S. Department of Energy january 2003, pp. 12, 24
  9. ^ Nuclear Fuel Fabrication Archived July 26, 2011, at the Wayback Machine., Fuel Fabrication Archived July 26, 2011, at the Wayback Machine. World Nuclear Association, March 2010
  10. ^ a b Delayed hydride cracking in zirconium alloys in pressure tube nuclear reactors, Final report of a coordinated research project 1998–2002, IAEA, October 2004
  11. ^ Japanese engineers work to contain nuclear reactor damage, Los Angeles Times, March 14, 2011
  12. ^ Baron, Matthias; Böck, Helmuth; Villa, Mario. "TRIGA Reactor Characteristics". IAEA Education and Training. IAEA. Retrieved 2 June 2016. 
  13. ^ Gylfe, J.D. "US Patent 3,145,150, Aug. 18, 1954, Fuel Moderator Element for a Nuclear Reactor, and Method of Making". U.S. Patent Office. U.S. Government. Retrieved 2 June 2016. 
  14. ^ Massie, Mark; Dewan, Leslie C. "US 20130083878 A1, April 4, 2013, NUCLEAR REACTORS AND RELATED METHODS AND APPARATUS". U.S. Patent Office. U.S. Government. Retrieved 2 June 2016. 
  15. ^ Alexander Roth (1994). Vacuum sealing techniques. Springer. pp. 212–. ISBN 978-1-56396-259-2. Retrieved 16 March 2011. 

41xx steelAL-6XNAlGaAlloy 20鋁鎳鈷合金Alumel鋁合金Aluminium bronzeAluminium-lithium alloy汞齊Argentium sterling silverArsenical bronzeArsenical copper巴氏合金Bell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅BrightrayBritannia metalBritannia silver青铜Bulat steelCalamine brass铸铁CelestriumChinese silverChromelChromium hydride白金 (合金)康銅氢化亚铜Copper–tungstenCorinthian bronzeCrown goldCrucible steelCunife白铜Cymbal alloys大馬士革鋼Devarda's alloyDoré bullion杜拉鋁Dutch metal电工钢琥珀金Elektron (alloy)ElinvarFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstanGilding metal玻璃GlucydurGoloidGuanín (bronze)Gum metalGunmetalHaynes InternationalHepatizonHiduminium高速鋼High-strength low-alloy steelHydronalium英高鎳合金不變鋼Iron–hydrogen alloyItalmaKanthal (alloy)Kovar镁铝合金Magnox (alloy)MangalloyManganin马氏体时效钢Marine grade stainless马氏体不锈钢MegalliumMelchior (alloy)MercuryMischmetalMolybdochalkosMonelΜ合金Muntz metalMushet steelNichromeNickel hydrideNickel silverNickel titaniumNicrosilNisil北歐金Ormolu透磁合金PewterPhosphor bronze生鐵Pinchbeck (alloy)塑料Platinum sterlingPlexiglasPlutonium–gallium alloyPseudo palladiumQueen's metalReynolds 531銠金礦Rose's metal釤鈷磁鐵Sanicro 28Scandium hydrideShakudōShibuichiSilver steel钠钾合金銲料Speculum metalSpiegeleisenSpring steelStaballoy不鏽鋼StelliteSterling silver钢结构超導磁率合金Surgical stainless steelTerfenol-DTerneTibetan silverTitanium alloyTi Beta-C.Titanium gold氢化钛氮化钛TombacTool steelTumbagaType metal氢化铀維塔立合金耐候钢White metal伍德合金烏茲鋼Y alloyZamakZeron 100甲烷Mezzanine原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material