powered by CADENAS

Social Share

Pewter (15456 views - Material Database)

Pewter is a malleable metal alloy. It is traditionally composed of 85–99% tin, mixed with copper, antimony, bismuth, and sometimes lead, although the use of lead is less common today. Silver is also sometimes used. Copper and antimony act as hardeners while lead is more common in the lower grades of pewter, which have a bluish tint. Pewter has a low melting point, around 170–230 °C (338–446 °F), depending on the exact mixture of metals. The word pewter is probably a variation of the word spelter, a term for zinc alloys (originally a colloquial name for zinc).
Go to Article

Pewter

Pewter

Pewter is a malleable metal alloy. It is traditionally composed of 85–99% tin, mixed with copper, antimony, bismuth, and sometimes lead, although the use of lead is less common today. Silver is also sometimes used. Copper and antimony act as hardeners while lead is more common in the lower grades of pewter, which have a bluish tint. Pewter has a low melting point, around 170–230 °C (338–446 °F), depending on the exact mixture of metals.[1] The word pewter is probably a variation of the word spelter, a term for zinc alloys (originally a colloquial name for zinc).[2]

History

Pewter was first used around the beginning of the Bronze Age in the Near East. The earliest piece of pewter found is from an Egyptian tomb from 1450 BC.[3]

Types

Pieces of pewter

The constituents of pewter were first controlled in the 12th century by town guilds in France. By the 15th century, the Worshipful Company of Pewterers controlled pewter constituents in England. This company originally had two grades of pewter, but in the 16th century a third grade was added. The first type, known as "fine metal", was used for tableware. It consisted of tin with as much copper as it could absorb, which is about 1%. The second type, known as "trifling metal" or "trifle", was used for holloware and is made up of fine metal with approximately 4% lead. The last type of pewter, known as "lay" or "ley" metal, was used for items that were not in contact with food or drink. It consisted of tin with 15% lead. These three alloys were used with little variation until the 20th century.[3]

Older pewters with higher lead content are heavier, tarnish faster, and oxidation gives them a darker silver-gray color.[4] Pewters containing lead are no longer used in items (such as cups, plates, or jewelry) that will come in contact with the human body due to health concerns stemming from the lead content. Modern pewters are available that are completely free of lead, although many pewters containing lead are still being produced for other purposes.[citation needed]

A typical European casting alloy contains 94% tin, 1% copper, and 5% antimony. A European pewter sheet would contain 92% tin, 2% copper, and 6% antimony. Asian pewter, produced mostly in Malaysia, Singapore, and Thailand, contains a higher percentage of tin, usually 97.5% tin, 1% copper, and 1.5% antimony. This makes the alloy slightly softer.[3]

Uses

Pewter was used in the ancient world by the Egyptians and later the Romans, and came into extensive use in Europe from the Middle Ages[5] until the various developments in pottery and glass-making during the 18th and 19th centuries. Pewter items are often found in churches. Pewter was the chief tableware until the making of porcelain. Mass production of pottery, porcelain and glass products has seen pewter universally replaced in day-to-day life. Pewter artifacts continue to be produced, mainly as decorative or specialty items. Pewter was also used around East Asia. Although some items still exist,[6] Ancient Roman pewter is rare.[7]

"Unlidded" mugs and lidded tankards may be the most familiar pewter artifacts from the late 17th and 18th centuries, although the metal was also used for many other items including porringers, plates, dishes, basins, spoons, measures, flagons, communion cups, teapots, sugar bowls, beer steins, and cream jugs. In the early 19th century, changes in fashion caused a decline in the use of pewter flatware. At the same time, production increased of both cast and spun pewter tea sets, whale-oil lamps, candlesticks, and so on. Later in the century, pewter alloys were often used as a base metal for silver-plated objects.[citation needed]

In the late 19th century, pewter came back into fashion with the revival of medieval objects for decoration. New replicas of medieval pewter objects were created, and collected for decoration. Today, pewter is used in decorative objects, mainly collectible statuettes and figurines, game figures, aircraft and other models, (replica) coins, pendants, plated jewellery and so on. Certain athletic contests, such as the United States Figure Skating Championships, award pewter medals to the fourth-place finishers.[8]

See also


41xx steelAL-6XNAlGaAlloy 20鋁鎳鈷合金Alumel鋁合金Aluminium bronzeAluminium-lithium alloy汞齊Argentium sterling silverArsenical bronzeArsenical copper巴氏合金Bell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅BrightrayBritannia metalBritannia silver青铜Bulat steelCalamine brass铸铁CelestriumChinese silverChromelChromium hydride白金 (合金)康銅氢化亚铜Copper–tungstenCorinthian bronzeCrown goldCrucible steelCunife白铜Cymbal alloys大馬士革鋼Devarda's alloyDoré bullion杜拉鋁Dutch metal电工钢琥珀金Elektron (alloy)ElinvarFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstanGilding metal玻璃GlucydurGoloidGuanín (bronze)Gum metalGunmetalHaynes InternationalHepatizonHiduminium高速鋼High-strength low-alloy steelHydronalium英高鎳合金不變鋼Iron–hydrogen alloyItalmaKanthal (alloy)Kovar镁铝合金Magnox (alloy)MangalloyManganin马氏体时效钢Marine grade stainless马氏体不锈钢MegalliumMelchior (alloy)MercuryMischmetalMolybdochalkosMonelΜ合金Muntz metalMushet steelNichromeNickel hydrideNickel silverNickel titaniumNicrosilNisil北歐金Ormolu透磁合金Phosphor bronze生鐵Pinchbeck (alloy)塑料Platinum sterlingPlexiglasPlutonium–gallium alloyPseudo palladiumReynolds 531銠金礦Rose's metal釤鈷磁鐵Sanicro 28Scandium hydrideShakudōShibuichiSilver steel钠钾合金銲料Speculum metalSpiegeleisenSpring steelStaballoy不鏽鋼StelliteSterling silver钢结构超導磁率合金Surgical stainless steelTerfenol-DTerneTibetan silverTitanium alloyTi Beta-C.Titanium gold氢化钛氮化钛TombacTool steelTumbagaType metal維塔立合金耐候钢伍德合金烏茲鋼Y alloyZeron 100Queen's metalWhite metal氢化铀ZamakZirconium hydride甲烷Mezzanine原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material