powered by CADENAS

Social Share

Britannia metal (14588 views - Material Database)

Britannia metal (also called britannium or Britannia ware) is a specific type of pewter alloy, favoured for its silvery appearance and smooth surface. The composition is typically about 92% tin, 6% antimony, and 2% copper. Britannia metal is usually spun rather than cast, and melts at 255 degrees Celsius.
Go to Article

Britannia metal

Britannia metal

Britannia metal (also called britannium or Britannia ware[1]) is a specific type of pewter alloy, favoured for its silvery appearance and smooth surface. The composition is typically about 92% tin, 6% antimony, and 2% copper.[2]

Britannia metal is usually spun rather than cast,[1] and melts at 255 degrees Celsius.[3]

History

Britannia metal was first produced[4] in 1769 or 1770. James Vickers created it after purchasing the formula from a dying friend. It was originally known as "Vickers White Metal" when made under contract by the Sheffield manufacturers Ebenezer Hancock and Richard Jessop. In 1776 James Vickers took over the manufacturing himself and remained as owner until his death in 1809, when the company passed to his son John and son-in-law Elijah West. In 1836 the company was sold to John Vickers's nephew Ebenezer Stacey (the son of Hannah Vickers and John Stacey).

After the development of electroplating with silver in 1846, Britannia metal was widely used as the base metal for silver-plated household goods and cutlery.[5] The abbreviation EPBM on such items denotes "electroplated Britannia metal". Britannia metal was generally used as a cheaper alternative to electroplated nickel silver (EPNS) which is more durable.

Britannium is used to make the Oscar statuettes handed out each year at the Academy Awards. The 8 12-pound statuettes are Britannia metal plated with gold.[6]

In his essay, "A Nice Cup of Tea", writer George Orwell asserts that "britanniaware" teapots "produce inferior tea" when compared to chinaware.[7]

See also


41xx steelAL-6XNAlGaAlloy 20鋁鎳鈷合金Alumel鋁合金Aluminium bronzeAluminium-lithium alloy汞齊Argentium sterling silverArsenical bronzeArsenical copper巴氏合金Bell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅BrightrayBritannia silver青铜Bulat steelCalamine brass铸铁CelestriumChinese silverChromelChromium hydride白金 (合金)康銅氢化亚铜Copper–tungstenCorinthian bronzeCrown goldCrucible steelCunife白铜Cymbal alloys大馬士革鋼Devarda's alloyDoré bullion杜拉鋁Dutch metal电工钢琥珀金Elektron (alloy)ElinvarFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstanGilding metal玻璃GlucydurGoloidGuanín (bronze)Gum metalGunmetalHaynes InternationalHepatizonHiduminium高速鋼High-strength low-alloy steelHydronalium英高鎳合金不變鋼Iron–hydrogen alloyItalmaKanthal (alloy)Kovar镁铝合金Magnox (alloy)MangalloyManganin马氏体时效钢Marine grade stainless马氏体不锈钢MegalliumMelchior (alloy)MercuryMischmetalMolybdochalkosMonelΜ合金Muntz metalMushet steelNichromeNickel hydrideNickel silverNickel titaniumNicrosilNisil北歐金Ormolu透磁合金Phosphor bronze生鐵Pinchbeck (alloy)塑料Platinum sterlingPlexiglasPlutonium–gallium alloyPseudo palladiumReynolds 531銠金礦Rose's metal釤鈷磁鐵Sanicro 28Scandium hydrideShakudōShibuichiSilver steel钠钾合金銲料Speculum metalSpiegeleisenSpring steelStaballoy不鏽鋼StelliteSterling silver钢结构超導磁率合金Surgical stainless steelTerfenol-DTerneTibetan silverTitanium alloyTi Beta-C.Titanium gold氢化钛氮化钛TombacTool steelTumbagaType metal維塔立合金耐候钢伍德合金烏茲鋼Y alloyZeron 100PewterQueen's metalWhite metal氢化铀ZamakZirconium hydride甲烷Mezzanine原子珩磨金屬加工材料科学

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material