powered by CADENAS

Social Share

Goloid (8867 views - Material Database)

Goloid is an alloy of silver, gold and copper patented by Dr. William Wheeler Hubbell on May 22, 1877 (U.S. patent #191,146). The patent specifies 1 part gold (about 3.6%), 24 parts silver (about 87.3%), and 2.5 parts copper (about 9.1%, all by weight); however, the patent also states that "The proportions may be slightly varied" and goes on to specify that the silver portion can range from 20 times to 30 times that of the gold, and the copper could range from one-eighth to one-twelfth (from 12.5% to 8.33%) of the total mixture. The patent specifies that the metals be separately melted, then mixed, along with "sulphate of sodium or sulphate of potassium" in the amount of one part sulfate to one thousand parts metal. The alloy, in varying proportions (sometimes slightly out of these specifications), was used by the United States Mint to strike pattern dollars, sometimes called "metric dollars" (some were marked with "metric" in the coin design, while all had metal proportions and total coin weight as design features) from 1878 to 1880. Patterns of the same design were struck in other metals, including aluminum, copper, normal coin silver, lead, and white metal. In the end, goloid was rejected as a coinage metal because it could not be distinguished from the normal U.S. 90% silver coin alloy without chemical analysis, thus inviting counterfeiters to use silver-copper alloys alone to make lower-value copies.
Go to Article

Goloid

Goloid

Goloid

Goloid is an alloy of silver, gold and copper patented by Dr. William Wheeler Hubbell on May 22, 1877 (U.S. patent #191,146). The patent specifies 1 part gold (about 3.6%), 24 parts silver (about 87.3%), and 2.5 parts copper (about 9.1%, all by weight); however, the patent also states that "The proportions may be slightly varied" and goes on to specify that the silver portion can range from 20 times to 30 times that of the gold, and the copper could range from one-eighth to one-twelfth (from 12.5% to 8.33%) of the total mixture. The patent specifies that the metals be separately melted, then mixed, along with "sulphate of sodium or sulphate of potassium" in the amount of one part sulfate to one thousand parts metal. The alloy, in varying proportions (sometimes slightly out of these specifications), was used by the United States Mint to strike pattern dollars, sometimes called "metric dollars" (some were marked with "metric" in the coin design, while all had metal proportions and total coin weight as design features) from 1878 to 1880. Patterns of the same design were struck in other metals, including aluminum, copper, normal coin silver, lead, and white metal.

In the end, goloid was rejected as a coinage metal because it could not be distinguished from the normal U.S. 90% silver coin alloy without chemical analysis, thus inviting counterfeiters to use silver-copper alloys alone to make lower-value copies.


41xx steelAL-6XNAlGaAlloy 20鋁鎳鈷合金Alumel鋁合金Aluminium bronzeAluminium-lithium alloy汞齊Argentium sterling silverArsenical bronzeArsenical copperBell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅BrightrayBritannia silver青铜Bulat steelCalamine brass铸铁CelestriumChinese silverChromelChromium hydride白金 (合金)康銅氢化亚铜Copper–tungstenCorinthian bronzeCrown goldCrucible steelCunife白铜Cymbal alloys大馬士革鋼Devarda's alloyDoré bullion杜拉鋁Dutch metal电工钢琥珀金Elektron (alloy)ElinvarFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstanGilding metal玻璃GlucydurGuanín (bronze)GunmetalHaynes InternationalHepatizonHiduminium高速鋼High-strength low-alloy steelHydronalium英高鎳合金不變鋼Iron–hydrogen alloyItalmaKanthal (alloy)Kovar镁铝合金Magnox (alloy)MangalloyManganin马氏体时效钢Marine grade stainless马氏体不锈钢MegalliumMelchior (alloy)MercuryMischmetalMolybdochalkosMonelΜ合金Muntz metalMushet steelNichromeNickel hydrideNickel silverNickel titaniumNicrosilNisil北歐金Ormolu透磁合金Phosphor bronze生鐵Pinchbeck (alloy)塑料PlexiglasPlutonium–gallium alloyPseudo palladiumReynolds 531銠金礦Rose's metal釤鈷磁鐵Sanicro 28Scandium hydrideShakudōSilver steel钠钾合金銲料Speculum metalSpiegeleisenSpring steelStaballoy不鏽鋼Stellite钢结构超導磁率合金Surgical stainless steelTerfenol-DTerneTombacTool steelTumbagaType metal維塔立合金耐候钢伍德合金烏茲鋼Y alloyZeron 100Platinum sterlingShibuichiSterling silverTibetan silverTi Beta-C.Titanium alloy氢化钛Gum metalTitanium gold氮化钛巴氏合金Britannia metalPewterQueen's metalWhite metal氢化铀ZamakZirconium hydride甲烷Mezzanine原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material