powered by CADENAS

Social Share

Brightray (9070 views - Material Database)

Brightray is a nickel-chromium alloy that is noted for its resistance to erosion by gas flow at high temperatures. It was used for hard-facing the exhaust valve heads and seats of petrol engines, particularly aircraft engines from the 1930s onwards. It was developed by Henry Wiggin and Co at Birmingham. As well as its use as a coating, it is also used in wire and strip form for electrical heating elements. The original Brightray alloy was composed of 80% nickel / 20% chromium. This alloy is still in use today as Brightray S and can be used at temperatures up to 1050°C. Several other variants are now available. These include nickel-iron-chromium Brightray F that offers better resistance to both reducing and oxidizing environments. Brightray C is a nickel-chromium alloy with rare-earth additions to extend its lifetime under fluctuating temperatures, particularly with heating elements that are being continually switched on and off.
Go to Article

Brightray

Brightray

Brightray is a nickel-chromium alloy that is noted for its resistance to erosion by gas flow at high temperatures.[1] It was used for hard-facing the exhaust valve heads and seats of petrol engines, particularly aircraft engines from the 1930s onwards. It was developed by Henry Wiggin and Co at Birmingham.

As well as its use as a coating, it is also used in wire and strip form for electrical heating elements.

The original Brightray alloy was composed of 80% nickel / 20% chromium. This alloy is still in use today as Brightray S[2] and can be used at temperatures up to 1050°C. Several other variants are now available. These include nickel-iron-chromium Brightray F[3] that offers better resistance to both reducing and oxidizing environments. Brightray C[4] is a nickel-chromium alloy with rare-earth additions to extend its lifetime under fluctuating temperatures, particularly with heating elements that are being continually switched on and off.

See also


41xx steelAL-6XNAlGaAlloy 20鋁鎳鈷合金Alumel鋁合金Aluminium bronzeAluminium-lithium alloy汞齊Arsenical bronzeArsenical copperBell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅青铜Bulat steelCalamine brass铸铁CelestriumChinese silverChromium hydride白金 (合金)康銅氢化亚铜Copper–tungstenCorinthian bronzeCrown goldCrucible steelCunife白铜Cymbal alloys大馬士革鋼Devarda's alloy杜拉鋁Dutch metal电工钢琥珀金Elektron (alloy)ElinvarFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstanGilding metal玻璃GlucydurGuanín (bronze)GunmetalHepatizonHiduminium高速鋼High-strength low-alloy steelHydronalium不變鋼Iron–hydrogen alloyItalmaKanthal (alloy)Kovar镁铝合金Magnox (alloy)MangalloyManganin马氏体时效钢Marine grade stainless马氏体不锈钢MegalliumMelchior (alloy)MercuryMolybdochalkosMuntz metalMushet steelNichromeNickel silver北歐金OrmoluPhosphor bronze生鐵Pinchbeck (alloy)塑料PlexiglasReynolds 531銠金礦Rose's metalSanicro 28ShakudōSilver steel銲料Speculum metalSpiegeleisenSpring steelStaballoy不鏽鋼Stellite钢结构Surgical stainless steelTerneTombacTool steelTumbagaType metal維塔立合金耐候钢伍德合金烏茲鋼Y alloyZeron 100ChromelHaynes International英高鎳合金MonelNicrosilNisilNickel titaniumΜ合金透磁合金超導磁率合金Nickel hydridePlutonium–gallium alloy钠钾合金MischmetalTerfenol-DPseudo palladiumScandium hydride釤鈷磁鐵Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTi Beta-C.Titanium alloy氢化钛Gum metalTitanium gold氮化钛巴氏合金Britannia metalPewterQueen's metalWhite metal氢化铀ZamakZirconium hydride甲烷Mezzanine原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material