powered by CADENAS

Social Share

Silver steel (12143 views - Material Database)

Silver steel is common tool steel that is supplied as a centerless ground round bar (with tolerances similar to that of drill rod). The name comes from the highly polished appearance of the rods; there is no silver in the alloy. Amongst other applications, it has been widely used to make such things as punches, engravers, screwdrivers. Sheffield silver steel is used in France as a blade steel for straight razors. In Finland, German silver steel was and still is widely used for Puukko knives. The composition is defined by UK specification BS-1407, and is given below. In the annealed state it has a hardness of 27 HRC. It can be hardened to 64 HRC. The European/Werkstoff equivalent is 1.2210 / 115CrV3, which also includes some vanadium.
Go to Article

Silver steel

Silver steel

Silver steel is common tool steel that is supplied as a centerless ground round bar (with tolerances similar to that of drill rod). The name comes from the highly polished appearance of the rods; there is no silver in the alloy.

Amongst other applications, it has been widely used to make such things as punches, engravers, screwdrivers. Sheffield silver steel is used in France as a blade steel for straight razors. In Finland, German silver steel was and still is widely used for Puukko knives.

The composition is defined by UK specification BS-1407, and is given below.

In the annealed state it has a hardness of 27 HRC. It can be hardened to 64 HRC.[1]

The European/Werkstoff equivalent is 1.2210 / 115CrV3, which also includes some vanadium.

Composition of Silver Steel
Element BS-1407 Silver Steel[2] DIN 1.2210 / 115CrV3[3]
Min Typ Max Min Max
Carbon 0.95% 1.13% 1.25% 1.10% 1.25%
Chromium 0.35% 0.43% 0.45% 0.50% 0.80%
Manganese 0.25% 0.37% 0.45% 0.20% 0.40%
Silicon 0 0.22% 0.40% 0.15% 0.30%
Vanadium 0.07% 0.12%
Phosphorus 0 0.014% 0.045% 0 0.03%
Sulphur 0 0.018% 0.045% 0 0.03%
Iron Balance Balance


  1. ^ Silver Steel, retrieved 28 September 2008 
  2. ^ Silver Steel BS1407, retrieved 28 September 2008 
  3. ^ http://www.ozct.com.tr/en/pdf/1.2210%20115CrV3.pdf

41xx steelAL-6XNAlGaAlloy 20鋁鎳鈷合金鋁合金Aluminium bronzeAluminium-lithium alloyArsenical bronzeArsenical copperBell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅青铜Bulat steelCalamine brass铸铁CelestriumChinese silverChromium hydride白金 (合金)康銅氢化亚铜Copper–tungstenCorinthian bronzeCrown goldCrucible steelCunife白铜Cymbal alloys大馬士革鋼Devarda's alloy杜拉鋁Dutch metal电工钢琥珀金ElinvarFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstanGilding metal玻璃GlucydurGuanín (bronze)GunmetalHepatizonHiduminium高速鋼High-strength low-alloy steelHydronalium不變鋼Iron–hydrogen alloyItalmaKanthal (alloy)Kovar镁铝合金MangalloyManganin马氏体时效钢Marine grade stainless马氏体不锈钢MegalliumMelchior (alloy)MercuryMolybdochalkosMuntz metalMushet steelNichromeNickel silver北歐金OrmoluPhosphor bronze生鐵Pinchbeck (alloy)塑料PlexiglasReynolds 531銠金礦Rose's metalSanicro 28ShakudōSpeculum metalSpiegeleisenSpring steelStaballoy不鏽鋼Stellite钢结构Surgical stainless steelTombacTumbaga維塔立合金伍德合金Y alloyZeron 100Tool steel耐候钢烏茲鋼銲料TerneType metalElektron (alloy)汞齊Magnox (alloy)AlumelBrightrayChromelHaynes International英高鎳合金MonelNicrosilNisilNickel titaniumΜ合金透磁合金超導磁率合金Nickel hydridePlutonium–gallium alloy钠钾合金MischmetalTerfenol-DPseudo palladiumScandium hydride釤鈷磁鐵Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTi Beta-C.Titanium alloy氢化钛Gum metalTitanium gold氮化钛巴氏合金Britannia metalPewterQueen's metalWhite metal氢化铀ZamakZirconium hydride甲烷Mezzanine原子煉鋼廠高爐Ironworks

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material