powered by CADENAS

Social Share

Surgical stainless steel (12201 views - Material Database)

Surgical stainless steel is an informal term which refers to certain grades of stainless steel that are used in biomedical applications. The most common "surgical steels" are austenitic 316 stainless and martensitic 440 and 420 stainless steels. There is no formal definition on what constitutes a "surgical stainless steel", so product manufacturers and distributors apply the term to refer to any grade of corrosion resistant steel. 316 stainless steel, also referred to as marine grade stainless steel, is a chromium, nickel, molybdenum alloy of steel that exhibits relatively good strength and corrosion resistance. Along with the titanium alloy Ti6Al4V, 316 stainless is a common choice of material for biomedical implants. Although Ti6Al4V provides greater strength per weight and corrosion resistance, 316 stainless components can be more economical to produce. However, immune system reaction to nickel is a potential complication of 316. Implants and equipment that are put under pressure (bone fixation screws, prostheses, body piercing jewelry) are made out of austenitic steel, often 316L and 316LVM compliant to ASTM F138,. 316 surgical steel is used in the manufacture and handling of food and pharmaceutical products where it is often required in order to minimize metallic contamination. ASTM F138-compliant steel is also used in the manufacture of body piercing jewellery and body modification implants. 440 and 420 stainless steels, known also by the name "Cutlery Stainless Steel", are high carbon steels alloyed with chromium. They have very good corrosion resistance compared to other cutlery steels, but their corrosion resistance is inferior to 316 stainless. Biomedical cutting instruments are often made from 440 or 420 stainless due to its high hardness coupled with acceptable corrosion resistance. This type of stainless steel may be slightly magnetic.
Go to Article

Surgical stainless steel

Surgical stainless steel

Surgical stainless steel is an informal term which refers to certain grades of stainless steel that are used in biomedical applications. The most common "surgical steels" are austenitic 316 stainless and martensitic 440 and 420 stainless steels. There is no formal definition on what constitutes a "surgical stainless steel", so product manufacturers and distributors apply the term to refer to any grade of corrosion resistant steel.

316 stainless steel, also referred to as marine grade stainless steel, is a chromium, nickel, molybdenum alloy of steel that exhibits relatively good strength and corrosion resistance. Along with the titanium alloy Ti6Al4V, 316 stainless is a common choice of material for biomedical implants. Although Ti6Al4V provides greater strength per weight and corrosion resistance, 316 stainless components can be more economical to produce. However, immune system reaction to nickel is a potential complication of 316.[1][2] Implants and equipment that are put under pressure (bone fixation screws, prostheses, body piercing jewelry) are made out of austenitic steel, often 316L and 316LVM compliant to ASTM F138,.[3] 316 surgical steel is used in the manufacture and handling of food and pharmaceutical products where it is often required in order to minimize metallic contamination. ASTM F138[3]-compliant steel is also used in the manufacture of body piercing jewellery[4] and body modification implants.

440 and 420 stainless steels, known also by the name "Cutlery Stainless Steel", are high carbon steels alloyed with chromium. They have very good corrosion resistance compared to other cutlery steels, but their corrosion resistance is inferior to 316 stainless. Biomedical cutting instruments are often made from 440 or 420 stainless due to its high hardness coupled with acceptable corrosion resistance. This type of stainless steel may be slightly magnetic.

See also


41xx steelAL-6XNAlGaAlloy 20鋁鎳鈷合金鋁合金Aluminium bronzeAluminium-lithium alloyArsenical bronzeArsenical copperBell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅青铜Bulat steelCalamine brass铸铁CelestriumChinese silverChromium hydride白金 (合金)康銅氢化亚铜Copper–tungstenCorinthian bronzeCrown goldCrucible steelCunife白铜Cymbal alloys大馬士革鋼Devarda's alloy杜拉鋁Dutch metal电工钢琥珀金ElinvarFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstanGilding metal玻璃GlucydurGuanín (bronze)GunmetalHepatizonHiduminium高速鋼High-strength low-alloy steelHydronalium不變鋼Iron–hydrogen alloyItalmaKanthal (alloy)Kovar镁铝合金MangalloyManganin马氏体时效钢Marine grade stainless马氏体不锈钢MegalliumMelchior (alloy)MercuryMolybdochalkosMuntz metalMushet steelNichromeNickel silver北歐金OrmoluPhosphor bronze生鐵Pinchbeck (alloy)塑料PlexiglasReynolds 531銠金礦Rose's metalSanicro 28ShakudōSpeculum metalSpiegeleisenSpring steelStaballoy不鏽鋼Stellite钢结构TombacTumbaga維塔立合金伍德合金Y alloyZeron 100Silver steelTool steel耐候钢烏茲鋼銲料TerneType metalElektron (alloy)汞齊Magnox (alloy)AlumelBrightrayChromelHaynes International英高鎳合金MonelNicrosilNisilNickel titaniumΜ合金透磁合金超導磁率合金Nickel hydridePlutonium–gallium alloy钠钾合金MischmetalTerfenol-DPseudo palladiumScandium hydride釤鈷磁鐵Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTi Beta-C.Titanium alloy氢化钛Gum metalTitanium gold氮化钛巴氏合金Britannia metalPewterQueen's metalWhite metal氢化铀ZamakZirconium hydride甲烷Mezzanine原子煉鋼廠Steelmaking铁矿高爐真空腔體

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material