powered by CADENAS

Social Share

马氏体不锈钢 (14291 views - Material Database)

马氏体不锈钢是不锈钢合金中的一种形态。 不锈钢可根据晶体结构分为三种主要形态:奥氏体,肥粒鐵和马氏体。马氏体不锈钢是一种大约根据410型钢(由铁,12%的铬和0.12%的碳组成)制造的低碳不锈钢。它们通常通过回火和硬化形成。回火马氏体使不锈钢变的拥有好的硬度和高韧性,未回火的马氏体韧性低,所以易碎。 马氏体的四方晶系微观结构在约1890年时首先被一位德国显微镜学家阿道夫·马顿斯所观察到。1912年,埃尔伍德·海恩斯申请了一个关于马氏体不锈钢合金的美国专利,这个专利直到1919年才被准许。 不像奥氏体不锈钢,马氏体不锈钢可以通过磁性粒子检查法進行无损检测。 也在1912年,英国谢菲尔德布朗弗思研究工作实验室的哈利·布雷尔利在寻找一种耐蚀的合金用于制造枪筒时,发现一种马氏体不锈钢合金并随后使其工业化。这个发现两年后被公布在1915年一月刊的《纽约时报》。在1915年间布雷尔利申请了一个美国专利。不久之后,它在英国弗思·威格士的“Staybrite”品牌下销售,而且在1929年被用于伦敦萨沃伊饭店的入口华盖。
Go to Article

马氏体不锈钢

马氏体不锈钢

马氏体不锈钢不锈钢合金中的一种形态。

不锈钢可根据晶体结构分为三种主要形态:奥氏体肥粒鐵马氏体。马氏体不锈钢是一种大约根据410型钢(由铁,12%的铬和0.12%的碳组成)制造的低碳不锈钢。它们通常通过回火和硬化形成。回火马氏体使不锈钢变的拥有好的硬度和高韧性,未回火的马氏体韧性低,所以易碎。

马氏体的四方晶系微观结构在约1890年时首先被一位德国显微镜学家阿道夫·马顿斯英语Adolf Martens所观察到。1912年,埃尔伍德·海恩斯英语Elwood Haynes申请了一个关于马氏体不锈钢合金的美国专利,这个专利直到1919年才被准许[1]

不像奥氏体不锈钢英语Austenitic stainless steel,马氏体不锈钢可以通过磁性粒子检查法英语Magnetic particle inspection進行无损检测

也在1912年,英国谢菲尔德布朗弗思英语Brown-Firth研究工作实验室的哈利·布雷尔利英语Harry Brearley在寻找一种耐蚀的合金用于制造枪筒时,发现一种马氏体不锈钢合金并随后使其工业化。这个发现两年后被公布在1915年一月刊的《纽约时报[2]。在1915年间布雷尔利申请了一个美国专利。不久之后,它在英国弗思·威格士英语Firth Vickers的“Staybrite”品牌下销售,而且在1929年被用于伦敦萨沃伊饭店的入口华盖[3]

參考文獻[编辑]

  1. ^ Rodney P. Carlisle. Scientific American Inventions and Discoveries. John Wiley and Sons. 2004: 380. ISBN 978-0-471-24410-3. 
  2. ^ A non-rusting steel. New York Times. 31 January 1915. 
  3. ^ Sheffield Steel, ISBN 0-7509-2856-5

41xx steelAL-6XNAlGaAlloy 20鋁鎳鈷合金鋁合金Aluminium bronzeAluminium-lithium alloyArsenical bronzeArsenical copperBell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅青铜Bulat steelCalamine brass铸铁CelestriumChinese silverChromium hydride白金 (合金)康銅氢化亚铜Copper–tungstenCorinthian bronzeCrown goldCrucible steelCunife白铜Cymbal alloys大馬士革鋼Devarda's alloy杜拉鋁Dutch metal电工钢琥珀金ElinvarFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstanGilding metal玻璃GlucydurGuanín (bronze)GunmetalHepatizonHiduminium高速鋼High-strength low-alloy steelHydronalium不變鋼Iron–hydrogen alloyItalmaKanthal (alloy)Kovar镁铝合金MangalloyManganin马氏体时效钢Marine grade stainlessMegalliumMelchior (alloy)MercuryMolybdochalkosMuntz metalMushet steelNichromeNickel silver北歐金OrmoluPhosphor bronze生鐵Pinchbeck (alloy)塑料PlexiglasReynolds 531銠金礦Rose's metalShakudōSpeculum metalSpiegeleisenSpring steelStaballoy不鏽鋼Stellite钢结构TombacTumbaga維塔立合金伍德合金Y alloySanicro 28Surgical stainless steelZeron 100Silver steelTool steel耐候钢烏茲鋼銲料TerneType metalElektron (alloy)汞齊Magnox (alloy)AlumelBrightrayChromelHaynes International英高鎳合金MonelNicrosilNisilNickel titaniumΜ合金透磁合金超導磁率合金Nickel hydridePlutonium–gallium alloy钠钾合金MischmetalTerfenol-DPseudo palladiumScandium hydride釤鈷磁鐵Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTi Beta-C.Titanium alloy氢化钛Gum metalTitanium gold氮化钛巴氏合金Britannia metalPewterQueen's metalWhite metal氢化铀ZamakZirconium hydride甲烷Mezzanine原子

This article uses material from the Wikipedia article "马氏体不锈钢", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material