powered by CADENAS

Social Share

Staballoy (9131 views - Material Database)

Staballoy is the name of two different classes of metal alloys, one class typically used for munitions and a different class developed for drilling rods.
Go to Article

Staballoy

Staballoy

Staballoy

Staballoy is the name of two different classes of metal alloys, one class typically used for munitions and a different class developed for drilling rods.

Kinetic penetrators

In a military context, staballoys are metal alloys of a high proportion of depleted uranium with other metals, usually titanium or molybdenum, designed for use in kinetic energy penetrator armor-piercing munitions. One formulation has a composition of 99.25% of depleted uranium and 0.75% of titanium. Other variants can have 3.5% of titanium. They are about 70% more dense than lead.

An alternative to staballoys in kinetic penetrator munition is tungsten, but it is more expensive, more difficult to machine and is not pyrophoric, so the munition lacks the incendiary effect enhancing its impact. Tungsten penetrators also tend to form a mushroom shaped tip during armor penetration, while uranium ones tend to be self-sharpening.[1]

An emerging alternative alloy of depleted uranium is stakalloy, formed of niobium (0.01-0.95 wt.%), vanadium (1-4.5 wt.%, between gamma-eutectoid and eutectic) and uranium (balance). It has improved machinability. It can be also used in structural applications.[2]

Drilling rods

Staballoy is also a name for a class of commercially used stainless steels used for drilling rods for drilling rigs. An example is Staballoy AG17 which is a different material from military staballoy, and contains 20.00% manganese, 17.00% chromium, 0.30% silicon, 0.03% carbon, 0.50% nitrogen, and 0.05% molybdenum, alloyed with iron. It is nonmagnetic. [1]

  • Trueman E. R.; Black S.; Read D. (2004). "Characterisation of depleted uranium (DU) from an unfired CHARM-3 penetrator". Science of the Total Environment. 327 (1–3): 337–340. PMID 15172592. doi:10.1016/S0048-9697(03)00401-7. 
  • Pollanen R.; Ikaheimonen T. K.; Klemola S.; Vartti V. P.; Vesterbacka K.; Ristonmaa S.; Honkamaa T.; Sipila P.; Jokelainen I.; Kosunen A.; Zilliacus R.; Kettunen M.; Hokkanen M. (2003). "Characterisation of projectiles composed of depleted uranium" (PDF). Review of tungsten-based kinetic energy penetrator materials. 2–3: 133–142. 



AlGa鋁鎳鈷合金鋁合金Aluminium bronzeAluminium-lithium alloyArsenical bronzeArsenical copperBell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅青铜Calamine brass铸铁Chinese silverChromium hydride白金 (合金)康銅氢化亚铜Copper–tungstenCorinthian bronzeCrown goldCunife白铜Cymbal alloysDevarda's alloy杜拉鋁Dutch metal琥珀金ElinvarFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstanGilding metal玻璃GlucydurGuanín (bronze)GunmetalHepatizonHiduminiumHydronalium不變鋼Iron–hydrogen alloyItalmaKanthal (alloy)Kovar镁铝合金ManganinMegalliumMelchior (alloy)MercuryMolybdochalkosMuntz metalNichromeNickel silver北歐金OrmoluPhosphor bronze生鐵Pinchbeck (alloy)塑料Plexiglas銠金礦Rose's metalShakudōSpeculum metal不鏽鋼Stellite钢结构TombacTumbaga維塔立合金伍德合金Y alloyBulat steelCrucible steel41xx steel大馬士革鋼Mangalloy高速鋼Mushet steel马氏体时效钢High-strength low-alloy steelReynolds 531电工钢Spring steelAL-6XNCelestriumAlloy 20Marine grade stainless马氏体不锈钢Sanicro 28Surgical stainless steelZeron 100Silver steelTool steel耐候钢烏茲鋼銲料TerneType metalElektron (alloy)汞齊Magnox (alloy)AlumelBrightrayChromelHaynes International英高鎳合金MonelNicrosilNisilNickel titaniumΜ合金透磁合金超導磁率合金Nickel hydridePlutonium–gallium alloy钠钾合金MischmetalTerfenol-DPseudo palladiumScandium hydride釤鈷磁鐵Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTi Beta-C.Titanium alloy氢化钛Gum metalTitanium gold氮化钛巴氏合金Britannia metalPewterQueen's metalWhite metal氢化铀ZamakZirconium hydride甲烷Mezzanine原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material