Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Ferromanganese, a ferroalloy with high content of manganese, is made by heating a mixture of the oxides MnO2 and Fe2O3, with carbon, usually as coal and coke, in either a blast furnace or an electric arc furnace-type system, called a submerged arc furnace. The oxides undergo carbothermal reduction in the furnaces, producing the ferromanganese. Ferromanganese is used as a deoxidizer for steel.
Henry Bessemer invented the use of ferromanganese as a method of introducing manganese in controlled proportions during the production of steel. The advantage of combining powdered iron oxide and manganese oxide together is the lower melting point of the combined alloy compared to pure manganese oxide.
A North American standard specification is ASTM A99. The ten grades covered under this specification includes;
A similar material is a pig iron with high content of manganese, is called spiegeleisen.
This section needs expansion. You can help by adding to it. (April 2014) |
In 1872 Lambert von Pantz produced ferromanganese in a blast furnace, with significantly higher manganese content than was previously possible (37% instead of the previous 12%). This won his company international recognition, including a gold medal at the 1873 World Exposition in Vienna and a certificate of award at the Centennial Exposition in Pennsylvania in 1876.[1][2]
This alloy-related article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
database,rohs,reach,compliancy,directory,listing,information,substance,material