Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Ferroalloy refers to various alloys of iron with a high proportion of one or more other elements such as manganese, aluminium, or silicon.[1] They are used in the production of steels and alloys.[2][3] The alloys impart distinctive qualities to steel and cast iron or serve important functions during production and are, therefore, closely associated with the iron and steel industry, the leading consumer of ferroalloys. The leading ferroalloy-producing countries in 2008 were Ukraine, China, South Africa and Russia, which accounted for 77% of the world production. World production of bulk chromium, manganese and silicon ferroalloys was estimated as 29.1 million tonnes (Mt) in 2008, a 3% decrease compared with 2007.[2]
The main ferroalloys are:
Ferroalloys are produced generally by two methods : in a blast furnace or in an electric arc furnace. Blast furnace production continuously decreased during the 20th century, whereas the electric arc production is still increasing. Today, feromanganese can be still efficiently produced in a blast furnace, but, even in this case, electric arc furnace are spreading. More commonly, ferroalloys are produced by carbothermic reactions, involving reduction of oxides with carbon (as coke) in the presence of iron. Some ferroalloys are produced by the addition of elements into molten iron.
It is also possible to produce somme ferroalloys by direct reduction[fr] processes. For example, the Krupp-Renn process[fr] is used in Japan to produce ferronickel.[4]
The leading world chromite ore-producing countries in 2008 were India (almost 4 Mt), Kazakhstan (more than 3 Mt), and South Africa (almost 10 Mt). More than 94% of chromite ore production was smelted in electric-arc furnaces to produce ferrochromium for the metallurgical industry. The leading world ferrochromium-producing countries in 2008 were China (more than 1 Mt), Kazakhstan (more than 1 Mt), and South Africa (more than 3 Mt). India and Russia each produced in excess of 0.5 Mt of ferrochromium. Most of the 7.84 Mt of ferrochromium produced worldwide was consumed in the manufacture of stainless steel which exceeded 26 Mt in 2008.[2] Production for this is very economical.
Two manganese ferroalloys, ferromanganese and silicomanganese, are key ingredients for steelmaking. China is the leading world producer of manganese ferroalloys (2.7 Mt), with output about much greater than that of the next three major producers—Brazil (0.34 Mt), South Africa (0.61 Mt) and Ukraine (0.38 Mt)—combined.[2]
Major producers of ferromolybdenum are Chile (16,918 t), China (40,000 t) and the United States which accounted for about 78% of world production of molybdenite ore in 2008, whereas Canada, Mexico and Peru accounted for the remainder. Molybdenite concentrates are roasted to form molybdic oxide, which can be converted into ferromolybdenum, molybdenum chemicals, or molybdenum metal. Although the United States was the second leading molybdenum-producing country in the world in 2008, it imported more than 70% of its ferromolybdenum requirements in 2008, mostly for the steel industry (83% of ferromolybdenum consumed).[2]
In 2008, the major ferronickel-producing countries were Japan (301,000 t), New Caledonia (144,000 t) and Colombia (105,000 t). Together, these three countries accounted for about 51% of world production if China is excluded. Ukraine, Indonesia, Greece, and Macedonia, in descending order of gross weight output, all produced between 68,000 t and 90,000 t of ferronickel, accounting for an additional 31%, excluding China. China was excluded from statistics because its industry produced large tonnages of nickel pig iron in addition to a spectrum of conventional ferronickel grades, for an estimated combined output of 590,000 t gross weight. The nickel content of individual Chinese products varied from about 1.6% to as much as 80%, depending upon customer end use.[2]
In the United States, the steel industry accounted for virtually all the ferronickel consumed in 2008, with more than 98% used in stainless and heat-resistant steels; no ferronickel was produced in the US in 2008.[2]
The nickel pig iron is a low grade ferronickel made in China, which is very popular since the 2010s.
Silicon ferroalloy consumption is driven by cast iron and steel production, where silicon alloys are used as deoxidizers. Some silicon metal was also used as an alloying agent with iron. On the basis of silicon content, net production of ferrosilicon and miscellaneous silicon alloys in the US was 148,000 t in 2008. China is the major supplier, which in 2008 produced more ferrosilicon (4.9 Mt) than the rest of the world combined. Other major manufacturers are Norway (0.21 Mt), Russia (0.85 Mt) and US (0.23 Mt).[2]
Titanium is used in steelmaking for deoxidation, grain-size control, and carbon and nitrogen control and stabilization. During steelmaking, titanium is usually introduced as ferrotitanium because of its relatively low melting temperature and high density. Steels with relatively high titanium content include interstitial-free, stainless and high-strength low-alloy steels. Ferrotitanium is usually produced by induction melting of titanium scrap with iron or steel; however, it also is produced directly from titanium mineral concentrates. The standard grades of ferrotitanium are 30% and 70% titanium. Ferrosilicon-titanium also is produced to allow the simultaneous addition of silicon and titanium. The leading ferrotitanium producing countries include Brazil, China, India, Japan, Russia, Ukraine, United Kingdom and the United States.[2]
Tungsten is an important alloying element in high-speed and other tool steels, and is used to a lesser extent in some stainless and structural steels. Tungsten is often added to steel melts as ferrotungsten, which can contain up to 80% tungsten. World ferrotungsten production is dominated by China, which in 2008 exported 4,835 t (gross weight) of the alloy. Ferrotungsten is relatively expensive, with the prices around $31–44 per kilogram of contained tungsten.[2]
In 2008, China, Russia (12,000 t) and South Africa (17,000 t) accounted for 98% of world vanadium mine production. In these three countries, vanadium was primarily recovered from titanium-bearing magnetite ore processed to produce pig iron. The process entails aluminothermic reduction of vanadium(V) oxide, aluminium (as oxide getter), and scrap iron.[1] This produces a slag containing 20% to 24% vanadium pentoxide, which can be further processed to ferrovanadium containing 40% to 50% vanadium. Of the 5,090 t of vanadium consumed in the United States in 2008, 84% came from ferrovanadium and nearly all of it (99%) went into steel manufacturing.[2]
This article incorporates public domain material from the United States Geological Survey document: "Ferroalloys" (PDF).
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
database,rohs,reach,compliancy,directory,listing,information,substance,material