powered by CADENAS

Social Share

Galfenol (8744 views - Material Database)

In materials science, galfenol is the general term for an alloy of iron and gallium. The name was first given to iron-gallium alloys by United States Navy researchers in 1998 when they discovered that adding gallium to iron could amplify iron's magnetostrictive effect up to tenfold. Galfenol is of interest to sonar researchers because magnetostrictor materials are used to detect sound, and amplifying the magnetostrictive effect could lead to better sensitivity of sonar detectors. Galfenol is also proposed for vibrational energy harvesting, actuators for precision machine tools, active anti-vibration systems, and anti-clogging devices for sifting screens and spray nozzles. Galfenol is machinable and can be produced in sheet and wire form. In 2009, scientists from Virginia Polytechnic Institute and State University, and National Institute of Standards and Technology (NIST) used neutron beams to determine the structure of galfenol. They determined that the addition of gallium changes the lattice structure of the iron atoms from regular cubic cells to one in which the faces of some of the cells become slightly rectangular. The elongated cells tend to clump together in the alloy, forming localized clumps within the material. These clumps have been described by Peter Gehring of the NIST Center for Neutron Research as "something like raisins within a cake".
Go to Article

Galfenol

Galfenol

In materials science, galfenol is the general term for an alloy of iron and gallium. The name was first given to iron-gallium alloys by United States Navy researchers in 1998 when they discovered that adding gallium to iron could amplify iron's magnetostrictive effect up to tenfold. Galfenol is of interest to sonar researchers because magnetostrictor materials are used to detect sound, and amplifying the magnetostrictive effect could lead to better sensitivity of sonar detectors.[1] Galfenol is also proposed for vibrational energy harvesting, actuators for precision machine tools, active anti-vibration systems, and anti-clogging devices for sifting screens and spray nozzles. Galfenol is machinable and can be produced in sheet and wire form.[2][3]

In 2009, scientists from Virginia Polytechnic Institute and State University, and National Institute of Standards and Technology (NIST) used neutron beams to determine the structure of galfenol. They determined that the addition of gallium changes the lattice structure of the iron atoms from regular cubic cells to one in which the faces of some of the cells become slightly rectangular. The elongated cells tend to clump together in the alloy, forming localized clumps within the material. These clumps have been described by Peter Gehring of the NIST Center for Neutron Research as "something like raisins within a cake".[1]

See also


AlGa鋁鎳鈷合金鋁合金Aluminium bronzeAluminium-lithium alloyArsenical bronzeArsenical copperBell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅青铜Calamine brassChinese silverChromium hydride康銅氢化亚铜Copper–tungstenCorinthian bronzeCunife白铜Cymbal alloysDevarda's alloy杜拉鋁Dutch metal琥珀金Florentine bronzeGilding metal玻璃GlucydurGuanín (bronze)GunmetalHepatizonHiduminiumHydronaliumItalma镁铝合金ManganinMegalliumMelchior (alloy)MercuryMolybdochalkosMuntz metalNichromeNickel silver北歐金OrmoluPhosphor bronzePinchbeck (alloy)塑料PlexiglasRose's metalShakudōSpeculum metal不鏽鋼Stellite钢结构TombacTumbaga維塔立合金伍德合金Y alloyGalinstan白金 (合金)銠金礦Crown goldElinvarField's metalFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouranium不變鋼铸铁Iron–hydrogen alloy生鐵Kanthal (alloy)KovarStaballoySpiegeleisenBulat steelCrucible steel41xx steel大馬士革鋼Mangalloy高速鋼Mushet steel马氏体时效钢High-strength low-alloy steelReynolds 531电工钢Spring steelAL-6XNCelestriumAlloy 20Marine grade stainless马氏体不锈钢Sanicro 28Surgical stainless steelZeron 100Silver steelTool steel耐候钢烏茲鋼銲料TerneType metalElektron (alloy)汞齊Magnox (alloy)AlumelBrightrayChromelHaynes International英高鎳合金MonelNicrosilNisilNickel titaniumΜ合金透磁合金超導磁率合金Nickel hydridePlutonium–gallium alloy钠钾合金MischmetalTerfenol-DPseudo palladiumScandium hydride釤鈷磁鐵Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTi Beta-C.Titanium alloy氢化钛Gum metalTitanium gold氮化钛巴氏合金Britannia metalPewterQueen's metalWhite metal氢化铀ZamakZirconium hydride甲烷Mezzanine原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material