Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Hepatizon (Greek etymology: ἧπαρ, English translation: "liver"), also known as Black Corinthian Bronze, was a highly valuable metal alloy in classical antiquity. It is thought to be an alloy of copper with the addition of a small proportion of gold and silver (perhaps as little as 8% of each), mixed and treated to produce a material with a dark purplish patina, similar to the colour of liver. It is referred to in various ancient texts, but few known examples of hepatizon exist today.
Of the known types of bronze or brass in classical antiquity (known in Latin as aes and in Greek as χαλκός), hepatizon was the second most valuable. Pliny the Elder mentions it in his Natural History, stating that it is less valuable than Corinthian bronze, which contained a greater proportion of gold or silver and as a result resembled the precious metals, but was esteemed before bronze from Delos and Aegina.[1][2] As a result of its dark colour, it was particularly valued for statues.[3] According to Pliny, the method of making it, like that for Corinthian bronze, had been lost for a long time.
Similar alloys are found outside Europe. For example, shakudō is a Japanese billon of gold and copper with a characteristic dark blue-purple patina.
The same term is part of the binomial species names of various living things:
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
database,rohs,reach,compliancy,directory,listing,information,substance,material