powered by CADENAS

Social Share

Ormolu (9743 views - Material Database)

Ormolu (from French or moulu, signifying ground or pounded gold) is an English term, used since the 18th century for the gilding technique of applying finely ground, high-carat gold–mercury amalgam to an object of bronze, and for objects finished in this way. The mercury is driven off in a kiln leaving behind a gold coating. The French refer to this technique as bronze doré; in English, it is known as "gilt bronze".
Go to Article

Ormolu

Ormolu

Ormolu

Ormolu /ˈɔːrməl/ (from French or moulu, signifying ground or pounded gold) is an English term, used since the 18th century for the gilding technique of applying finely ground, high-carat goldmercury amalgam to an object of bronze, and for objects finished in this way.

The mercury is driven off in a kiln leaving behind a gold coating. The French refer to this technique as bronze doré; in English, it is known as "gilt bronze".

Process

The manufacture of true ormolu employs a process known as mercury-gilding or fire-gilding, in which a solution of mercuric nitrate is applied to a piece of copper, brass, or bronze; followed by the application of an amalgam of gold and mercury. The item is then exposed to extreme heat until the mercury vaporises and the gold remains, adhering to the metal object.

This process has generally been supplanted by the electroplating of gold over a nickel substrate, which is more economical and less dangerous.

Health risk

Due to exposure to the harmful mercury fumes, most gilders did not survive beyond 40 years of age. In literature there is a reference from John Webster:

Hang him; a gilder that hath his brains perished with quicksilver is not more cold in the liver

After around 1830 the legislation in France had outlawed the use of mercury, although it continued to be commonly employed until circa 1900 and even was still in use around 1960 in very few workshops. To replace ormolu, other gilding techniques (like electroplating from the mid-19th century on) were utilized instead, but nothing surpasses the original mercury-firing method for durability, sheer beauty and richness of colour.[2] Electroplating is the most common modern technique. Ormolu techniques are essentially the same as those used on silver, to produce silver-gilt (also known as vermeil).

Alternatives

A later substitute of a mixture of metals resembling ormolu was developed in France and called pomponne, though, confusingly, the mix of copper and zinc, sometimes with an addition of tin, is technically a type of brass. From the 19th century the term has been popularized to refer to gilt metal or imitation gold.[3]

Gilt-bronze is found from antiquity onwards across Eurasia, but especially in Chinese art, where it was always more common than silver-gilt, the opposite of Europe.

Applications

Craftsmen principally used ormolu for the decorative mountings of furniture, clocks, lighting devices, and porcelain. The great French furniture designers and cabinetmakers, or ébénistes, of the 18th and 19th centuries made maximum use of the exquisite gilt-bronze mounts produced by fondeurs-ciseleurs ("founders and finishers") such as the renowned Jacques Caffieri (1678–1755), whose finished gilt-bronze pieces were almost as fine as jeweler's work. Ormolu mountings attained their highest artistic and technical development in France.[citation needed]

Similarly fine results could be achieved for lighting devices, such as chandeliers and candelabra, as well as for the ornamental metal mounts applied to clock cases and even to ceramic pieces. In the hands of the Parisian marchands-merciers, the precursors of decorators, ormolu or gilt-bronze sculptures could be used for bright, non-oxidizing fireplace accessories or for Rococo or Neoclassical mantel-clocks or wall-mounted clock-cases – a specialty of Charles Cressent (1685–1768) – complemented by rock-crystal drops on gilt-bronze chandeliers and wall-lights.

The bronze mounts were cast by lost wax casting, and then chiseled and chased to add detail. Rococo gilt bronze tends to be finely cast, lightly chiseled, and part-burnished. Neoclassical gilt-bronze is often entirely chiseled and chased with extraordinary skill and delicacy to create finely varied surfaces.

The ormolu technique was extensively used in the French Empire mantel clocks, reaching its peak during this period.[4]

Chinese and European porcelains mounted in gilt-bronze were luxury wares that heightened the impact of often-costly and ornamental ceramic pieces sometimes used for display. Chinese ceramics with gilt-bronze mounts were produced under the guidance of the Parisian marchands-merciers, for only they had access to the ceramics (often purchased in the Netherlands) and the ability to overleap the guild restrictions.[citation needed] A few surviving pieces of 16th-century Chinese porcelain subsequently mounted in contemporary European silver-gilt, or vermeil, show where the foundations of the later fashion lay.

From the late 1760s, Matthew Boulton (1728–1809) of Birmingham produced English ormolu vases and perfume-burners in the latest Neoclassical style. Though the venture never became a financial success, it produced the finest English ormolu. In the early 19th century fine English ormolu came from the workshops of Benjamin Lewis Vulliamy (1780–1854).

In France, the tradition of neoclassic ormolu to Pierre-Philippe Thomire (1751–1843) was continued by Lucien-François Feuchère. Beurdeley & Cie. produced excellent ormolu in rococo and neoclassical styles in Paris, and rococo gilt-bronze is characteristic of the furniture of François Linke.

See also


鋁鎳鈷合金鋁合金Aluminium bronzeAluminium-lithium alloyArsenical bronzeArsenical copperBell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅青铜Calamine brassChinese silverChromium hydride杜拉鋁Dutch metalFlorentine bronzeGilding metal玻璃GlucydurGuanín (bronze)GunmetalHiduminiumHydronaliumItalma镁铝合金MegalliumMercuryMuntz metalNichromePhosphor bronzePinchbeck (alloy)塑料PlexiglasRose's metal不鏽鋼Stellite钢结构Tombac維塔立合金伍德合金Y alloySpeculum metal康銅氢化亚铜Copper–tungstenCorinthian bronzeCunife白铜Cymbal alloysDevarda's alloy琥珀金HepatizonManganinMelchior (alloy)Nickel silverMolybdochalkos北歐金ShakudōTumbagaAlGaGalfenolGalinstan白金 (合金)銠金礦Crown goldElinvarField's metalFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouranium不變鋼铸铁Iron–hydrogen alloy生鐵Kanthal (alloy)KovarStaballoyBulat steelCrucible steel41xx steel大馬士革鋼Mangalloy高速鋼Mushet steel马氏体时效钢High-strength low-alloy steelReynolds 531电工钢Spring steelAL-6XNCelestriumAlloy 20Marine grade stainless马氏体不锈钢Sanicro 28Surgical stainless steelZeron 100Silver steelTool steel耐候钢烏茲鋼銲料TerneType metalElektron (alloy)汞齊Magnox (alloy)AlumelBrightrayChromelHaynes International英高鎳合金MonelNicrosilNisilNickel titaniumΜ合金透磁合金超導磁率合金Nickel hydridePlutonium–gallium alloy钠钾合金MischmetalTerfenol-DPseudo palladiumScandium hydride釤鈷磁鐵Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTi Beta-C.Titanium alloy氢化钛Gum metalTitanium gold氮化钛巴氏合金Britannia metalPewterQueen's metalWhite metal氢化铀ZamakZirconium hydride甲烷Mezzanine原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material