powered by CADENAS

Social Share

Gunmetal (15972 views - Material Database)

Gunmetal, also known as red brass in the United States, is a type of bronze – an alloy of copper, tin, and zinc. Proportions vary by source, but 88% copper, 8–10% tin, and 2–4% zinc is an approximation. Originally used chiefly for making guns, it was eventually superseded in this department by steel. Gunmetal, which casts and machines well and is resistant to corrosion from steam and salt water, is used to make steam and hydraulic castings, valves, gears, statues, and various small objects, such as buttons. It has a tensile strength of 221 to 310 MPa, a specific gravity of 8.7, a Brinell hardness of 65 to 74, and a melting point of around 1,000 degrees Celsius.
Go to Article

Gunmetal

Gunmetal

Gunmetal

Licensed under Creative Commons Attribution-Share Alike 2.5 (de:Benutzer:Hans Chr. R. (Dr. Hans Chr. Riedelbauch)).

Gunmetal, also known as red brass in the United States, is a type of bronze – an alloy of copper, tin, and zinc. Proportions vary by source,[1][2] but 88% copper, 8–10% tin, and 2–4% zinc is an approximation. Originally used chiefly for making guns, it was eventually superseded in this department by steel. Gunmetal, which casts and machines well and is resistant to corrosion from steam and salt water,[3] is used to make steam and hydraulic castings, valves, gears, statues, and various small objects, such as buttons. It has a tensile strength of 221 to 310 MPa, a specific gravity of 8.7, a Brinell hardness of 65 to 74, and a melting point of around 1,000 degrees Celsius.

Variants

  • Gunmetal ingot is a related alloy where the zinc is replaced by 2% lead; this makes the alloy easier to cast but it has less strength.[4]
  • Modified gunmetal contains lead in addition to the zinc; it is typically composed of 86% copper, 9.5% tin, 2.5% lead, and 2% zinc. It is used for gears and bearings.[4]
  • U.S. Government bronze specification G C90500 is composed of 88% copper, 10% tin, and 2% zinc.
  • G bronze (or Copper Alloy No. C90300) contains 88% copper, 8% tin, and 4% zinc.[4][5]
  • U.S. Government bronze specification H is composed of 83% copper, 14% tin, 3% zinc, and 0.8% phosphorus.[citation needed]
  • Red brass is used to produce pipes, valves, and plumbing fixtures and is considered to offer a good mixture of corrosion resistance, strength and ease of casting.[6] It typically contains 85% copper, 5% tin, 5% lead, and 5% zinc.
  • Copper Alloy C23000, which is also known as red brass, contains 84–86% copper, 0.05% each iron and lead, with the balance being zinc.[7]

Gunmetal can also mean steel treated to simulate gunmetal bronze.[2] Bushings made of this metal are used in machinery.

Other uses

The Victoria Cross, Britain's highest award for military valour, is traditionally made using gunmetal from a cannon captured at the Siege of Sevastopol during the Crimean War.

The British Gwalior Star medal, awarded to the British participants in the 1843 campaign against the Scindias, is made from guns captured at the Battles of Maharajpur and Punniar, during the Gwalior Campaign.

Gun money, Irish late 17th-century emergency coins, contain gunmetal, as worn and scrapped guns were used to make them; but also many other metals, in particular brass and bronze, as people donated pots and pans and other metal objects.

Colour

Gunmetal
 
    Color coordinates
Hex triplet #536267
sRGBB  (rgb) (83, 98, 103)
CMYKH   (c, m, y, k) (19, 5, 0, 60)
Source [Unsourced]
B: Normalized to [0–255] (byte)
H: Normalized to [0–100] (hundred)

Gunmetal as a colour is entirely different to the reddish alloy of the same name described above. It is a shade of grey that has a bluish purplish tinge.[8]

  1. ^ "Gunmetal". Retrieved 2008-04-09. 
  2. ^ a b "Gunmetal". Retrieved 2008-04-09. 
  3. ^ "Gunmetal". Retrieved 2008-04-09. 
  4. ^ a b c Brady, George Stuart; Henry R. Clauser; John A. Vaccari (2002). Materials Handbook. McGraw-Hill Professional. pp. 468–469. ISBN 0-07-136076-X. 
  5. ^ "C90300 Bronze Navy G - CDA 903". Anchor Bronze & Metals, Inc. 
  6. ^ Ammen, C.W. (2000). Metalcasting. McGraw-Hill Professional. p. 133. ISBN 0-07-134246-X. 
  7. ^ "C23000 Copper Alloys [Red Brass, C230] Material Property Data Sheet". Metal Suppliers Online. 
  8. ^ "Definition: Gunmetal". Dictionary.com. Retrieved 8 August 2017. 

鋁鎳鈷合金鋁合金Aluminium bronzeAluminium-lithium alloyArsenical bronzeArsenical copperBell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅青铜Calamine brassChinese silverChromium hydride杜拉鋁Dutch metalFlorentine bronzeGilding metal玻璃GlucydurGuanín (bronze)HiduminiumHydronaliumItalma镁铝合金MegalliumMercuryMuntz metalNichromePinchbeck (alloy)塑料PlexiglasRose's metal不鏽鋼Stellite钢结构Tombac維塔立合金伍德合金Y alloyPhosphor bronzeOrmoluSpeculum metal康銅氢化亚铜Copper–tungstenCorinthian bronzeCunife白铜Cymbal alloysDevarda's alloy琥珀金HepatizonManganinMelchior (alloy)Nickel silverMolybdochalkos北歐金ShakudōTumbagaAlGaGalfenolGalinstan白金 (合金)銠金礦Crown goldElinvarField's metalFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouranium不變鋼铸铁Iron–hydrogen alloy生鐵Kanthal (alloy)KovarStaballoySpiegeleisenBulat steelCrucible steel41xx steel大馬士革鋼Mangalloy高速鋼Mushet steel马氏体时效钢High-strength low-alloy steelReynolds 531电工钢Spring steelAL-6XNCelestriumAlloy 20Marine grade stainless马氏体不锈钢Sanicro 28Surgical stainless steelZeron 100Silver steelTool steel耐候钢烏茲鋼銲料TerneType metalElektron (alloy)汞齊Magnox (alloy)AlumelBrightrayChromelHaynes International英高鎳合金MonelNicrosilNisilNickel titaniumΜ合金透磁合金超導磁率合金Nickel hydridePlutonium–gallium alloy钠钾合金MischmetalTerfenol-DPseudo palladiumScandium hydride釤鈷磁鐵Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTi Beta-C.Titanium alloy氢化钛Gum metalTitanium gold氮化钛巴氏合金Britannia metalPewterQueen's metalWhite metal氢化铀ZamakZirconium hydride甲烷大砲Mezzanine原子加农炮材料科学

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material