powered by CADENAS

Social Share

Glucydur (10397 views - Material Database)

Glucydur is the trade name of a metal alloy with a low coefficient of thermal expansion, used for making balance wheels and other parts of mechanical watches. Glucydur is a beryllium bronze; an alloy of beryllium, copper and iron. In addition to its low coefficient of thermal expansion, its hardness (400 Brinell), nonmagnetizability, and resistance to deformation and damage make it suited for making precision parts that must have high dimensional stability. Glucydur is also resistant to corrosion; it is rather inert chemically. Glucydur was developed about the same time as another non-magnetic material, Nivarox.
Go to Article

Glucydur

Glucydur

Glucydur is the trade name of a metal alloy with a low coefficient of thermal expansion, used for making balance wheels and other parts of mechanical watches.

Glucydur is a beryllium bronze; an alloy of beryllium, copper and iron. In addition to its low coefficient of thermal expansion, its hardness (400 Brinell), nonmagnetizability, and resistance to deformation and damage make it suited for making precision parts that must have high dimensional stability. Glucydur is also resistant to corrosion; it is rather inert chemically.

Glucydur was developed about the same time as another non-magnetic material, Nivarox.


鋁鎳鈷合金鋁合金Aluminium bronzeAluminium-lithium alloyArsenical bronzeArsenical copperBell metalBeryllium copperBillon (alloy)BirmabrightBismanol黃銅青铜Calamine brassChinese silverChromium hydride杜拉鋁Dutch metalFlorentine bronzeGilding metal玻璃HiduminiumHydronaliumItalma镁铝合金MegalliumMercuryMuntz metalNichromePinchbeck (alloy)塑料PlexiglasRose's metal不鏽鋼Stellite钢结构Tombac維塔立合金伍德合金Y alloyGuanín (bronze)GunmetalPhosphor bronzeOrmoluSpeculum metal康銅氢化亚铜Copper–tungstenCorinthian bronzeCunife白铜Cymbal alloysDevarda's alloy琥珀金HepatizonManganinMelchior (alloy)Nickel silverMolybdochalkos北歐金ShakudōTumbagaAlGaGalfenolGalinstan白金 (合金)銠金礦Crown goldElinvarField's metalFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouranium不變鋼铸铁Iron–hydrogen alloy生鐵Kanthal (alloy)KovarStaballoySpiegeleisenBulat steelCrucible steel41xx steel大馬士革鋼Mangalloy高速鋼Mushet steel马氏体时效钢High-strength low-alloy steelReynolds 531电工钢Spring steelAL-6XNCelestriumAlloy 20Marine grade stainless马氏体不锈钢Sanicro 28Surgical stainless steelZeron 100Silver steelTool steel耐候钢烏茲鋼銲料TerneType metalElektron (alloy)汞齊Magnox (alloy)AlumelBrightrayChromelHaynes International英高鎳合金MonelNicrosilNisilNickel titaniumΜ合金透磁合金超導磁率合金Nickel hydridePlutonium–gallium alloy钠钾合金MischmetalTerfenol-DPseudo palladiumScandium hydride釤鈷磁鐵Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTi Beta-C.Titanium alloy氢化钛Gum metalTitanium gold氮化钛巴氏合金Britannia metalPewterQueen's metalWhite metal氢化铀ZamakZirconium hydride甲烷Mezzanine原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material