Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Gilding metal is a copper alloy, a brass, comprising 95% copper and 5% zinc.[1] British Army Dress Regulations define gilding metal as '8 parts copper to 1 of zinc'.[2]
Gilding metal is used for various purposes, including the jackets of bullets, driving bands on some artillery shells,[3] as well as enameled badges and other jewellery. The sheet is widely used for craft metalworking by hammer working.[1] It is also used particularly as a lower-cost training material for silversmiths.
Gilding metal may be annealed by heating to between 800–1,450 °F (427–788 °C).[4] It should be cooled slowly afterwards, to reduce risk of cracking.[5]
This alloy-related article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
database,rohs,reach,compliancy,directory,listing,information,substance,material