powered by CADENAS

Social Share

Baby powder (3790 views - Medical & Health)

Baby powder is an astringent powder used for preventing diaper rash, as a deodorant, and for other cosmetic uses. It may be composed of talcum (in which case it is also called talcum powder) or corn starch (in which case it is also called corn starch). Talcum powder is dangerous if inhaled since it may cause aspiration pneumonia or granuloma. Pediatricians generally prefer cornstarch to talc because it is unlikely to be easily inhaled. Baby powder can also be used as a shampoo, cleaning agent, and freshener. Some studies have found a statistical relationship between talc applied to the perineal area by women and incidence of ovarian cancer. However, there is not a consensus that the two are linked. In 2017, over 1,000 U.S. women sued Johnson & Johnson for covering up the possible cancer risk with its Baby Powder product.
Go to Article

Explanation by Hotspot Model

Baby powder

Baby powder

Baby powder is an astringent powder used for preventing diaper rash, as a deodorant, and for other cosmetic uses. It may be composed of talcum (in which case it is also called talcum powder) or corn starch (in which case it is also called corn starch). Talcum powder is dangerous if inhaled since it may cause aspiration pneumonia or granuloma.[1] Pediatricians generally prefer cornstarch to talc because it is unlikely to be easily inhaled.[citation needed] Baby powder can also be used as a shampoo, cleaning agent, and freshener.[2]

Some studies have found a statistical relationship between talc applied to the perineal area by women and incidence of ovarian cancer. However, there is not a consensus that the two are linked.[3][4] In 2017, over 1,000 U.S. women sued Johnson & Johnson for covering up the possible cancer risk with its Baby Powder product.[5]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Medicine & Health

3D,virus,bacteria,medicine, molecule,atom,chemistry,labor