powered by CADENAS

Social Share

Electric cooker (6537 views - Interior Design)

An electric cooker is an electric powered cooking device for heating and cooking of food. An electric cooker often has four stoves and one or two ovens. There will be knobs to determine the temperature of the ovens and stoves. Unlike gas stoves that are powered by gas, it is powered by electricity. Usually they have four rings on top of the hob. Besides stoves or ranges, common types include hot plates, slow cookers (or crock pots), electric toasters, rice cookers, electric teakettles, and the now obsolete Dub Cookers.
Go to Article

Explanation by Hotspot Model

Electric cooker

Electric cooker

An electric cooker is an electric powered cooking device for heating and cooking of food. An electric cooker often has four stoves and one or two ovens. There will be knobs to determine the temperature of the ovens and stoves. Unlike gas stoves that are powered by gas, it is powered by electricity. Usually they have four rings on top of the hob.

Besides stoves or ranges, common types include hot plates, slow cookers (or crock pots), electric toasters, rice cookers, electric teakettles, and the now obsolete Dub Cookers.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Interior Design

3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art