powered by CADENAS

Social Share

Ducati Diavel (9257 views - Cars & Motorbikes & Trucks & Buse)

The Ducati Diavel is the second cruiser motorcycle from Ducati, after the Indiana of 1986–1990. The 2011 model year Diavel debuted in November 2010 at the EICMA motorcycle show in Milan. The engine is a retuned version of the 1,198.4 cc (73.13 cu in) Testastretta from the 1198 superbike, now called the Testastretta 11° for its 11° valve overlap (reduced from 41°). Styling for the Diavel was developed in-house, although the project began under the leadership of Ducati's previous design chief, Pierre Terblanche, who commissioned Glynn Kerr, freelance designer and design columnist for Motorcycle Consumer News, to produce the initial concept sketches. In the US, most Diavel buyers appear to be existing riders age 50 and over, with more women than usual attracted to the bike, and some Harley-Davidson owners, especially V-Rod riders, trading for the new Ducati power cruiser. For 2017 Ducati released the Ducati Diavel Diesel with a limited production of 666 bikes. The bike is a collaboration of Ducati and Diesel, a premium denim retail and fashion brand. Cycle World commented that it has a appearance of "a Mad Max-inspired retro-futuristic theme...". They also stated that the Diavel is "owner of the quickest 0-60 mph time of any production motorcycle Cycle World has ever tested".
Go to Article

Explanation by Hotspot Model

Ducati Diavel

Ducati Diavel

Ducati Diavel
Manufacturer Ducati
Production 2010–
Class Cruiser
Engine 1,198.4 cc (73.13 cu in) 4-valve desmodromic liquid-cooled 90° L-twin engine[1]
Bore / stroke 106.0 mm × 67.9 mm (4.17 in × 2.67 in)
Compression ratio 11.5:1
Top speed 169 mph (272 km/h) [2]
Power 162 hp (121 kW) @ 9,250 rpm (claimed)[3]
Torque 130.5 N·m (96.3 lbf·ft) @ 8,800 rpm (claimed)[3]
Ignition type Electronic
Transmission 6-speed constant-mesh
Wet, hydraulic multi-plate slipper clutch
Frame type Steel trellis. Cast aluminium rear subframe
Suspension Aluminium single-sided swingarm
Brakes

Front: 2 × 320 mm semi-floating discs, radially mounted 4-piston, Brembo callipers, radial master cylinder
Rear: 265 mm disc, 2-piston calliper
ABS standard

Bosch-Brembo ABS
Tires Front: 120/70 ZR 17
Rear: 240/45 ZR17
Rake, trail 28°
Wheelbase 1,590 mm (63 in)
Seat height 770 mm (30 in)
Weight 516 lb (234 kg) [3] (wet)
Fuel capacity 17 L (3.7 imp gal; 4.5 US gal)

The Ducati Diavel is the second cruiser motorcycle from Ducati,[4] after the Indiana of 1986–1990. The 2011 model year Diavel debuted in November 2010 at the EICMA motorcycle show in Milan.[4]

The engine is a retuned version of the 1,198.4 cc (73.13 cu in) Testastretta from the 1198 superbike,[5] now called the Testastretta 11° for its 11° valve overlap (reduced from 41°).

Styling for the Diavel was developed in-house, although the project began under the leadership of Ducati's previous design chief, Pierre Terblanche, who commissioned Glynn Kerr, freelance designer and design columnist for Motorcycle Consumer News, to produce the initial concept sketches.[6] In the US, most Diavel buyers appear to be existing riders age 50 and over, with more women than usual attracted to the bike, and some Harley-Davidson owners, especially V-Rod riders, trading for the new Ducati power cruiser.[7]

For 2017 Ducati released the Ducati Diavel Diesel with a limited production of 666 bikes. The bike is a collaboration of Ducati and Diesel, a premium denim retail and fashion brand. Cycle World commented that it has a appearance of "a Mad Max-inspired retro-futuristic theme...". They also stated that the Diavel is "owner of the quickest 0-60 mph time of any production motorcycle Cycle World has ever tested".[8]

  1. ^ http://www.ducati.com/bikes/diavel/diavel/tech_spec.do
  2. ^ http://www.motorcyclenews.com/bike-reviews/ducati/diavel/2011/ Motorcycle News Ducati Diavel 2011 review
  3. ^ a b c http://www.ducati.es/motocicletas/diavel/diavel_carbon/tech_spec.do DUCATI Diavel official webpage
  4. ^ a b Hinchliffe, Mark (23 October 2010). "A Ducati kind of cruiser". The Mercury (Hobart). Retrieved 20 November 2010. 
  5. ^ 2011 Ducati Diavel Specifications, motorcycle-usa.com 
  6. ^ Kerr, Glynn (February 2011), "Design; Tricoloré Italiano", Motorcycle Consumer News, Irvine, California: Aviation News Corp, vol. 42 no. 2, pp. 38–39, ISSN 1073-9408 
  7. ^ Siler, Wes (2 December 2010), "Who's buying the Diavel?", Hell for Leather, archived from the original on 25 January 2013, retrieved 7 March 2011 
  8. ^ Canet, Don (May 26, 2017). "2017 Ducati Diavel Diesel - FIRST RIDE REVIEW". Cycle World. Retrieved July 22, 2017. 

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks

Car, Truck,MotorBike, Bicycle, Engine, Racer