powered by CADENAS

Social Share

Ford Cortina (14691 views - Cars & Motorbikes & Trucks & Buse)

The Ford Cortina is a car which was built by Ford of Britain in various guises from 1962 to 1982, and was the United Kingdom's best-selling car of the 1970s. The Cortina was produced in five generations (Mark I through to Mark V, although officially the last one was only the Cortina 80 facelift of the Mk IV) from 1962 until 1982. From 1970 onward, it was almost identical to the German-market Ford Taunus (being built on the same platform) which was originally a different car model. This was part of a Ford attempt to unify its European operations. By 1976, when the revised Taunus was launched, the Cortina was identical. The new Taunus/Cortina used the doors and some panels from the 1970 Taunus. It was replaced in 1982 by the Ford Sierra. In Asia and Australasia, it was replaced by the Mazda 626-based Ford Telstar, though Ford New Zealand did import British-made CKD kits of the Ford Sierra estate for local assembly from 1984. The name was inspired by the name of the Italian ski resort Cortina d'Ampezzo, site of the 1956 Winter Olympics. As a publicity stunt, several Cortinas were driven down the bobsled run at the resort which was called Cortina Auto-Bobbing.
Go to Article

Explanation by Hotspot Model

Ford Cortina

Ford Cortina

Ford Cortina
Ford Cortina Super 2 door saloon ("Mark 1")
Overview
Manufacturer Ford UK
Hyundai
Also called Ford Consul Cortina
Production 1962–1982
Body and chassis
Class Large family car (D)
Layout Front-engine, rear-wheel drive
Related Ford Capri
Chronology
Predecessor Ford Consul Classic
Successor Ford Sierra
Ford Telstar
Hyundai Stellar

The Ford Cortina is a car which was built by Ford of Britain in various guises from 1962 to 1982, and was the United Kingdom's best-selling car of the 1970s.

The Cortina was produced in five generations (Mark I through to Mark V, although officially the last one was only the Cortina 80 facelift of the Mk IV) from 1962 until 1982. From 1970 onward, it was almost identical to the German-market Ford Taunus (being built on the same platform) which was originally a different car model. This was part of a Ford attempt to unify its European operations. By 1976, when the revised Taunus was launched, the Cortina was identical. The new Taunus/Cortina used the doors and some panels from the 1970 Taunus. It was replaced in 1982 by the Ford Sierra. In Asia and Australasia, it was replaced by the Mazda 626-based Ford Telstar, though Ford New Zealand did import British-made CKD kits of the Ford Sierra estate for local assembly from 1984.

The name was inspired by the name of the Italian ski resort Cortina d'Ampezzo, site of the 1956 Winter Olympics. As a publicity stunt, several Cortinas were driven down the bobsled run at the resort which was called Cortina Auto-Bobbing.[1]

Mark I (1962–1966)

Cortina Mark I
1963 Ford Consul Cortina Super 2 door saloon ("Mark 1")
Overview
Production 1962–1966
Assembly Ford Dagenham assembly plant (Dagenham, Essex, England)
Ford Lio Ho
(Zhongli, Taoyuan, Taiwan)
Amsterdam, Netherlands
Broadmeadows, Victoria, Australia[2]
Lower Hutt, New Zealand
Ulsan, South Korea
Singapore, Malaysia[3][4]
Designer Roy Brown Jr.
Body and chassis
Body style 2-door saloon
4-door saloon
5-door estate
Powertrain
Engine 1.2 L Kent I4
1.5 L Kent I4
1.6 L Twin-Cam I4
Transmission 4-speed manual[5]
3-speed automatic
Dimensions
Wheelbase 98 in (2,489 mm)[6]
Length 168.25 in (4,274 mm) (saloon)
168.5 in (4,280 mm) (estate)
Width 62.5 in (1,588 mm)
Height 56.5 in (1,435 mm) (saloon)
57.75 in (1,467 mm) (estate)
Curb weight 1,736 lb (787 kg) (De Luxe)
2,072 lb (940 kg) (Estate)

Using the project name of "Archbishop", management at Ford of Britain in Dagenham created a family-sized car which they could sell in large numbers. The chief designer was Roy Brown Jr., the designer of the Edsel, who had been banished to Dagenham following the failure of that car.[7] The Cortina, aimed at buyers of the Morris Oxford Farina and Vauxhall Victor, was launched on 20 September 1962.[8] The car was designed to be economical, cheap to run and easy and inexpensive to produce in Britain. The front-wheel drive configuration used by Ford of Germany for the new Ford Taunus P4, a similarly sized model, was rejected in favour of traditional rear-wheel drive layout. Originally to be called Ford Consul 225, the car was launched as the Consul Cortina until a modest facelift in 1964, after which it was sold simply as the Cortina.[9]

The Cortina was available with 1200 and (from early 1963[10]) 1500 four-cylinder engines with all synchromesh gearbox, in two-door and four-door saloon, as well as in five-door estate (from March 1963) forms. Standard, Deluxe, Super, and GT trims were offered but not across all body styles. Early Standard models featured a simple body coloured front grille, earning it the nickname 'Ironbar'. Since this version cost almost the same as the better equipped Deluxe it sold poorly and is very rare today. Options included heater and bench seat with column gearchange. Super versions of the estates offered the option of simulated wood side and tailgate trim. In an early example of product placement many examples of the brand new Cortina featured as "Glamcabs" in the comedy film Carry On Cabby.

There were two main variations of the Mark 1. The Mark 1a possessed elliptical front side-lights, whereas the Mark 1b had a re-designed front grille incorporating the more rectangular side-light and indicator units. A notable variant was the Ford Cortina Lotus.

The Cortina was launched a few weeks before the London Motor Show of October 1962 with a 1,198 cc three-bearing engine, which was an enlarged version of the 997 cc engine then fitted in the Ford Anglia.[5] A few months later, in January 1963, the Cortina Super was announced with a five-bearing 1,498 cc engine.[5] Versions of the larger engine found their way into subsequent variations, including the Cortina GT which appeared in spring 1963 with lowered suspension and engine tuned to give a claimed output of 78 bhp (58 kW; 79 PS) ahead of the 60 bhp (45 kW; 61 PS) claimed for the Cortina 1500 Super. The engines used across the Mark I range were of identical design, differing only in capacity and setup. The formula used was a four-cylinder pushrod (over head valve) design that came to be known as the "pre-crossflow" version as both inlet and exhaust ports were located on the same side of the head. The most powerful version of this engine (used in the GT Cortina) was 1,498 cc (1500) and produced 78 bhp (58 kW). This engine contained a different camshaft profile, a different cast of head featuring larger ports, tubular exhaust headers and a Weber double barrel carburettor.

Advertising of the revised version, which appeared at the London Motor Show in October 1964, made much of the newly introduced "Aeroflow" through-flow ventilation, evidenced by the extractor vents on the rear pillars. A subsequent test on a warm day involving the four different Cortina models manufactured between 1964 and 1979 determined that the air delivery from the simple eyeball outlets on the 1964 Mark I Cortina was actually greater than that on the Mark II, the Mark III or the Mark IV.[11] The dashboard, instruments and controls were revised, for the second time, having already been reworked in October 1963 when round instruments replaced the oblong speedometer with which the car had been launched:[5] twelve years later, however, the painted steel dashboard, its "knobs scattered all over the place and its heater controls stuck underneath as a very obvious afterthought" on the 1964 Mark I Cortina was felt to have aged much less well than the car's ventilation system.[11] It was also in 1964 that front disc brakes became standard across the range.[5]

Ford Cortina Lotus was offered only as a two-door saloon all in white with a contrasting green side flash down each flank. It had a unique 1,557 cc twin-cam engine by Lotus, but based on the Cortina's Kent OHV engine. Aluminium was used for some body panels. For a certain time, it also had a unique A-frame rear suspension, but this proved fragile and the model soon reverted to the standard Cortina semi-elliptic rear end.

Mark II (1966–1970)

Cortina Mark II
Ford Cortina GT Mark II 2-door Saloon
Overview
Production 1966–1970
Assembly Ford Dagenham assembly plant (Dagenham, Essex, England, United Kingdom)
Ford Lio Ho (Zhongli City, Taoyuan County (now Zhongli District, Taoyuan City), Taiwan)
Amsterdam, Netherlands
Broadmeadows, Victoria, Australia
Lower Hutt, New Zealand
Ulsan, South Korea
Designer Roy Haynes
Body and chassis
Body style 2-door saloon
4-door saloon
5-door estate
Related Ford Capri Mk 1
Powertrain
Engine
Transmission 4-speed manual
Dimensions
Wheelbase 98 in (2,489 mm)[6]
Length 168 in (4,267 mm) (saloon)
Width 64.9 in (1,648 mm)
Height 55.7 in (1,415 mm)
Curb weight 1,890 lb (857 kg) (De Luxe)
2,032 lb (922 kg) (1600E)

The second incarnation of the Cortina was designed by Roy Haynes, and launched on 18 October 1966,[12] four years after the original Cortina. Although the launch was accompanied by the slogan "New Cortina is more Cortina", the car, at 168 in (427 cm) long, was fractionally shorter than before.[13] Its 2 12 inches (6.4 cm) of extra width and curved side panels provided more interior space.[13] Other improvements included a smaller turning circle, softer suspension, self-adjusting brakes and clutch together with the availability on the smaller-engined models, for the UK and some other markets, of a new five bearing 1,300 cc engine.[14]

A stripped-out 1,200 cc version running the engine of the Ford Anglia Super was also available for certain markets where the 1,300 cc engine attracted a higher rate of tax. The 1,500 cc engines were at first carried over, but were discontinued in July 1967 as a new engine was on its way.[15] A month later, in August, the 1,300 received a new crossflow cylinder head design, making it more efficient, while a crossflow 1,600 replaced the 1,500. The new models carried additional "1300" or "1600" designations at the rear.[15] The Cortina Lotus continued with its own unique engine, although for this generation it was built in-house by Ford themselves.

The Cortina was Britain's most popular new car in 1967,[16] achieving the goal that Ford had been trying to achieve since it set out to create the original Cortina back in 1962. This interrupted the long run of BMC's 1100/1300 range as Britain's best selling car.

Period reviews were favourable concerning both the styling and performance.[17]

Again, two-door and four-door saloons were offered with base, Deluxe, Super, GT and, later, 1600E trims available, but again, not across all body styles and engine options. A few months after the introduction of the saloon versions, a four-door estate was launched, released on the UK market on 15 February 1967:[18] much was made at the time of its class topping load capacity.

The four-door Cortina 1600E, a higher trim version, was introduced at the Paris Motor Show in October 1967,[19] a year after the arrival of the Cortina Mark II. It combined the lowered suspension of the Cortina Lotus with the high-tune GT 1600 Kent engine and luxury trim featuring a burr walnut woodgrain-trimmed dashboard and door cappings, bucket seating, leather-clad aluminium sports steering wheel, and full instrumentation inside, while a black grille, tail panel, front fog lights, and plated Rostyle wheels on radial tyres featured outside.[15] According to author and Cortina expert Graham Robson, the 1600E would be the first Cortina recognized as a classic.[20]

Ford New Zealand developed its own variant of this model called the GTE, since the GT and Lotus Cortinas were not assembled there. The four-door only GTE had a wooden dash, a vinyl roof, and special stripes and badging.[21]

For 1969, the Mark II range was given subtle revisions, with separate "FORD" block letters mounted on the bonnet and boot lids, a blacked out grille and chrome strips on top and below the taillights running the full width of the tail panel marking them out.

A 3.0-litre Essex V6-engined variant was developed privately in South Africa by Basil Green Motors, and was sold through the Grosvenor Ford network of dealers as the Cortina Perana; a similar model appeared later in Britain and was known as the Cortina Savage. Savage was available with 1600E trim in all three body styles, while her South African stablemate was offered only as a four-door saloon initially with GT and later E trim.[22]

TC Mark III (1970–1976)

Cortina TC Mark III
1972 Ford Cortina Mk3 GXL four door.
Overview
Production 1970–1976
Assembly Ford Dagenham assembly plant (Dagenham, Essex, England, United Kingdom)
Ford Lio Ho (Zhongli City, Taoyuan County (now Zhongli District, Taoyuan City), Taiwan)
Amsterdam, Netherlands 1962–1975
Broadmeadows, Victoria, Australia
Lower Hutt, New Zealand
Ulsan, South Korea
Body and chassis
Body style 2-door saloon
4-door saloon
5-door estate
2-door coupé utility (P100)
Related Ford Taunus TC
Powertrain
Engine 1.3 L Crossflow I4
1.6 L Crossflow I4
1.6 L Pinto TL16 I4
2.0 L Pinto TL20 I4
2.0 L Essex V4 (South Africa)
2.5 L Essex V6 (South Africa)
3.0 L Essex V6 (South Africa)
3.3 L Falcon 200 I6
4.1 L Falcon 250 I6
Transmission 3/4-speed manual
3-speed automatic
Dimensions
Wheelbase 101 in (2,565 mm)
Length 167.75 in (4,261 mm) (saloon)
171.5 in (4,356 mm) (estate)
Width 67 in (1,702 mm)
Height 52 in (1,321 mm)

In the late 1960s, Ford set about developing the third-generation Cortina, the Mark III, which would be produced in higher volumes than before, following the recent merger of Ford of Britain and Ford of Germany into the modern-day Ford of Europe. The car marked the convergence of the German Taunus and British Cortina platforms with only minor differences between the two, hence the car's internal name TC1, standing for Taunus-Cortina. It was also the last European car engineered by Harley Copp as Vice President Engineering and head of Brentwood, before he returned to Detroit.

Ford UK originally wanted to call it something other than Cortina, but the name stuck. Although the Mark III looked significantly larger than the boxier Mark II Cortina, it was actually the same overall length, but 4 inches (100 mm) wider.[23] Within the overall length, a wheelbase lengthened by more than 3 inches (76 mm) also contributed to the slightly more spacious interior.[23]

The Mark III Cortina was inspired by the contemporary "coke bottle" design language which had emanated from Detroit – the car sported similar fluted bonnet and beltline design elements to the North American Mercury Montego and Ford LTD of the same era. It replaced both the Mark II Cortina and the larger, more expensive Ford Corsair, offering more trim levels and the option of larger engines than the Mark II Cortina. The Mark III's continental European sister car – the Taunus TC – was subtly different in appearance, with longer front indicators, different door skins and rear wing pressings that toned down the drooping beltline in order to lose the "coke-bottle" appearance of the Cortina.

The MacPherson strut front suspension was replaced with more conventional double A-arm suspension (Also known as double wishbone suspension) which gave the Mark III a much softer ride on the road' but did give cars fitted with the larger, heavier engines distinct understeer.

Trim levels for the Mark III Cortina were Base, L (for Luxury), XL (Xtra Luxury), GT (Grand Touring) and GXL (Grand Xtra Luxury).

The early Mark III Cortinas came with the same 1,300 and 1,600 cc engines as the Mark II Cortinas, except for the 1,600 cc GXL. These engines are known as the Kent, crossflow engine or over head valve (OHV) engine. There was also the introduction of the 2000 cc engine, the single overhead cam engine, now known as the Pinto engine. SOHC. The OHV Kent unit was fitted with a single choke carburetor and was used for the early models up to GT trim, the SOHC twin choke carburetor Pinto unit was used for the GT and GXL models. The GXL was also offered in 1,600 in the later Cortina Mark IIIs.

In left-hand drive markets, the 1,600 cc OHC was replaced by a twin-carb OHV (Kent) unit not offered in the home market, in order to distinguish it from the competing Taunus which only came with the OHC Pinto engine.[24] 2.0-litre variants used a larger version of the 1,600 cc Pinto unit and were available in all trim levels except base. Base, L and XL versions were available as a five-door estate.

Although no longer than its predecessor, the Mark III was a heavier car, reflecting a trend towards improving secondary safety by making car bodies more substantial.[23] Weight was also increased by the stout cross-member incorporated into the new simplified front suspension set-up,[25] and by the inclusion of far more sound deadening material which insulated the cabin from engine and exhaust noise, making the car usefully quieter than its predecessor, though on many cars the benefit was diminished by high levels of wind noise apparently resulting from poor door fit around the windows.[23] Four-speed manual transmissions were by now almost universally offered in the UK for this class of car, and contemporary road tests commented on the rather large gap between second and third gear, and the resulting temptation to slip the clutch when accelerating through the gears in the smaller-engined cars:[23] it was presumably in tacit acknowledgment of the car's marginal power-to-weight ratio that Ford no longer offered the automatic transmission option with the smallest 1,298 cc-engined Cortina.[23]

Four headlights and Rostyle wheels marked out the GT and GXL versions, while the GXL also had bodyside rub strips, a vinyl roof and a brushed aluminum and black boot lid panel on the GXLs, while the GTs had a black painted section of the boot with a chrome trim at either site of it. All pre-facelift models featured a downward sloping dashboard with deeply recessed dials and all coil suspension all round. In general styling and technical make up, many[who?] observed that the Mark III Cortina aped the Vauxhall Victor FD of 1967.

The Cortina went on sale on 23 October 1970,[26] but sales got off to a particularly slow start because of production difficulties that culminated with a ten-week strike at Ford's plant between April and June 1971, which was at the time reported to have cost production of 100,000 vehicles, equivalent to almost a quarter of the output for a full year.[27]

During 1971 the spring rates and damper settings were altered along with the front suspension bushes which reduced the bounciness of the ride and low speed ride harshness which had generated press criticism at the time of the Cortina Mark III's launch.[23]

Volumes recovered, and with the ageing Austin/Morris 1100/1300 now losing out to various newer models, the Cortina was Britain's top selling car in 1972,[28] closely followed by the Escort.[29] It remained the UK's top selling car until 1976 when it overtaken by the Mk2 Escort.

In late 1973 the Cortina Mark III was given a facelift, and was redesignated TD. The main difference was the dashboard and clocks, no longer did it slope away from the driver's line of sight. But shared the same dash and clocks as the later Mark IV and Mark V Cortinas, upgraded trim levels and revised grilles, revised rear lights, rectangular headlights for the XL, GT and the new 2000E (the "E" standing for executive), which replaced the GXL. The 1.3-litre Kent engine was carried over but now, 1.6-litre models all used the more modern 1.6-litre SOHC engine. Whilst the TD Cortina still had double A-arm suspension with coils at the front and a four-link system at the rear, handling was improved. The 2000E reverted to the classy treatment offered by the 1600E and later Mark IV/V Ghia models instead of the faux wood-grain trim offered by the GXL. The 2000E was also available as an estate version.

Export markets

The Mark III was sold in Canada until 1973.

In addition to four-cylinder models, the Mark III was available in South Africa as the 'Big Six' L and GL with the Essex V6 2.5-litre engine and Perana, GT and XLE with the Essex V6 3.0-litre engine. There was also a pick-up truck version available. In addition to the 1.6-litre inline-four, there was also a version with a locally built two-litre V4 engine, unlike anywhere else in the world. Max power is 76.6 kW (104 PS; 103 hp) SAE, and it was also available with pick-up bodywork beginning in late 1972. The Cortina 2000 V4 arrived during 1972 and also became available as a station wagon later in the year.[30] The shorter engine required a radiator shroud to compensate.[31] The Cortina GT, however, received an OHC inline-four in South Africa as well.

Ford Australia built its own versions using both the UK four-cylinder engines (1.6 and 2.0) and locally made inline six-cylinder engines (3.3- and 4.1-litre) from its Falcon line.

Ford Lio Ho in Taiwan began local production of the Cortina in March 1973.[32]

For Japan, the cars were narrowed by a few millimetres on arrival in the country in order that they fit into a lower tax bracket determined by exterior dimensions.[33] The Cortina was joined by the Ford Capri in Japan and was imported by Kintetsu Motors, an exclusive retailer of Ford products.

Mark IV (1976–1979)

Cortina Mark IV
Ford Cortina Mk IV saloon
Overview
Production 1976–1979
Assembly Ford Dagenham assembly plant (Dagenham, Essex, England, United Kingdom)
Ford Lio Ho (Zhongli City, Taoyuan County), Taiwan)
Broadmeadows, Victoria, Australia
Lower Hutt, New Zealand
Ulsan, South Korea
Designer Uwe Bahnsen
Body and chassis
Body style
Related Ford Taunus TC2
Powertrain
Engine 1.3 L Crossflow I4
1.6 L Crossflow I4
1.6 L Pinto TL16 I4
2.0 L Pinto TL20 I4
2.0 L Cologne V6
2.3 L Cologne V6
3.0 L Essex V6
3.3 L Falcon 200 I6
4.1 L Falcon 250 I6
Transmission 3/4-speed manual
3-speed automatic

The fourth-generation Cortina was a more conventional design than its predecessor, but this was largely appreciated by fleet buyers. Generally a rebody of the Mark III, as an integration of Ford's model range, this car was really a rebadged Ford Taunus. However, although the updated Taunus was introduced to Continental Europe in January 1976, Ford were able to continue selling the Cortina Mark III in undiminished numbers in the UK until they were ready to launch its successor as the Dagenham built Cortina Mark IV, which went on sale on 29 September 1976.[34]

Many parts were carried over, most notably the running gear. The raised driving position and the new instrument panel had, along with some of the suspension upgrades, already been introduced to the Cortina Mark III in 1975, so that from the driving position the new car looked much more familiar to owners of recent existing Cortinas than from the outside.[11] Cinema audiences received an early glimpse of the new Cortina (or Taunus) through its appearance in the James Bond The Spy Who Loved Me 1977 film.

The most obvious change was the new body, which achieved the marketing department objective of larger windows giving a better view out and a brighter feel to the cabin, but at the expense of body weight which was increased, albeit only marginally, by approximately 30 lb (14 kg).[11] Ford claimed an overall increase in window area of some 15%, with "40% better visibility" through the wider deeper back window.[11] Regardless of how these figures were computed, there must have been substantial weight-saving gains through reduced steel usage in the design, given the unavoidable extra weight of glass.[11]

This series spawned the first Ghia top-of-the-range model, which replaced the 2000E. The 2.3-litre Ford Cologne V6 engine was introduced in 1977 as an engine above the 2.0-litre Pinto engine, already a staple of the Capri and Granada ranges. However, 2.3-litre Cortinas never sold particularly well in the UK. The Cologne V6 was certainly a much smoother and more refined power unit than the Pinto, but the V6 models were more expensive to fuel and insure and were only slightly faster, being about 0.5 seconds faster from 0–60 and having a top speed of about 109 mph compared to the 104 mph of the 2.0-litre models. The 2.0-litre Ford Cologne V6 engine continued to be offered on Taunus badged cars in parallel with the Pinto unit,[35] and offers here an interesting comparison with the similarly sized in-line four-cylinder Pinto engine. The V6 with a lower compression ratio offered less power and less performance, needing over an extra second to reach 50 mph (80 km/h).[35] It did, however, consume 12½% less fuel and was considered by motor journalists to be a far quieter and smoother unit.[35] The 2.3-litre was available to the GL, S and Ghia variants. A 1.6-litre Ghia option was also introduced at the same time as the 2.3-litre V6 models in response to private and fleet buyers who wanted Ghia refinements with the improved fuel economy of the smaller 1.6-litre Pinto engine. Few cars were sold with the 1.6-litre engine though, the 2.0-litre Pinto was always by far the most common engine option for Ghia models.

Two-door and four-door saloons and a five-door estate were offered with all other engines being carried over. However, at launch only 1.3-litre-engined cars could be ordered in the UK with the two-door body, and then only with "standard" or "L" equipment packages.[11] In practice, relatively few two-door Mark IV Cortinas were sold. In some markets, the two-door saloon was marketed as a coupe, but this was not the case in Britain. Ford already competed in the coupe sector in Europe with the Capri, which was particularly successful on the British market.

There was a choice of base, L, GL, S (for Sport) and Ghia trims, again not universal to all engines and body styles. Rostyle wheels were fitted as standard to all Mark IV GL, S and Ghia models, with alloy wheels available as an extra cost option. The dashboard was carried over intact from the last of the Mark III Cortinas while the estate used the rear body pressings of the previous 1970 release Taunus.

Despite its status as Britain's bestselling car throughout its production run the Mark IV is now the rarest Cortina, with poor rustproofing and the model's popularity with banger racers cited as being the main reasons for its demise. Particularly scarce are the 2.0 and 2.3S models which were discontinued when the Mark V was introduced in August 1979.

Ford Australia built its own version, known as the TE, with the 2.0-litre 4-cylinder Pinto unit and the Ford Falcon's 3.3-litre and 4.1-litre 6-cylinder unit.[36] The six-cylinder versions were rather nose heavy and did not handle as well as the fours or the European V6 models.[37] Interior door hardware and steering columns were shared with the Falcons and the Australian versions also had their own instrument clusters, optional air conditioning, and much larger bumpers. It also had side indicators. The Cortina wagon was assembled by Renault Australia at its plant in Heidelberg in Victoria.[38]

A considerable number were exported to New Zealand under a free trade agreement where they were sold alongside locally assembled models similar to those available in the UK.

In South Africa, the Mark IV was built with the Kent 1.6-litre and the three-litre "Essex" V6. Beginning in mid-1978, the Cologne-built two-litre "Pinto" four also became available, rather than the old "Essex" V4 unit.[39] They were sold as L (1600), GL (2000), and Ghia (V6) with four-door saloon or estate bodywork.

Mark V (1979–1985)

Cortina Mark V
Ford Cortina GL Mark V Saloon
Overview
Production 1979–1986
Assembly Ford Dagenham assembly plant (Dagenham, England, United Kingdom)
Ford Lio Ho (Zhongli City, Taoyuan County (now Zhongli District, Taoyuan City), Taiwan)
Broadmeadows, Victoria, Australia
Lower Hutt, New Zealand
Ulsan, South Korea
Port Elizabeth, South Africa [40]
Body and chassis
Body style
Related Ford Taunus TC3
Powertrain
Engine 1298 cc Crossflow I4
1.6 L Crossflow I4
1.6 L Pinto TL16 I4
2.0 L Pinto TL20 I4
2.3 L Cologne V6
3.0 L Essex V6
3.3 L Falcon 200 I6
4.1 L Falcon 250 I6
Transmission
Sedan
Estate

The Mark V was announced on 24 August 1979.[41] Officially the programme was code named Teresa, although externally it was marketed as "Cortina 80", but the Mark V tag was given to it immediately on release by the press, insiders and the general public.

Largely an update of the Mark IV, it was really a step between a facelift and a rebody. The Mark V differentiated itself from the Mark IV by having revised headlights with larger turn indicators incorporated (which were now visible on the side too), a wider slatted grille said to be more aerodynamically efficient, a flattened roof, larger glass area, slimmer C-pillars with revised vent covers, larger slatted tail lights (on saloon models) and upgraded trim. The styling upgrades were done primarily to bring the Cortina into line with Ford's current design language seen on the Fiesta MkI, Capri MkIII and the forthcoming Escort MkIII.

Prices started at £3,475 for a basic 1.3-litre engined model.[42]

Improvements were also made to the engine range, with slight improvements to both fuel economy and power output compared to the Mark IV. The 2.3-litre V6 engine was given electronic ignition and a slight boost in power output to 116 bhp (87 kW; 118 PS), compared to the 108 bhp (81 kW; 109 PS) of the Mark IV. Ford also claimed improved corrosion protection on Mark V models; as a result, more Mark Vs have survived; however, corrosion was still quite a problem.

The estate models combined the Mark IV's bodyshell (which was initially from the 1970 Ford Taunus) with Mark V front body pressings. A pick-up ("bakkie") version was also built in South Africa. These later received a longer bed and were then marketed as the P100.

Variants included the Base, L, GL, and Ghia (all available in saloon and estate forms), together with Base and L spec 2-door sedan versions (this bodystyle was available up to Ghia V6 level on overseas markets). The replacement for the previous Mark IV S models was an S pack of optional extras which was available as an upgrade on most Mark V models from L trim level upwards. For the final model year of 1982 this consisted of front and rear bumper overriders, sports driving lamps, an S badge on the boot, tachometer, 4 spoke steering wheel, revised suspension settings, front gas shock absorbers,'Sports' gear lever knob, sports road wheels, 185/70 SR x 13 tyres and Fishnet Recaro sports seats (optional). Various "special editions" were announced, including the Calypso and Carousel. The final production model was the Crusader special edition which was available as a 1.3-litre, 1.6-litre, and 2.0-litre saloons or 1.6-litre and 2.0-litre estates. The Crusader was a final run-out model in 1982, along with the newly introduced Sierra. It was the best-specified Cortina produced to date and 30,000 were sold, which also made it Ford's best-selling special edition model. Another special edition model was the Cortina Huntsman, of which 150 were produced. By this time, the Cortina was starting to feel the competition from a rejuvenated (and Opel influenced) Vauxhall, which with the 1981 release Cavalier J-Car, was starting to make inroads on the Cortina's traditional fleet market, largely helped by the front wheel drive benefits of weight.

The Mk V Cortina was released in Australia in April 1980, where it was known as the TF Cortina.[43] It sold poorly and was dropped in 1982.[44]

Up to and including 1981, the Cortina was the best selling car in Britain. Even during its final production year, 1982, the Cortina was Britain's second best selling car and most popular large family car. On the continent, the Taunus version was competing with more modern and practical designs like the Talbot Alpine, Volkswagen Passat, and Opel Ascona.

The very last Cortina – a silver Crusader – rolled off the Dagenham production line on 22 July 1982 on the launch of the Sierra, though there were still a few leaving the forecourt as late as 1987, with one final unregistered Cortina GL leaving a Derbyshire dealership in 2005.[45] The last Cortina built remains in the Ford Heritage Centre in Dagenham, Essex, not far from the factory where it was assembled.[46]

Sales success

In 1967, the Ford Cortina interrupted the Austin/Morris 1100/1300s reign as Britain's best selling car. It was Britain's best selling car for nine out of ten years between 1972 and 1981, narrowly being outsold by the Ford Escort in 1976.

The final incarnation of the Cortina was Britain's best selling car in 1980 and 1981, also topping the sales charts for 1979 when the range was making the transition from the fourth generation model to the fifth - in that year it achieved a British record of more than 193,000 sales. Even in 1982, when during its final year of production it was second only to the Ford Escort.

The Cortina was also a very popular selling car in New Zealand throughout its production and continued to be sold new until 1984.[citation needed]

Although the Sierra went on sale in October 1982, thousands of Cortinas were still unsold at this point. More than 11,000 were sold in 1983, with six examples being sold as late as 1987.

Its demise left Ford without a traditional four-door saloon of this size, as the Sierra was initially available only as a hatchback or estate. Ford later addressed this by launching a saloon version of the Sierra (the Sierra Sapphire) at the time of a major facelift in early 1987. It also added an Escort-based four-door saloon, the Orion, to the range in 1983.

A total of nearly 2.6 million Cortinas were sold in Britain during its 20-year production life, and in March 2009 it was revealed that the Cortina was still the third most popular car ever sold there, despite having been out of production for nearly three decades.[47] Such was its popularity that even though it was only produced for three years of the 1980s, the Cortina was still Britain's seventh best selling car of that decade with almost 500,000 sales. It remained a popular buy on the used market and a common sight on British roads until well into the 1990s.[48]

The Cortina remained a popular second-hand buy and a common sight on British roads until well into the 1990s.

The BBC Two documentary series Arena had a segment about the car and its enthusiasts.[49]

The British punk rock band The Clash reference the car in the song Janie Jones, singing "He's got a Ford Cortina that just run without fuel."

Racing and rallying

During the 1960s and 1970s the Ford Cortina Lotus, as detailed on its own page, was a successful rally and racing car in a wide variety of competitions across Europe and North America. The standard Cortina was rarely used in competition of any sort, but benefited from the publicity generated by the Lotus versions.

At the end of their lives, however, many Cortinas did see action on oval racing circuits in the UK, as their rigidity and ready availability during the 1980s and 1990s made them a popular choice for banger racing. Although Cortinas are now relatively rare they remain coveted by the banger racing fraternity and all-Cortina meetings are still occasional fixtures on the racing calendar.

Ian Geoghegan won the 1964 Australian Touring Car Championship driving a Ford Cortina GT.

Other cars using Cortina engines

The Kent engines used in the Cortina (popularly known as the "Crossflow"), being lightweight, reliable and inexpensive, were popular with several low-volume sports car manufacturers, including Morgan who used them in the 1962–81 4/4 (and continue to use Ford engines in most of their current models). The engines are also found in a number of British kit cars, and until recently was the basis of Formula Ford racing, until replaced by the "Zetec" engine.

The Kent engines were also used in several smaller Fords, most notably the Escort, lower end Capris and Fiesta.

The Pinto overhead cam units used in the Mk.III onwards, as well as being fitted to contemporary Capris, Granadas and Transits, were carried over to the Sierra for its first few years of production, before gradually being phased out by the newer CVH and DOHC units. Like the Kent Crossflow, it was also extensively used in kit cars – as a result many Cortinas were scrapped solely for their engines – the 2.0-litre Pintos being the most popular.

In recent years, the opposite phenomenon has become popular among enthusiasts, where classic Cortinas have been retrofitted with modern Ford engines – the most popular unit being the Zetec unit from the Mondeo and Focus. The Zetec, although originally intended only for front wheel drive installation can be adapted fairly easily owing to the engine's use as a replacement for Kent units in Formula Ford.

Sales and manufacture outside the United Kingdom

The Cortina was also sold in other right hand drive markets such as Ireland where it was assembled locally, Australia, New Zealand, Indonesia, Malaysia, Singapore, Thailand (local production 1961-76 as a joint venture with Anglo-Thai Motor Company, Ford's import distributor), Malta and South Africa. Mark III Cortina estates were adopted as police cars in Hong Kong. The Cortina was also assembled in left hand drive (carrying Taunus badging) in the Philippines, in South Korea (by Hyundai), Turkey (by Ford-Otosan in Kocaeli), and in Taiwan (by Ford Lio Ho) until the early 1980s.

The first two generations of the car were also sold through American Ford dealers in the 1960s. The Cortina competed fairly successfully there against most of the other small imports of its day, including GM's Opel Kadett, the Renault Dauphine, and the just-appearing Toyotas and Datsuns, although none of them approached the phenomenal success of the Volkswagen Beetle. The Cortina was withdrawn from the US market when Ford decided to produce a domestic small car in 1971, the Ford Pinto, though it continued in Canada (with the Cortina Mark III) until the end of the 1973 model year. Subsequent European Ford products after the Cortina for the USA market (with the exception of the Fiesta Mk I c. 1978-80) were sold through Lincoln-Mercury dealerships (most notably the Ford Capri (MkI and II) and Ford Sierra - the latter of which was marketed in the USA under the Merkur marque).

The third generation Cortina was also sold in some continental European markets, such as Scandinavia, alongside the Taunus.[50] The Ford Cortina was also assembled in the Amsterdam Ford Factory from the launch in 1962 until 1975. Production was for the Dutch market, but also for export to non EU countries and even for export to the UK if the demand there was higher than the UK production capacity.

New Zealand

The New Zealand Cortina range generally followed that of Britain. Overall CKD assembly ran from 1962 to June 1983, at Ford's Lower Hutt (Seaview) plant.[21]

The Mark IV Cortina range, introduced into local assembly early in 1977, was very similar to that offered in the UK – a main specification difference, however, was the use of metric instrumentation, and that a two-door sedan was not offered. Engine sizes of 1.6 litres and 2.0 litres were available. The 2.0-litre was a very popular fleet vehicle and the transport of thousands of sales reps in New Zealand over the years.

Additionally there were limited imports of Australian Mark IV Cortinas, equipped with both 2.0-litre four-cylinder engines which featured more emissions control equipment than the UK-sourced cars, and the Falcon's 4.1-litre six-cylinder engines.

The Mark V range was introduced early in 1980, a range that featured 1.6 base, 2.0 L, 2.0 GL, 2.0 Ghia, 2.3 V6 Ghia, and wagon variants for the 1.6 base and 2.0 L. The 2.0, unencumbered by emissions regulations, has 74 kW (101 PS; 99 hp) at 5200 rpm. In 1982 the 2.0 GL model was discontinued and replaced with a 2.0 S (Sport) model, and unlike in the UK, it was a model in its own right. The "S" received a black, two-piece front spoiler and a rear spoiler. Two halogen extra lights were standard, as was a body-coloured grille. Most of the chrome trim was blacked out, while the steel wheels received a chrome band.[51] A 2.0 commercial van was also introduced – essentially a Cortina estate without rear seats, aimed towards fleet buyers.[37]

All 2.0-litre models had the option of automatic transmission, and with the 2.3-litre V6, it was the only transmission offered. The 2.3 also received power steering and additional sound deadening material.[37] A five-speed box was not available. A unique option, offered under guarantee by a dealership, South Auckland Ford, was a turbocharger.

The Ghia models were similarly equipped to UK models, but only the 2.3-litre V6 models featured imported Ford alloy wheels. Ford 'Rostyle' steel rims were fitted to all 2.0 GL, Ghia and S models, optionally on the other models. New Zealand Ghia models, however, did not feature a steel sliding sunroof (fitted as standard on UK Ghia models), although some models did feature an aftermarket sunroof.

The Cortina was a popular car in New Zealand, being the most sold car in seven years with over 100,000 assembled in total.[37] It was missed by many when it ceased production in June 1983, notably after Ford New Zealand had scoured the globe for surplus assembly kits, a number of which came from Cork in Ireland. Station wagons (estate models) remained available until 1984. The Cortina range was finally replaced by the 1983 Ford Telstar range and the 1984 Ford Sierra station wagon. Sales had been dropping in the early 1980s, however, with the average age of buyers in 1981 being between 45 and 54. Quality and fitment were also issues of concern, with the local assembler welcoming the Cortina's Mazda-built replacement.[52]

Compared with Britain and many other countries where the Cortina was originally exported, in New Zealand it has a far superior survival rate due to the climate being far drier and more favourable to the preservation of rust-free classic cars. It is not uncommon to see examples in everyday use especially New Zealand's rural areas, and obtaining spare parts to keep them on the roads is yet to become a significant problem.

Portugal

P100 pick-up

From 1971, the Cortina formed the basis of the Ford P100 pick-up truck, which was produced in South Africa purely for that market. The vehicle had a six-foot load bed with a locally sourced rear body.

In the mid-1970s grey imports of this model to the UK spurred Ford to examine the market for official import. The study culminated in the P100 which was a heavily revised version of the South African product with a seven-foot loadbed and T88 "Pinto" engine. The vehicle was for RHD markets only and was developed under the codename "Atlas" to reflect its market leading one tonne payload capability.

Other markets within Ford's European operation also wanted the vehicle, so when time came for a follow on product it was decided to source it from a European plant. At the time, Ford had divested from South Africa and sold its stake in Samcor, although it continued to assemble Ford models under licence. All production of the European engineered and Sierra-bodied P100, codename PE45, was produced for Europe in the Azambuja plant in Portugal. This vehicle was available in both RHD and LHD forms.

Ironically, the MK5 Cortina-based P100 was launched in 1982, the year that the standard Cortina was being replaced by the Sierra. However, it remained a popular choice with pick-up truck buyers until the Sierra-based P100 was launched in 1988; this version lasted until the end of Sierra production in early 1993.

South Africa

In South Africa, the Cortina range included V6 "Essex"-engined variants, in both 2.5-litre and 3.0-litre forms.

From July 1971, a locally designed pick-up truck version (known in Afrikaans as a "bakkie") was also offered, and this remained in production after the Cortina was replaced by the Sierra. The Cortina pick-up was exported to the UK, in a lengthened wheelbase form, as the Ford P100 until 1988, when Ford divested from South Africa, and a European built pick-up truck version of the Sierra was introduced in its place.

The Mark V model range, introduced in 1980 for the South African market included: 1.3-litre L (1980–1982), 1.6-litre L GL (1980–1983), 2.0-litre GL, Ghia, (1980–1984), 3.0-litre XR6 (1980–1983), 1.6-litre L Estate (1980–1983), 2.0-litre GL Estate (1980–1983), 3.0-litre GLS (1980–1984), 1.6-litre One-Tonner (1980–1985), 3.0-litre One-Tonner (1980–1985).

The XR6 was a sports version which used the Essex V6 and featured body aerofoils and sport seats.

In 1981 a version called the XR6 Intercepter was released as a homologation special made to compete in production car racing. They featured triple Weber DCNF carburetors, aggressive camshaft, tubular exhaust manifold, suspension revisions and wider Ronal 13 inch wheels. They produced 118 kW and were only available in red. 200 were produced.[53]

Later on a special edition XR6 TF was released to celebrate 'Team Fords' racing success with the XR6. They were essentially XR6s in exterior and interior Team Ford colours, which were blue and white.

In 1983 a special version was created by Simpson Ford to appease the demand for an Intercepter-like Cortina and was sold through Ford dealerships countrywide. It was called the XR6 X-ocet and featured a Holley carbureter, aggressive camshaft and tuned exhaust. They came in red with a white lower quarter and did 0–100 km/h (62 mph) in 8.5 seconds with a top speed of 195 km/h (121 mph).

South African Mark V models differed slightly from UK models with different wheels, bumpers and interior trim.

The last brand new Cortina was sold in South Africa by mid-1984. It was often the country's top selling car, being far more popular than the Sierra, Telstar and Mondeo models that followed it.

Pakistan

In the early 1960s Cortinas were assembled by Ali Automobiles in Karachi.[54]

  1. ^ Cortina Auto-Bobbing FordHeritage YouTube channel. Retrieved 2010-06-06.
  2. ^ "Aussie Ford now adds Cortinas to Falcon line". The Straits Times. 30 September 1963. Retrieved 25 February 2016. 
  3. ^ "Ford's big new venture". The Straits Times. 29 October 1963. Retrieved 25 February 2016. 
  4. ^ "First motor assembly plant in Malaysia is 38 years old". The Straits Times. 9 February 1964. Retrieved 25 February 2016. 
  5. ^ a b c d e "Used Car Test: 1962 Ford Cortina". Autocar. 3804 (130): 22–23. 9 January 1969. 
  6. ^ a b Culshaw; Horrobin (1974). Complete Catalogue of British Cars. London: Macmillan. ISBN 0-333-16689-2. 
  7. ^ "Obituaries: Roy Brown". The Telegraph. 5 March 2013. Retrieved 23 March 2014. 
  8. ^ Evening Times - Google News Archive Search
  9. ^ "Ford Cortina Mk1 UK Domain". Fordcortina.co.uk. 16 May 1998. Retrieved 22 July 2011. 
  10. ^ A More Zestful Cortina. The Times, Friday, Jan 18, 1963; pg. 3; Issue 55602
  11. ^ a b c d e f g Daniels, Jeffrey (2 October 1976). "The Fourth Cortina". Autocar: 12–16. 
  12. ^ The Glasgow Herald - Google News Archive Search
  13. ^ a b "Cortina – new right through". The Motor. 3360: 152–158. 22 October 1968. 
  14. ^ "Cortina – new right through". The Motor: 152–158. 22 October 1966. 
  15. ^ a b c Logoz, Arthur, ed. (1971), "Die Taunus-Cortina-Story", Auto-Universum 1971 (in German), Zürich, Switzerland: Verlag Internationale Automobil-Parade AG, XIV: 39 
  16. ^ "Ford Cortina celebrates 50th on BBC’s One Show". Ford UK. 21 September 2012. Retrieved 2 March 2015. 
  17. ^ Driving & Leisure, 1970, p34-39
  18. ^ "Ford Cortina Estate Car". Autocar. 126 (3705): 20–21, 32. 15 February 1967. 
  19. ^ "54th Paris Show". Autocar. 127 (3739): 66–71. 12 October 1967. 
  20. ^ "In this case the ‘E’ is for Executive". Sorted Corty. 2016-11-01. Retrieved 2016-11-05. 
  21. ^ a b Anderson, Donn (March 1993). "Classic Cars". New Zealand Car. Auckland, New Zealand: Accent Publishing Cnr. 7 (5): 82. ISSN 0113-0196. 
  22. ^ "Cortina Perana Mk 2". http://www.africanmusclecars.com. Retrieved 4 September 2012.  External link in |work= (help)
  23. ^ a b c d e f g "Road test: Ford Cortina 1300XL". Motor: 12–16. 12 February 1972. 
  24. ^ Auto-Universum 1971, p. 41
  25. ^ Smith, Maurice A, ed. (16 November 1967). "Know your car: Ford Cortina". Autocar: 25–26. 
  26. ^ Strike may put brake on Cortinas, The Glasgow Herald, October 23, 1970
  27. ^ "World wide: Ford and their market gap". Autocar. 134 (3928): 3. 8 July 1971. 
  28. ^ Best Selling Cars – Matt's blog " UK 1972-1973: Ford Cortina best seller
  29. ^ "Autotest Ford Cortina 1600 XL". Autocar. 138. 4004): 16–21. 22 February 1973. 
  30. ^ Wright, Cedric, ed. (December 1972). "Ford Cortina 2000 V4 station wagon". CAR (South Africa). Vol. 16 no. 11. Cape Town, South Africa: Ramsay, Son & Parker (Pty) Ltd. p. 48. 
  31. ^ Wright, Cedric, ed. (November 1972). "Ford Cortina V4 2000 L sedan". CAR (South Africa). Vol. 16 no. 10. Cape Town, South Africa: Ramsay, Son & Parker (Pty) Ltd. p. 32. 
  32. ^ Distribution in Asia/Pacific's Developing Markets, Business International Asia/Pacific Limited, 1978, page 144
  33. ^ Ford at Dagenham: The Rise and Fall of Detroit in Europe, David Burgess Wise, Breedon, 2001, page 177
  34. ^ New Cortina steps into sports car class, The Glasgow Herald, September 29, 1976
  35. ^ a b c "Qual der Wahl: Taunus Kaufberatung". Auto, Motor und Sport. Heft. 17: 45–52. 18 August 1976. 
  36. ^ David-sized car with Goliath motor, The Age, September 13, 1977, page 18
  37. ^ a b c d Anderson, p. 83
  38. ^ Renault Aust to assemble Ford waggons, The Sydney Morning Herald, February 15, 1977, page 3
  39. ^ Wright, Cedric, ed. (August 1978). "Ford Cortina 2000 GL Station Wagon". CAR (South Africa). Vol. 22 no. 7. Ramsay, Son & Parker (Pty) ltd. p. 59. 
  40. ^ Africa, members.casema.nl Retrieved on 9 March 2015
  41. ^ Evening Times - Google News Archive Search
  42. ^ "FORD Cortina ‘80 | Car Specs | Octane". Classicandperformancecar.com. Retrieved 22 July 2011. 
  43. ^ Driver beware - 40 new car models ahead, The Sydney Morning Herald, January 6, 1980
  44. ^ The right blend at the right time, The Sydney Morning Herald, May 25, 1982
  45. ^ "Owners' Photos". Ford Cortina 80/Mk5 E&OC. Archived from the original on 1 July 2013. Retrieved 16 June 2015. 
  46. ^ "Hammond's trip down memory lane". Norfolk Motoring News. Retrieved 10 September 2010. [dead link]
  47. ^ "icLiverpool – Recession-proof wise-buys revealed". Icliverpool.icnetwork.co.uk. 17 March 2009. Archived from the original on 29 September 2010. Retrieved 27 July 2010. 
  48. ^ Slavin, John (20 January 2014). "Top 10 Selling Cars of the 1980s". honestjohn. Retrieved 4 July 2015. 
  49. ^ "Arena: The Private Life of the Ford Cortina (1982)". British Film Institute. Retrieved 7 November 2012. 
  50. ^ Ford at Dagenham: The Rise and Fall of Detroit in Europe, David Burgess Wise, Breedon, 2001, page 172
  51. ^ Anderson, p. 85
  52. ^ Webster, Mark (2002), Assembly: New Zealand Car Production 1921-98, Birkenhead, Auckland, New Zealand: Reed, p. 154, ISBN 0-7900-0846-7 
  53. ^ "Cortina XR6 Interceptor". africanmusclecars.com. Retrieved 4 September 2012. 
  54. ^ Zaman, Habibuz (1999). Seventy years in a shaky subcontinent. London, England: Janus. p. 198. ISBN 1857564057. Retrieved 9 April 2016. 



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks

Car, Truck,MotorBike, Bicycle, Engine, Racer