Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution 2.0 (ФигÑÑки).
霍尔效应传感器也称霍尔传感器,是一个换能器,将变化的磁场转化为输出电压的变化。霍尔传感器首先是用来测磁场的,此外还可以被用来测量产生和影响磁场的物理量[1],例如,被用于接近开关[2],霍尔乘法器,位置测量,转速测量,和电流测量设备[3]。
其最简单的形式是,传感器作为一个模拟换能器,直接返回一个电压。[4]
在已知磁场下,其距霍尔盘的距离是可以被设定的。使用多组传感器,磁铁的相关位置可被推断出。
通过导体的电流会产生一个随电流变化的磁场,并且霍尔效应传感器可以在不干扰电流情况下而测量电流。典型的为,将其和绕组磁芯或在被测导体旁的永磁体合成一体。
通常,霍尔效应传感器和电路相连,从而允许设备以數位(开/关)模式操作,在这种情况下可以被称为开关[5]。工业中常见的设备,例如气缸,也被用于日常设备中;如一些打印机使用他们来监测缺纸和敞盖的情况。当键盘被要求高可靠性时,也被应用于键盘中。
霍尔效应传感器通常被用于计量车轮和轴的速度,例如在内燃机点火定时(正時)或转速表上[6]。其在无刷直流电动机的使用,用来检测永磁铁的位置。图示中的轮子,带有两个等距的磁铁,传感器上的电压在一个周期内将两次达到峰值。此设置通常被用来校准磁盘驱动的速率。
霍尔探头使用铟的化合物晶体,如锑化铟。晶体大小为5平方毫米左右,置于铝基上,通过封装成为探头。晶体平面垂直于探头底侧,底侧由非铁磁材料制成,以避免自身影响磁场。引线自晶体出发,穿过底侧,进入到电路模块。
把探头置于磁场中,当电流流经晶体时,载流子受洛伦兹力作用出现偏转导致载流子在晶体上的分布不均匀,晶体两端的铝基上因此可以探测到霍尔电压。
霍尔探头可以测量微弱的地球磁场。霍尔探测器首先需要根据已知磁场强度进行调校。然后,探头需要以适当方向放置以使地磁场磁流线直接穿过它。然后再以反方向放置,所读出的流密度是地球磁流密度的两倍。
This article uses material from the Wikipedia article "霍尔效应传感器", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD