powered by CADENAS

Social Share

Amazon

Caduceus as a symbol of medicine (2941 views - Medical & Health)

The caduceus is the traditional symbol of Hermes and features two snakes winding around an often winged staff. It is often mistakenly used as a symbol of medicine instead of the Rod of Asclepius, especially in the United States. The two-snake caduceus design has ancient and consistent associations with trade, eloquence, negotiation, alchemy and wisdom. The modern use of the caduceus as a symbol of medicine became established in the United States in the late 19th and early 20th century as a result of documented mistakes, misunderstandings and confusion.
Go to Article

Explanation by Hotspot Model

Youtube


    

Caduceus as a symbol of medicine

Caduceus as a symbol of medicine

Caduceus as a symbol of medicine

The caduceus is the traditional symbol of Hermes and features two snakes winding around an often winged staff. It is often mistakenly used as a symbol of medicine instead of the Rod of Asclepius, especially in the United States. The two-snake caduceus design has ancient and consistent associations with trade, eloquence, negotiation, alchemy and wisdom.

The modern use of the caduceus as a symbol of medicine became established in the United States in the late 19th and early 20th century as a result of documented mistakes, misunderstandings and confusion.[1][2][3][4][5]note a[›]

Early use in a possible medical context

Before the ancient Romans and Greeks (about 2612 BC), older representations from Syria and India of sticks and animals looking like serpents or worms are interpreted as a direct representation of traditional treatment of dracunculiasis, the Guinea worm disease.[6]

While there is ample historical evidence of the use of the caduceus, or herald's staff, to represent Hermes or Mercury (and by extension commerce and negotiation), early evidence of any symbolic association between the caduceus and medicine or medical practice is scarce and ambiguous. It is likely linked to the alchemical "universal solvent", Azoth, the symbol of which was the caduceus.

The Guildhall Museum in London holds a 3rd-century oculist's seal with caduceus symbols both top and bottom. The seal was apparently used to mark preparations of eye medicine.[7] It is believed likely that rather than being evidence of a medical association per se, this is rather an allusion to the words of the Greek poet Homer who described the caduceus as "possessing the ability to charm the eyes of men", which relates to the business of an oculist.[7]

Walter Friedlander proposed that early association of the caduceus with medicine might have derived from the association of Hermes Trismegistus ("Thrice-Great Hermes") with early chemistry and medicine as aspects of alchemy as an esoteric practice. He notes however, that "although these various factors may link Hermes/Mercury, along with his caduceus, with alchemical medicine, they may just as well link all the other non-medical aspects of alchemy with Hermes/Mercury and the caduceus."[1]

Beginning with the 16th century there is limited evidence of the use of the caduceus in what is arguably a medical context. However, this evidence is also ambiguous. In some cases it is clear that the caduceus symbolized wisdom, without any specific medical connotations.[1]

The caduceus appears in a general medical context in the printer's device used by the Swiss medical printer Johann Frobenius (1460–1527), who depicted the staff entwined with serpents and surmounted by a dove, with a biblical epigraph in Greek, "Be ye therefore wise as serpents and harmless as doves" (Matthew 10:16, here in the KJV translation),[3] in keeping with the connotations of the caduceus as a symbol of messengers and publishers based on the association of Hermes or Mercury with eloquence and negotiation. Friedlander observed that Frobenius could hardly be considered a medical printer, as had previously been asserted, noting that in a review of 257 of the works bearing this printer's device only one was related to medicine. Similar use of the caduceus in printers' marks continues to the present day, with companies including F. A. Davis Company still using the symbol as an element of their insignia.

There are a few other examples of use in this period. It may have been used as a symbol by Sir William Butts, physician to Henry VIII.[3] Similarly, physician John Caius, founder of Caius College, Cambridge, and at the time President of the Royal College of Physicians, during official visits to his eponymous college, had carried before him a silver caduceus on a cushion, and later presented this artefact to the college, where it remains in the College's possession.[8] This use was adduced by the medical historian (and primary apologist for the use of the caduceus in a medical context) Fielding Garrison to support his argument that the caduceus was used as a symbol of medicine as far back as the 16th century. However, as Walter Friedlander noted, "what Caius used was a non-specific herald's wand, rather than the caduceus of Hermes." In support of this assertion he quotes Caius's own words on why he chose a herald's wand as a symbol, making it clear that he chose it as a symbol of prudence.[1] This same passage was also earlier referenced by Engle in refuting Garrison's claim. Engle and Friedlander are not the only ones to have noted that the use of the Caduceus by Caius had nothing to do with supposed medical symbolism; as indicated in a publication produced by the Royal College of Physicians itself: "[...] by introducing the caduceus into the ceremony of the College of Physicians, Caius unintentionally added to the confusion between the two emblems for later times, when few people understand the visual signs with which he was so familiar."[9]

In support of the idea that the caduceus had a long-standing association with medicine, Garrison also mentioned the fact that the English medical printer Churchill used the symbol as a printer's device, beginning some time around 1844. Friedlander has examined this subject in detail, and shows that Churchill was well aware that the rod of Asclepius was the accepted symbol of medicine. He is, it seems, inclined to think that the adoption of the caduceus in this context probably had something to do with the relation between publishing and the role of Mercury as a messenger and scribe. He notes, however

That John Churchill adopted the caduceus as his printer's device independent of any idea that it symbolized medicine does not mean that, once having adopted it, it did not play some role in the caduceus coming to be accepted as a symbol of medicine, at least in the United States. During the remaining part of the nineteenth century several United States publishers appear to have copied or modified Churchill's caduceus and placed this mark on their medical books. Other contemporary British publishers did not use a caduceus and the caduceus had never been as widely connected to medicine in Great Britain or in Europe as it has been in the United States.

— Walter J Friedlander, The Golden Wand of Medicine: A History of the Caduceus Symbol in Medicine[1]

In any case, in Great Britain, as late as 1854, the distinction between the rod of Asclepius and the caduceus as symbols of two very different professions was apparently still quite clear. In his article On Tradesmen's Signs of London A.H. Burkitt notes that among the very old symbols still used in London at that time, which were based on associations between pagan gods and professions, "we find Mercury, or his caduceus, appropriate in trade, as indicating expedition. Esculapius, his Serpent and staff, or his cock, for professors of the healing art"[10]

Adoption by the US military

Widespread confusion regarding the supposed medical significance apparently arose as a result of events in the United States that occurred in the second half of the 19th century.[5] As pointed out by Garrison, the caduceus had appeared on the chevrons of Army hospital stewards as early as 1856[11] (William K. Emerson indicates the insignia was adopted earlier, in 1851). It has been asserted that this was a result of ignorance or misinterpretation regarding the pre-existing designation of the rod of Asclepius by the Surgeon General of the United States for this purpose.[7] It is worth noting that hospital stewards were not physicians; they played a supporting role preparing drugs for surgeons, supervising nurses and cooks, maintaining accounting and medical records, and in emergencies sometimes performed minor surgery or provided prescriptions.[12]

Later, in 1871, the Surgeon General designated the caduceus as the seal of the Marine Hospital Service (destined to become the U.S. Public Health Service in 1912). Gershen states that the change was for aesthetic reasons,[13] whereas Friedlander states the caduceus was adopted by the Marine Hospital Service "because of its relationship with merchant seamen and the maritime industry".[1]

The caduceus was formally adopted by the Medical Department of the United States Army in 1902 and was added to the uniforms of Army medical officers. According to Friedlander, this was brought about by one Captain Frederick P. Reynolds, although Bernice Engle states "the use of the caduceus in our army I believe to be due chiefly to the late Colonel Hoff, who has emphasized the suitability of the caduceus as an emblem of neutrality.[3] Reynolds had the idea rejected several times by the Surgeon General, but persuaded the new incumbent — Brig. Gen. William H. Forwood — to adopt it. This resulted in considerable controversy.

The Army and Navy Register of 28 June 1902 discusses the argument, which reflects the fact that a number of medical officers were unhappy with the choice. The article editor claims that the symbol was not chosen for its medical connotations and proposes the following symbolic interpretation: "the rod represents power, the serpents stand for wisdom and the two wings imply diligence and activity, qualities which are undoubtedly possessed by our Medical officers."[14] The editor also points out that the majority of Medical Corps personnel are not even doctors. According to this line of reasoning, the caduceus was never intended to be a symbol of medicine. The inconsistency was noticed several years later by the librarian to the Surgeon General, but for reasons which are not entirely clear, the symbol was not changed.[5]

Considerable light is shed on this confusion by an anonymous letter republished by Emerson, a historian of United States Army insignia and uniforms. He indicates that the April 1924 issue of The Military Surgeon printed a review of an earlier article that appeared in the Presse Médicale in which the author stated "There is nothing in history to justify the use of the caduceus as the emblem of the physician [...] it is most unfortunate that the 'confusion' exists." In an anonymous rebuttal contained in a letter to the editor published three months later in The Military Surgeon it was claimed that the late Col. John R. van Hoff was a member of the board that selected the emblem ("if he was not the one who was chiefly instrumental in its adoption"). In the letter to the editor reproduced by Emerson, the anonymous author claims

According to this view the caduceus was not intended to be a medical symbol (and, though explained differently, this reflects the view advanced by the editor commenting in The Army and Navy Register of 28 June 1902 discussed above). Nevertheless, after World War I the caduceus was employed as an emblem by both the Army Medical Department and the Navy Hospital Corps. Even the American Medical Association used the symbol for a time, but in 1912, after considerable discussion, the caduceus was abandoned by the AMA and the rod of Asclepius was adopted instead.[3]

This shift back to use of the rod of Asclepius to symbolize medicine can also be seen in the United States military. The Army Medical Corps, having popularised the caduceus, while retaining the caduceus for its own plaque and insignia, is now part of the Army Medical Department, which has since adopted the Rod of Asclepius as its main symbol. Furthermore, when the U.S. Air Force designed new medical insignia, it also adopted the rod of Asclepius.

Contemporary views

Despite widespread acceptance of the caduceus as a medical symbol in the United States, it has been observed that the rod of Asclepius has "the more ancient and authentic claim to be the emblem of medicine".[15] Most attempts to defend its use in a medical context date from the last quarter of the 19th century through the first quarter of the 20th, and have been characterized as "based on flimsy and pseudo-historical research".[7]

In a survey of 242 logos used by organizations related to health or medicine, Friedlander found that professional associations were more likely to display the rod of Asclepius (62%), while organizations with a commercial focus were more likely to use the caduceus (76%). Hospitals were an exception (37% used a staff of Asclepius whereas 63% used a caduceus). Friedlander felt it likely that this might reflect the fact that "professional medical organizations have more often sought a real understanding of the meaning of the two symbols whereas commercial organizations have been less interested in the historical basis of their logo or insignia and more concerned with how well a certain symbol will be recognized by the iconographically unsophisticated audience they are trying to attract to their wares."[1]

The use of the caduceus in a medical context has long been frowned upon by many professionals, academics and others who are familiar with the historical significance of both symbols. This has occasioned impassioned remarks by those frustrated with the continuing confusion.

It has been observed that the caduceus is particularly inappropriate for use as a medical symbol due to its long associations with the Greek god Hermes, who was patron of commerce and traders as well as thieves, liars, and gamblers.[17]

On the other hand, it has also been remarked – not without considerable irony – that commercial aims in medicine, especially in the United States of America, make the caduceus an appropriate symbol, at least for some physicians.

Others are unapologetic about the association of medicine with commerce, recognizing the importance of "advertising essential for competitive marketing", and suggesting that it is up to individual physicians to choose between the two symbols, based on their own views about what associations are appropriate.[19] In 2009, conspiracy theorist David Icke suggested that the American Medical Association deliberately adopted the symbol due to their underlying profit motives,[20] although the AMA has used the Rod of Asclepius for over a century,[21] and its current logo since 2005.[22]

In North America, there are calls to clarify the symbol and to move to a uniform use of the rod of Asclepius. For example, the director of communications of the Minnesota Medical Association is quoted as saying, "If it's got wings on it, it's not really the symbol of medicine; some may find it hard to believe, but it's true. It's something like using the logo for the National Rifle Association when referring to the Audubon Society".[23]

However, Andrew Weil, a proponent of alternative medicine, has suggested that the caduceus is appropriate as a medical symbol "because it embodies an esoteric truth that must be grasped to gain practical control over the shifting forces that determine health and illness."[24]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Medicine & Health

3D,virus,bacteria,medicine, molecule,atom,chemistry,labor