powered by CADENAS

Social Share

Amazon

Oceanium (4852 views - Animals)

The Oceanium is a public aquarium that opened in 2001 in Diergaarde Blijdorp, a zoo in Rotterdam, Netherlands. The Oceanium lies in the expansion area of the zoo, which includes a new entrance and parking area, and was the biggest project to date for the zoo. The area around the Oceanium is home to projects depicting the Americas. The Oceanium is also home to scientific research into the conservation of coral.
Go to Article

Explanation by Hotspot Model

Youtube


    

Oceanium

Oceanium

Oceanium
Oceanium
Viewing tunnel at the aquarium
Date opened2001
LocationRotterdam, Netherlands
Coordinates51°55′43″N 4°26′43″E / 51.9286°N 4.4454°E / 51.9286; 4.4454Coordinates: 51°55′43″N 4°26′43″E / 51.9286°N 4.4454°E / 51.9286; 4.4454
Volume of largest tank3,375,000 l (742,000 imp gal; 892,000 US gal)
Total volume of tanks8,000,000 l (1,800,000 imp gal; 2,100,000 US gal)[1]
Websitewww.diergaardeblijdorp.nl?lang=EN

The Oceanium is a public aquarium that opened in 2001 in Diergaarde Blijdorp, a zoo in Rotterdam, Netherlands. The Oceanium lies in the expansion area of the zoo, which includes a new entrance and parking area, and was the biggest project to date for the zoo.[1] The area around the Oceanium is home to projects depicting the Americas.

The Oceanium is also home to scientific research into the conservation of coral.

  1. ^ a b Rotterdamistop: Diergaarde Blijdorp - Oceanium. Retrieved 15 September 2013




This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Animals

3D,data,libary,model,catalog,rendering,skull,bone,animal,reptile,bird,insect,mammal,class,classification,order,family,species,genus