Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (CZmarlin — Christopher Ziemnowicz, releases all rights but a photo credit would be appreciated if this image is used anywhere other than Wikipedia. Please leave a note at Wikipedia here. Thank you!).
Body-on-frame is an automobile construction method where a separate body is mounted on a relatively rigid frame or chassis carrying the engine and drivetrain. The original method of building automobiles, body-on-frame construction is now used mainly for pickup trucks and (mostly full size) SUVs.
In the late 19th century the frames, like those of the carriages they replaced, might be made of wood (commonly ash), reinforced by steel flitch plates - but in the early 20th century steel ladder frames or chassis rapidly became standard. Mass production of all-metal bodies began with the Budd Company and the Dodge Brothers. Mass production of all-metal bodies became general in the 1920s but Europe, with exceptions, followed almost a decade later. Europe's custom-made or "coachbuilt" cars usually contained some wood framing or used aluminium alloy castings.
Unibody or monocoque designs, where panels within the body supported the car on its suspension, were developed by European manufacturers in the late 1920s with Budd USA (which had a number of large factories in Europe) and its technical knowhow; but not in USA until the 1950s and generally later. Because of the high cost of designing and developing these structures and the high cost of specialised machinery to make the large pressings required by this style of construction it is not used by low-volume manufacturers, who might construct an equivalent by welding steel tube to form a suitable space frame.
The Ford Model T carried the tradition of body-on-frame over from horse-drawn buggies, helping to facilitate high volume manufacturing on a moving assembly line.[2] In the United States, frequent changes in automotive design made it necessary to use a ladder frame rather than unibody construction to make it possible to change the design without having to change the chassis, allowing frequent changes and improvements to the car's bodywork and interior (where they were most noticeable to customers) while leaving the chassis and driveline unchanged, and thus keeping costs down and design times short. It was also easy to use the same chassis and driveline for several very different cars. Especially in the days before computer-aided design, this was an advantage.[3]
Most small passenger vehicles switched to unibody construction by the end of the 1930s. The trend had started with cars like the Citroen Traction Avant (1934) and Opel Olympia (a General Motors design) introduced in 1935. Trucks, bus manufacturers and large low volume cars or those made in the United States continued to use separate bodies on "conventional" frames. Body-on-frame remains the preferred construction method for heavy-duty commercial vehicles (especially those intended to carry or pull heavy loads, such as trucks and some sport utility vehicles (SUVs)) but as production volumes rise increasing numbers of SUVs and crossover SUVs are switching to unibody frames. Mass-market manufacturers Ford, General Motors and Chrysler are abandoning true body-on-frame SUVs, opting, when sales volume permits, for more efficient unibody construction.[4] Toyota currently manufactures the most body-on-frame SUVs with the 4Runner, Sequoia, Land Cruiser, Lexus GX and LX followed by Nissan with the Patrol, Armada, and Infiniti QX56/80.[5] The Ford Panther platform, which was discontinued in 2011, was the last series of traditional passenger cars to be built in this manner.
One variant used by Chevrolet for its Corvette incorporates the inner skeleton to the frame.
An intermediate to full monocoque construction was the 'semi-monocoque' used by the Volkswagen Beetle and Renault 4. These used a lightweight separate chassis made from pressed sheet steel panels forming a 'platform chassis', to give the benefits of a traditional chassis, but with lower weight and greater stiffness. Both of these chassis were used for several different models. The mid-1930s designed Volkswagen made use of the bodyshell for structural strength as well as the chassis — hence 'semi-monocoque'. Traditionally chassis had "compliance", they were designed to allow some twisting. As suspensions improved they could not perform correctly unless supporting a rigid structure like that intended to be provided by unibody or monocoque construction.
The Lincoln Town Car once dominated the American limousine market because it was the last American luxury car made on the body-on-frame system and was easily lengthened for livery work. With the Town Car discontinued since 2011, the de facto replacement is the Lincoln Navigator SUV.
This section needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. Find sources: "Body-on-frame" – news · newspapers · books · scholar · JSTOR (January 2017) (Learn how and when to remove this template message) |
The following is a list of production cars, SUVs, and light-duty pickup trucks available in the United States that currently have a body-on-frame construction. The list is divided by vehicle category.
SUV
Pickup Truck
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer, Bus