Licensed under Creative Commons Attribution-Share Alike 3.0 (Robert Prummel from nl).
Cross of Merit for Women and Girls Ehrenkreuz für Frauen und Jungfrauen | |
---|---|
Awarded by King of Prussia | |
Country | Prussia |
Eligibility | Prussian women and girls |
Awarded for | self-sacrificing work for the good of the fighting troops and their families |
Campaign(s) | Franco-Prussian War |
Statistics | |
Total awarded | 2979 |
Related | Iron Cross |
The Cross of Merit for Women and Girls (Ehrenkreuz für Frauen und Jungfrauen) was created on 22 March 1871 by Kaiser Wilhelm I, German Emperor, in his capacity as King of Prussia. The award was presented only to women, but was not a Ladies Order in the most narrow sense. Women and girls were awarded at the request of Empress Augusta, and the award was bestowed by the Kaiser.
The appearance and shape is very similar to the Iron Cross, but on the obverse at the junction of the arms is an emblem of the Red cross. On the reverse there is the royal crown above the intertwined monograms "A" and "W" and the date of 1870–1871. The cross was worn from suspended by a bow on the left chest. The ribbon is the same as that of the Iron Cross for non-combattants, white with black stripes at the edge.
Orders | ||
---|---|---|
Military decorations | ||
Civil decorations |
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,model,library,rendering,Inca,Maya,Egypt,Pyramids,Bible, Quoran,Gizeh,Greek,Ancient,Medival Times, Stone Age