powered by CADENAS

Social Share

Amazon

Wastegate (11318 views - Mechanical Engineering)

A wastegate is a valve that diverts exhaust gases away from the turbine wheel in a turbocharged engine system. Diversion of exhaust gases regulates the turbine speed, which in turn regulates the rotating speed of the compressor. The primary function of the wastegate is to regulate the maximum boost pressure in turbocharger systems, to protect the engine and the turbocharger. One advantage of installing a remote mount wastegate to a free-float (or non-WG) turbo includes allowance for a smaller A/R turbine housing, resulting in less lag time before the turbo begins to spool and create boost.
Go to Article

Explanation by Hotspot Model

Youtube


    

Wastegate

Wastegate

A wastegate is a valve that diverts exhaust gases away from the turbine wheel in a turbocharged engine system.

Diversion of exhaust gases regulates the turbine speed, which in turn regulates the rotating speed of the compressor. The primary function of the wastegate is to regulate the maximum boost pressure in turbocharger systems, to protect the engine and the turbocharger. One advantage of installing a remote mount wastegate to a free-float (or non-WG) turbo includes allowance for a smaller A/R turbine housing, resulting in less lag time before the turbo begins to spool and create boost.[1]

Wastegate types

External

An external wastegate is a separate self-contained mechanism typically used with turbochargers that do not have internal wastegates. An external wastegate requires a specially constructed turbo manifold with a dedicated runner going to the wastegate. The external wastegate may be part of the exhaust housing itself. External wastegates are commonly used for regulating boost levels more precisely than internal wastegates in high power applications, where high boost levels can be achieved. External wastegates can be much larger since there is no constraint of integrating the valve or spring into the turbocharger and turbine housing. It is possible to use an external wastegate with an internally gated turbocharger. This can be achieved through a specially designed bracket that easily bolts on and restricts the movement of the actuator arm, keeping it from opening. Another route involves welding the internal wastegate shut which permanently keeps it from opening, but failure of the weld can allow it to open again.

External wastegates generally use a valve similar to the poppet valve found in the cylinder head. However they are controlled by pneumatics rather than a camshaft and open in the opposite direction. External wastegates can also use a butterfly valve, though that is far less common.

Internal

An internal wastegate is a built-in bypass valve and passage within the turbocharger housing which allows excess exhaust pressure to bypass the turbine into the downstream exhaust. Control of the internal wastegate valve by a pressure signal from the intake manifold is identical to that of an external wastegate. Advantages include simpler and more compact installation, with no external wastegate piping. Additionally, all waste exhaust gases are automatically routed back into the catalytic converter and exhaust system. Many OEM turbochargers are of this type. Disadvantages in comparison to an external wastegate include a limited ability to bleed off exhaust pressure due to the relatively small diameter of the internal bypass valve, and less efficient performance under boost conditions.

Atmospheric/divorced wastegates

A "divorced" wastegate dumps the gases directly into the atmosphere, instead of returning them with the rest of an engine's exhaust. This is done to prevent turbulence to the exhaust flow and reduce total back pressure in the exhaust system. A Divorced wastegate dumper pipe is commonly referred to as a screamer pipe due to the unmuffled waste exhaust gases and the associated loud noises they produce.[citation needed]

Control

Manual

The simplest control for a wastegate is a mechanical linkage that allows the operator to directly control the wastegate valve position. This manual control is used in some turbo-charged light aircraft.[2]

Pneumatic

The simplest closed-loop control for a wastegate is to supply boost pressure directly from the charge air side to the wastegate actuator. A small hose can connect from the turbocharger compressor outlet, charge pipes, or intake manifold to the nipple on the wastegate actuator. The wastegate will open further as the boost pressure pushes against the force of the spring in the wastegate actuator until equilibrium is obtained. More intelligent control can be added by integrating an electronic boost controller.

Standard wastegates have one port for attaching the boost control line from the charge air supply line or boost control solenoid. Recent advances in internal wastegate actuators bring dual port control.

A dual port wastegate adds a second port on the opposite side of the actuator. Air pressure allowed to enter this second port aids the spring to push harder in the direction of closing the wastegate. This is exactly the opposite of the first port. The ability to help the wastegate remain closed as boost pressure builds can be increased. This also adds further complexity to boost control, requiring more control ports on the solenoid or possibly a complete second boost control system with its own separate solenoid. Use of the second port is not necessary. Secondary ports, unlike primary ports, cannot be simply attached to a boost control line and require electronic or manual control to be useful. CO2 can also be used to apply pressure to the second port, to control boost on a much finer level.

Electric

Some 1940s aircraft engines featured electrically operated wastegates, such as the Wright R-1820 on the B-17 Flying Fortress. General Electric was the biggest manufacturer of these systems. Being before the age of computers, they were entirely analog. Pilots had a cockpit control to select different boost levels. Electric wastegates soon fell out of favor due to design philosophies which mandated the separation of the engine controls from the electrical system.

Beginning in November 2015[3] Honda Earth Dreams direct injected turbocharged engines with 1.5 litre displacement employ an ECU driven electric wastegate. This was first introduced in the Honda Civic 2016 model and followed by the CR-V in 2017. In 2018 1.5L and 2.0L turbocharged direct injected engines replaced the 2.4L and 3.6L 6 cylinder normally aspirated engines in the Honda Accord[4].

Hydraulic

Most modern turbocharged aircraft use a hydraulic wastegate control with engine oil as the fluid. Systems from Lycoming and Continental operate on the same principles and use similar parts which differ only in name. Inside the wastegate actuator, a spring acts to open the wastegate, and oil pressure acts to close the wastegate. On the oil output side of the wastegate actuator sits the density controller, an air-controlled oil valve which senses upper deck pressure and controls how fast oil can bleed from the wastegate actuator back to the engine. As the aircraft climbs and the air density drops, the density controller slowly closes the valve and traps more oil in the wastegate actuator, closing the wastegate to increase the speed of the turbocharger and maintain rated power. Some systems also use a differential pressure controller which senses the air pressures on either side of the throttle plate and adjusts the wastegate to maintain a set differential. This maintains an optimum balance between a low turbocharger workload and a quick spool-up time, and also prevents surging caused by a bootstrapping effect.

Wastegate sizing

Wastegate sizing is inversely proportional to the desired level of boost and is somewhat independent of the size or power of the engine. One vendor's guide for wastegate sizing is as follows:[5]

  • big turbo/low boost = bigger wastegate
  • big turbo/high boost = smaller wastegate
  • small turbo/low boost = bigger wastegate
  • small turbo/high boost = smaller wastegate

However, exhaust flow is an effect of power. So, another decision chart should look like this.

  • big turbo/small engine/small power = small wastegate
  • big turbo/small engine/big power = big wastegate
  • small turbo/small engine/small power = small wastegate
  • big turbo/big engine/ small power = medium wastegate
  • small turbo/big engine/any power level = big wastegate -->The reason for this is that the small turbine will easily try to overspin from excess exhaust gas volume.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD