Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 2.0 (Uri Tours).
The examples and perspective in this article deal primarily with the United States and do not represent a worldwide view of the subject. You may improve this article, discuss the issue on the talk page, or create a new article, as appropriate. (August 2014) (Learn how and when to remove this template message) |
A golf cart (called golf car in ANSI standard Z130.1, since "carts" are not self-propelled)[1] is a small vehicle designed originally to carry two golfers and their golf clubs around a golf course or on desert trails with less effort than walking.
Golf carts come in a wide range of formats and are more generally used to convey small numbers of passengers short distances at speeds less than 15 mph (24 km/h) per ANSI Standard z130.1 as originally manufactured. They are generally around 4 feet (1.2 m) wide × 8 feet (2.4 m) long × 6 feet (1.8 m) high and weigh 900 pounds (410 kg) to 1,000 pounds (450 kg). Most are powered by 4-stroke engines.
The price of a golf cart can range anywhere from under US$1,000 to well over US$20,000 per cart, depending on several factors. These factors may include whether or not a fleet of carts is being purchased for a golf course or a country club, for example, and whether the carts are new or used. Other factors may include options such as equipment requirements, and how many people the cart is meant to transport. With the rise in popularity of golf carts, many golf clubs or country clubs offer storage and energy options to golf cart owners. This has led to the modification of golf carts to suit use at a particular golf course. Typical modifications include windshields, ball cleaners, cooler trays, upgraded motor or speed controller (to increase speed and/or torque), and lift kits.
Originally golf carts were only electrically powered, but in time gasoline-powered variants appeared. The electric variety is now used in many communities where their lack of pollutants, lack of noise, and safety for pedestrians and other carts (due to slow speeds) are beneficial. When purpose-built for general transportation these are called Neighborhood Electric Vehicles (NEVs), but with various operating limitations such as top speed and heavy regulation on which type of streets these types of carts are permitted to be used. These may resemble the golf carts shown above, although some are now being made with all-weather car-like bodies.
The minimum age to drive a golf cart is 13 in Georgia, Alabama, California, Kansas, Kentucky, Rhode Island, Vermont, and South Carolina.[citation needed] Other US states, such as Florida,[2] have a minimum age of 14–15 years.
Reportedly, the first use of a motorized cart on a golf course was by JK Wadley of Texarkana, Texas/Arkansas, who saw a three-wheeled electric cart being used in Los Angeles to transport senior citizens to the grocery store. Later, he purchased a cart and found that it worked poorly on a golf course.[3] The first electric golf cart was custom-made in 1932, but did not gain widespread acceptance.[4] In the 1930s until the 1950s the most widespread use of golf carts was for those with disabilities who could not walk far.[5] By the mid 1950s the golf cart had gained wide acceptance with golfers, with several manufactures (e.g. Victor Adding Machine Co. and Sears Roebuck) producing various models. Most were electric.[6]
Merle Williams of Long Beach, California was an early innovator of the electric golf cart.[citation needed] He started with knowledge gained from production of electric cars due to World War II gasoline rationing. In 1951 his Marketeer Company began production of an electric golf cart in Redlands, California. E-Z-Go began producing golf cars in 1954, Cushman in 1955, Club Car in 1958, Taylor-Dunn in 1961, Harley-Davidson in 1963, Yamaha Golf Car in 1979 and CT&T in 2002.
Max Walker created the first gasoline-powered golf cart "The Walker Executive" in 1957.[citation needed] This three-wheeled vehicle was shaped with a Vespa-style front end and, like any golf cart, carried two passengers and golf bags.
In 1963 the Harley-Davidson Motor Company began producing golf carts. Over the years they manufactured and distributed thousands of three- and four-wheeled gasoline-powered and electric vehicles that are still highly sought after. The iconic three-wheeled cart, with either a steering wheel or a tiller-based steering control, boasted a reversible two-stroke engine similar to one used today in some high-end snowmobiles. (The engine runs clockwise in forward mode.) Harley Davidson sold the production of golf carts to American Machine and Foundry Company, who in turn sold production to Columbia Par Car. Many of these gems survive today, and are the prized possessions of proud owners, restorers, and collectors worldwide.
New technology such as the SoloRider, an adaptive golf cart designed for a single user, is allowing disabled persons access to the golf course and the game itself. The cart’s seat swivels around, extends to an upright position, and allows the golfer to stand upright, be supported, and swing using both hands.[7][8]
Golf carts are now taking on an extreme nature, being highly modified from their original configuration to perform similar to the growing popularity of the Side by Side (UTV). Modifications as minor as suspension upgrades are commonplace, while entire redesigns may include axles and an engine from a full size automobile. Solar-powered golf carts are an alternative to gas or regular charged electric golf cart. While this technology is still new and not as efficient as gas or electric, it is becoming more and more popular. In 2014, citEcar built and tested a solar-powered street-legal golf cart that will travel 105 miles on a single charge.[9]
One of the most recent developments in golf cart technology is the GolfBoard, a golf cart that is inspired by the skateboard. The GolfBoard is driven by front and back gear boxes providing power to all four wheels. The golfer controls the cart in a standing upright position as if riding skateboard, leaning left or right to make turns. The GolfBoard has been well received by the golfing community, as it speeds up play and, according to the manufacturers, has up to 75% less impact on turf than traditional golf carts. In 2014 the GolfBoard was voted the Best New Product at the PGA Show.[10]
Peachtree City, Georgia has many miles of golf cart paths that link the city together. Golf cart travel is used by a great majority of the community, especially among high school students. McIntosh High School even has a student golf cart parking lot on campus.
On islands (such as Santa Catalina Island, California, Bald Head Island, North Captiva Island, North Carolina, and Hamilton Island), motor vehicles are sometimes restricted and residents use golf carts instead.
The Villages, Florida, a retirement community of over 70,000 people, has an extensive golf cart trail system (estimated at around 100 miles (160 km)) and also allows golf carts on many streets. It is the most popular form of transportation in this community.
On the tropical islands of Belize golf carts are a major form of road transport and can be rented by tourists.
The residential community of Discovery Bay, Hong Kong does not allow the use of private vehicles apart from a fleet of 520 golf carts (excluding the ones operating exclusively in the Golf or the Marina Clubs). The remainder of the 20,000 residents rely on a mixture of shuttle buses and hire cars to travel around the township.
The Palm Springs Area in California contains multiple golf cart communities including PGA West, The Madison Club, The Hideaway, and many other golf course/golf cart communities. The PGA Tour is held at PGA West every January.
Along with the rising frequency of golf cart crashes, the number of golf-cart-related injuries has increased significantly over the last decade. A study conducted by researchers in the Center for Injury Research and Policy of The Research Institute at the Nationwide Children's Hospital found that the number of golf cart-related injuries rose 132% during the 17-year study period. According to the study, published in the July 2008 issue of the American Journal of Preventive Medicine, there were an estimated 148,000 golf cart-related injuries between 1990 and 2006, ranging from an estimated 5,770 cases in 1990 to approximately 13,411 cases in 2006. More than 30% of golf cart-related injuries involved children under the age of 16.[11]
The most common type of injury was soft tissue damage, usually just bruises, followed by fractures, constituting 22.3% of the cases, and lacerations, accounting for 15.5% of injuries.[12] Other types of injuries include concussions, internal injuries, subdural hematoma, spinal cord injury, or acute respiratory compromise. While rare, a few cases had severe outcomes: 4 fatalities, 2 paraplegic, and 1 quadriplegic injuries have been documented.[13]
Some of the main causes of injury related to golf cart accidents included cart overturn, falling/jumping from a moving golf cart, collision with another vehicle or stationary object, struck/run over by a cart, getting into or out of a moving cart. Out of all these, "falling or jumping from a golf cart" was the most common cause of injury for both adults and children.[12]
One contributing reason is that current golf cart safety features are insufficient to prevent passenger falls or ejection.[14] Golf carts moving at speeds as low as 11 miles per hour (18 km/h) could readily eject a passenger during a turn. Furthermore, rear-facing golf cart seats are associated with high rates of passenger ejection during fast acceleration, and most standard (stock) golf carts do not have brakes on all four wheels (typically brakes are only on the rear wheels, thus sharply limiting their braking power).[12][15]
Golf cart injuries are also commonly found in desert areas (e.g. Johnson Valley, California). Driving golf carts on bumpy dirt trails, along cliffs, down rocky trails that should only be traversed using 4-wheel-drive vehicles, can all lead to injuries.
Arizona has a large snowbird population, and many of them live in large RV parks or retirement communities that use golf carts to get around. In 2014, Arizona Governor Jan Brewer signed a law permitting golf cart drivers to drive as close to the right-hand edge of the roadway as possible. Prior to the passage of the law, golf cart drivers received traffic tickets for failing to drive in the center of the roadway. Complementing the new law, a golf cart safety education program was initiated.[16]
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer, Bus