powered by CADENAS

Social Share

Amazon

Miniature wargaming (9639 views - Game & Play & Gamification)

Miniature wargaming is a form of wargaming in which players enact battles between opposing military forces that are represented by miniature physical models. The use of physical models to represent military units is in contrast to other tabletop wargames that use abstract pieces such as counters or blocks, or computer wargames which use virtual models. The primary benefit of using models is aesthetics, though in certain wargames the size and shape of the models can have practical consequences on how the match plays out.
Go to Article

Explanation by Hotspot Model

Youtube


    

Miniature wargaming

Miniature wargaming

Miniature wargaming

Licensed under Creative Commons Attribution-Share Alike 4.0 (Allan Wright).

Miniature wargaming is a form of wargaming in which players enact battles between opposing military forces that are represented by miniature physical models. The use of physical models to represent military units is in contrast to other tabletop wargames that use abstract pieces such as counters or blocks, or computer wargames which use virtual models. The primary benefit of using models is aesthetics, though in certain wargames the size and shape of the models can have practical consequences on how the match plays out.

Overview

A miniature wargame is played with miniature models of soldiers, artillery, and vehicles on a model of a battlefield. The primary benefit of using models as opposed to abstract pieces is primarily an aesthetic one. Models offer a visually-pleasing way of identifying the units on the battlefield. In most miniature wargame systems, the model itself may be irrelevant as far as the rules are concerned; what really matters is the dimensions of the base that the model is mounted on. Distances between infantry units are measured from the base of the model.[1] The exception to this trend may be models of vehicles such as tanks, which do not require a base to be stable and have naturally rectangular shapes; in such cases, the distances between units may be measured from the edge of the model itself. Some miniature wargames use the dimensions of the model do determine whether a target behind cover is within line-of-fire of an attacker.

Most miniature wargames are turn-based. Players take turns to move their model warriors across the model battlefield and declare attacks on the opponent. In most miniature wargames, the outcomes of fights between units are resolved through simple arithmetic, sometimes combined with dice rolls or playing cards.

All wargames have a setting that is based on some historical era of warfare. The setting determines what kind of units the players can deploy in their match. For instance, a wargame set in the Napoleonic Wars should use models of Napoleonic-era soldiers, wielding muskets and cannons, and not spears or automatic rifles. A fantasy wargame has a fictional setting and may thus feature fictional or anachronistic armaments, but the setting should be similar enough to some real historical era of warfare so as to preserve a reasonable degree of realism.[2] For instance, Warhammer Age of Sigmar is mostly based on medieval warfare, but includes supernatural elements such as wizards and dragons. The most popular historical settings are World War 2, the Napoleonic Wars, and the American Civil War (in that order).[3] The most popular fantasy setting is Warhammer 40,000.[4][5]

Miniature wargames are played either at the skirmish level or the tactical level. At the skirmish level, the player controls his warriors individually, whereas in a tactical level game he controls groups of warriors—typically the model warriors are mounted in groups on the same base. Miniature wargames are not played at the strategic or operational level because at that scale the models would become imperceptibly tiny.

Miniature wargames are generally played for recreation, as the physical limitations of the medium prevents it from representing modern warfare accurately enough for use in military instruction and research.

Models

Plastic wargaming models are usually sold unpainted and attached to their sprues. Players are expected to cut them out, glue them together, and paint them. Scale is frequently specified by the height of the eyes, since hats often conceal the crown of the head.[6]

Historically, these models were commonly made of tin or lead, but nowadays they are often made of polystyrene or resin. Plastic models are cheaper to mass-produce but require a larger investment because they require expensive steel molds. Lead and tin models, by contrast, can be cast in cheap rubber molds. Larger firms such as Games Workshop prefer to produce plastic models, whereas smaller firms with less money prefer metal models.[7]

Wargaming figurines often come with unrealistic body proportions. Their hands may be oversized, or their rifles excessively thick. One reason for this is to make the models more robust: thicker parts are less likely to bend or break. Another reason is that manufacturing methods often stipulate a minimum thickness for casting (molten plastic has difficulty flowing through thin channels in the mold). Finally, odd proportions may actually make the model look better for its size by accentuating certain features that the human eye focuses on.[8]

Assembly and painting

Wargaming models are often sold in parts. In the case of plastic models, they're often sold still affixed to their sprues. The player is expected to cut out the parts and glue them together. This is the norm because, depending on the design of the model, it may not be possible to mold it whole, and selling the parts un-assembled saves on labor costs. After assembling the model, the player should then paint it to make it more presentable and easier to identify. Understandably, the time and skill involved in assembling and painting models deters many people from miniature wargaming. Some firms have tried to address this by selling pre-assembled and pre-painted models, but these are rare because, with current technologies, it's hard to mass-produce ready-to-play miniatures that are both cheap and match the beauty of hand-painted models.[9] The other options for players are to buy finished models second-hand or hire a professional painter.

Proprietary models vs generic models

Historical miniature wargames are typically designed to use generic models. It's generally not possible to copyright the look of a historical soldier. Anyone, for instance, may freely produce miniature models of Napoleonic infantrymen. A player of a Napoleonic-era wargame could thus obtain his models from any manufacturer who produces Napoleonic models at the requisite scale. Consequently, it's difficult if not impossible for a historical wargame designer to oblige players to buy models from a certain manufacturer.

By contrast, fantasy wargames feature fictional warriors, and fictional characters can be copyrighted. By incorporating original characters into his wargame, a wargame designer can oblige the player to purchase his models from a specific manufacturer who is licensed to produce the requisite models. An example of this Warhammer 40,000. Warhammer 40,000 features many original characters who have a distinctive aesthetic, and Games Workshop and its subsidiaries reserve the exclusive right to manufacture models of these characters. Games Workshop models tend to be expensive because competing manufacturers are not allowed to offer cheaper copies of official Warhammer 40,000 models. While there's nothing to stop players using foreign wargaming models (generics or proprietary models from other wargames), doing so could spoil the aesthetic and cause confusion.

The battlefield

A miniature wargame is played on a model of a battlefield. The model battlefield is usually mounted on a table. As far as size goes, every part of the battlefield should be within arm's reach of the players—a width of four feet is recommended.[10][11][12]

Most miniature wargames are written to allow players to design their own battlefields, as opposed to board wargames which are often tied to a pre-set layout. For this, players prefer to use modular terrain kits that permit easy customization.

Historical wargamers sometimes re-enact historical battles, but this is rare. Players more often prefer to design their own scenarios. The first advantage is that they can design a scenario that fits the resources they have at hand, whereas reconstructing a historical battle may require them to purchase additional models and rulebooks, and perhaps a larger gaming table. The second advantage is that a fictional scenario can be designed such that either player has a fair chance of winning.[13]

Mininature wargames are rarely set in urban environments. The first reason is that it's harder to reach models when there are lots of buildings in the way. Another reason is that the buildings may highlight the abstract scale at which the wargame operates. For instance, in the 28mm wargame Bolt Action, a rifle's range is 24 inches, which is barely the length of a few houses at 28mm scale. If placed in an urban environment, a rifleman would not be able to hit a target at the far end of a small street, which makes no intuitive sense and thus shatters the illusion of realism.[14]

Scale

Model size

The scale of a model vehicle can be expressed as a scale ratio. A scale ratio of 1:100 means that 1cm represents 100cm; at this scale, if a model car is 4.5cm long, then it represents a real car that is 4.5m long.

When it comes to figurines of humans, the preferred method of expressing scale is the height of a figurine in millimeters. There is no standardized system of measuring figurine size in the wargaming hobby. Some manufacturers measure the height of a figurine up to the crown of the head, whereas others may measure it up to the eyes (the latter is more sensible if the figurine is wearing a hat).[15] Furthermore, the advertised scale of a model may not reflect its actual scale. In order to make their products stand out against their competitors, some manufacturers make their models a little oversized, e.g. a model from a certain manufacturer that is advertised as suitable for 28mm wargames could actually be 30mm tall in practice. This makes the model look more imposing, and allows for more detail.[16]

Manufacturers of generic wargaming models are generally obliged to build their models to some standard scale so as to ensure compatibility with third-party wargames. Manufacturers who make proprietary models designed exclusively for use in a specific wargame do not have this concern. For instance, Warhammer 40,000 officially does not have a scale. It doesn't need to conform to a standard scale, because Games Workshop is the exclusive manufacturer of official Warhammer 40,000 models, said models are intended exclusively for use in Warhammer 40,000, and Games Workshop doesn't want players using foreign models from other manufacturers.

Figurine sizes and roughly equivalent scale ratios[a]
mm 90 54 45 28 25 20 15 6 2
scale 1:20 1:33 1:40 1:64 1:71 1:89 1:120 1:300 1:890

Abstract scaling

Most miniature wargames do not have an absolute scale, i.e. where the figurines, terrain, movement and firing ranges all conform to single scale ratio. This is largely because of the need to compress the battle into the confined space of a table surface. Instead, miniature wargames prefer to use abstract scaling.

For example, a 28mm model rifleman realistically ought to be able to hit a target from over 23 feet away,[b] but this is larger than most tables. A miniature wargame would not be much fun if the models could shoot each other from opposite ends of the table, and thus not have to maneuver around the battlefield. The 28mmm wargame Bolt Action solves this problem by compressing the range of a rifle to just 24 inches;[17] a sub-machine gun's range is 12 inches and a pistol's range is 6 inches.[18] These ranges may not be realistic, but their proportions do make intuitive sense, giving an illusion of realism.

Abstract scaling may also be applied to terrain features, e.g. model houses and trees may be a little undersized compared the model warriors so as to make more room on the table for the warriors.

Time

Most miniature wargames do not have a fixed time scale (i.e. how many seconds a turn represents). Most wargame rulebooks instead prefer to define how far a unit can move in a turn, and this movement range is proportioned to the size of a typical game table. For example, Bolt Action sets a movement range of six inches in a turn for most units.

Rulesets

There are many miniature wargaming rulesets, not all of which are currently in print, including some which are available free on the internet; many gamers also write their own, creating so-called "house rules" or "club sets". Most rulesets are intended for a specific historical period or fictional genre. Rules also vary in the model scale they use: one infantry figure may represent one man, one squad, or much larger numbers of actual troops.

Wargaming in general owes its origins to military simulations, most famously to the Prussian staff training system Kriegsspiel. Consequently, rules designers struggle with the perceived obligation to actually 'simulate' something, and with the seldom compatible necessity to make an enjoyable 'game'. Historical battles were seldom fair or even, and the potential detail that can be brought to bear to represent this in a set of rules always comes at the cost of pace of the game and enjoyment. In Osprey Publishing's book about the Battle of Crécy, from its series on historical campaigns, there is included a detailed section on wargaming the battle, in which Stuart Asquith writes:

When refighting a particular battle, it is important to adhere as closely as possible to the original historical engagement. The counter-argument is that the wargamer(s) know who is going to win. Fair comment, but knowing the outcome of any battle does not usually prevent one from reading about that action, so why should such knowledge debar a refight?[19]

He adds that unless at least the initial moves are recreated, "then an interesting medieval battle may well take place, but it will not be a re-creation of Crécy."[19] Still, rules aimed at the non-professional hobby market therefore inevitably contain abstractions. It is generally in the area of the abstraction liberties taken by the designers that the differences between rules can be found. Most follow tried and true conventions to the extent that a chess player would recognize wargaming merely as a different scaled version of his or her own game.

Role-playing games

During the 1960s and 1970s, two new trends in wargaming emerged: First were small-unit rules sets which allowed individual players to portray small units down to even a single figure. These rules expanded the abilities of the smaller units accordingly, to magnify their effect on the overall battle.

Second was an interest in fantasy miniatures wargaming. J.R.R. Tolkien's novel The Hobbit and his epic cycle The Lord of the Rings were gaining strong interest in the United States, and as a result, rules were quickly developed to play medieval and Roman-era wargames, where these eras had previously been largely ignored in favor of Napoleonic and American Civil War gaming.

The two converged in a set of miniatures rules entitled Chainmail, published by a tiny company called Guidon Games, headquartered in Lake Geneva, Wisconsin. Later, in 1974, TSR designer E. Gary Gygax wrote a set of rules for individual characters under Chainmail, and entitled it Dungeons & Dragons. Further developments ensued, and the role-playing game hobby quickly became distinct from the wargaming hobby which preceded it.

Naval wargames

Although generally less popular than wargames set on land, naval wargaming nevertheless enjoys a degree of support around the world. Model ships have long been used for wargaming, but it was the introduction of elaborate rules in the early 20th century that made the hobby more popular. Small miniature ships, often in 1:1200 scale and 1:1250 scale, were maneuvered on large playing surfaces to recreate historical battles. Prior to World War II, firms such as Bassett-Lowke in England and the German company Wiking marketed these to the public.[20][21] After World War II, several manufacturers started business in Germany, which remains the center of production to this day,[22] while other companies started in England and the United States.

Rules can vary greatly between game systems; both in complexity and era. Historical rulesets range from the ancient and medieval ships to the fleets of the Age of Sail and the modern era. Often the hobbyists have to provide their own models of ships. The 1972 game, Don't Give Up The Ship!, called for pencil and paper, six-sided dice, rulers and protractors, and model ships, ideally of 1:1200 scale. The elaborate rules cover morale, sinking, fires, broken masts, and boarding. Dice determined wind speed and direction, and hence the ship's speed and the use of its cannon by measuring angles with the protractor.[23]

In naval wargaming of the modern period, General Quarters, primarily (though not exclusively) using six-sided dice, has established itself as one of the leading sets of World War I and II era rules.[24]

Some land-based miniature wargames have also been adapted to naval wargaming. All at Sea, for example, is an adaptation of The Lord of the Rings Strategy Battle Game rules for naval conflicts. The game's mechanics centered around boarding parties, with options for ramming actions and siege engines.[25] As such, the ship's scale ratio corresponds to the 25 mm scale miniatures used by The Lord of the Rings. Model ships are built by hobbyists, just as normal miniature terrain, such as "great ships" of Pelargir, cogs of Dol Amroth and Corsair galleys.[26]

Air wargames

Air wargaming, like naval wargaming, is a smaller niche within the larger hobby of miniatures wargaming. Aerial combat has developed over a relatively short time compared with naval or land warfare. As such, air wargaming tends to break down into three broad periods:

  • World War I – from the earliest air combat to the 1920s
  • World War II – 1930s to the early 1950s
  • "Modern" – the missile age

In addition there are science fiction and "alternative history" games such as Aeronefs and those in the Crimson Skies universe.

History

Precursors

Wargaming was invented in Prussia, primarily as a means of teaching strategy and tactics to military officers, though many people played them for fun as well. The first wargame was invented by Johann Christian Ludwig Hellwig in 1780. It was variation of chess, but wherein the pieces represented real army units, such as infantry, cavalry, and artillery. The pieces had limited ranges of movement, and infantry and artillery could kill an enemy at a distance. Like chess, it was played on a grid of squares, but the squares were color-coded to represent different types of terrain, and the battlefield was customizable. Inspired by Hellwig's game, other German designers created more realistic wargames, adding innovations such as realistic maps, free-form unit movement, dice rolls, and probability tables. Eventually, the Prussian military embraced wargaming as a training tool for its officers. After Prussia defeated France in the Franco-Prussian War (1870), wargaming spread around the world. German wargames were referred to as Kriegsspiel, which literally means "war game" in German.

German wargames didn't use realistic miniature models to represent the units nor terrain. Instead, they used abstract pieces such as little wooden blocks, or chess-like statuettes.

Birth

In 1881, the English writer Robert Louis Stevenson became the first documented person to use toy soldiers in a wargame, and thus he might be the inventor of miniature wargaming. Stevenson never published his rules, but according to an account by his stepson, they were very sophisticated and realistic, on par with German military wargames. Stevenson played his wargame on the floor, on a map drawn with chalk.[27]

In 1898, the British writer Fred T. Jane published the first rulebook for a naval wargame: Rules for the Jane Naval War Game. Jane's wargame was also the first published wargame to use miniature models. It used models of warships made out of cork and wires; the wires were used for guns and masts. Jane's rulebook described in great detail the capabilities of the warships, such as the range and armor-penetrating power of the guns. It also simulated localized damage, such as what would happen to a warship if its boiler was damaged, or its gun battery.

The English writer H. G. Wells developed his own codified rules for playing with toy soldiers, which he published in a book titled Little Wars (1913). This is widely remembered as the first rulebook for miniature wargaming (for terrestrial armies, at least). Little Wars had very simple rules to make it fun and accessible to anyone. Little Wars did not use dice or computation to resolve fights. For artillery attacks, players used spring-loaded toy cannons which fired little wooden cylinders to physically knock over enemy models. As for infantry and cavalry, they could only engage in hand-to-hand combat (even if the figurines exhibited firearms). When two infantry units fought in close quarters, the units would suffer non-random losses determined by their relative sizes. Little Wars was designed for a large field of play, such as a lawn or the floor of a large room, because the toy soldiers available to wells were too large for tabletop play. An infantryman could move up to one foot per turn, and a cavalryman could move up to two feet per turn. To measure these distances, players used a two-foot long piece of string. Wells was also the first wargamer to use models of buildings, trees, and other terrain features to create a three-dimensional battlefield.[28]

Wells' rulebook was for a long time regarded as the standard system by which other miniature wargames were judged. However, the nascent miniature wargaming community would remain very small for a long time to come. A possible reason was the two World Wars, which de-glamorized war and caused shortages of tin and lead that made model soldiers expensive.[29][30] Another reason may have been the lack of magazines or clubs dedicated to miniature wargames. Miniature wargaming was seen as a niche within the larger hobby of making and collecting model soldiers.

Post-War growth

In 1955, a California man named Jack Scruby began making inexpensive miniature models for miniature wargames out of type metal. Scruby's major contribution to the miniature wargaming hobby was to network players across America and the UK. At the time, the miniature wargaming community was miniscule, and players struggled to find each other. In 1956, Scruby organized the first miniature wargaming convention in America, which was attended by just fourteen people. From 1957 to 1962, he self-published the world's first miniature wargaming magazine, titled The War Game Digest, through which wargamers could publish their rules and share game reports. It had less than two hundred subscribers, but it did establish a community that kept growing.[31]

Around the same time in the United Kingdom, Donald Featherstone began writing an influential series of books on wargaming, which represented the first mainstream published contribution to wargaming since Little Wars. Titles included : War Games (1962), Advanced Wargames, Solo Wargaming, Wargame Campaigns, Battles with Model Tanks, Skirmish Wargaming. Such was the popularity of such titles that other authors were able to have published wargaming titles. This output of published wargaming titles from British authors coupled with the emergence at the same time of several manufacturers providing suitable wargame miniatures (e.g. Miniature Figurines, Hinchliffe, Peter Laing, Garrisson, Skytrex, Davco, Heroic & Ros) was responsible for the huge upsurge of popularity of the hobby in the late 1960s and into the 1970s.[32]

In 1956, Tony Bath published what was the first ruleset for a miniature wargame set in the medieval period. In 1971, Gary Gygax developed a his own miniature wargame system for medieval warfare called Chainmail. Gygax later produced a supplement for Chainmail that added magic and fantasy creatures, making this the first fantasy miniature wargame. This supplement was inspired by the growing popularity of the Lord of the Rings novels by J. R. R. Tolkien.

Gygax later went on to develop the first tabletop role-playing game: Dungeons and Dragons. Dungeons and Dragons was a story-driven game, but adapted wargaming rules to model the fights players could get in. Battles in Dungeons and Dragons rarely featured more than a dozen combatants, so the combat rules were designed to model the capabilities of the warriors in very great detail. Strictly speaking, Dungeons and Dragons did not require miniature models to play, but many players found that using miniature models made the fights easier to arbitrate and more immersive.

Commercial wargames with proprietary models

In 1983, a British company called Games Workshop released a fantasy miniature wargame called Warhammer,[c] which was the first miniature wargame designed to use proprietary models. Games Workshop at the time made miniature models for use in Dungeons and Dragons. Warhammer was meant to encourage customers to buy more of these models. Whereas miniature models were optional in Dungeons and Dragons, Warhammer mandated their use and the battles tended to be larger.[33] Initially, Warhammer had a threadbare fictional setting and used generic stock characters common to fantasy fiction, but as time went on, Games Workshop expanded the setting with original characters with distinctive visual designs. Games Workshop's official line of models for Warhammer eventually took on such a distinctive look that rival manufacturers could not produce similar-looking models without risking a lawsuit over copyright infringement. Although there was nothing to stop players of Warhammer from using foreign models from third-party manufacturers, doing so could spoil the aesthetic and cause confusion.

In 1987, Games Workshop released a fantasy miniature wargame called Warhammer 40,000, which was a science-fiction spinoff of Warhammer. Like Warhammer, Warhammer 40,000 obliged players to buy proprietary models from Games Workshop. Warhammer 40,000 became even more successful than Warhammer. The success of the Warhammer games promoted the sales of Games Workshop's line of gaming models.

Other gaming companies sought to emulate Games Workshop's business model. Examples include Fantasy Flight Games, Privateer Press, and Warlord Games, all of which have released their own miniature wargame systems that were designed to promote sales of their respective lines of proprietary gaming models. This business model has proven lucrative, and thanks to the marketing resources of these companies, fantasy wargames have displaced historical wargames in popularity.

Community and culture

Players of miniature wargames tend to be more extroverted than players of board wargames and computer wargames.[34][35] Players of miniature wargames are obliged meet in each other in person and play in the same room around a table whereas board wargames can be played via correspondence and computer wargames can be played online, therefore miniature wargaming places a premium on sociability.

Consequently, conventions and clubs are important to the wargaming community. Some conventions have become very large affairs, such as Gen-Con, Origins and Historical Miniatures Gaming Society's Historicon, called the "mother of all wargaming conventions".[35] Players also tend to be middle-aged or older. One reason is that the hobby is expensive and older people tend to be wealthier.

Notable organizations

  • International Wargames Federation (IWF) promotes historical wargaming competitions between players or teams from different countries. [1]
  • Johnny Reb Gaming Society – the leading international gaming society devoted exclusively to wargaming the American Civil War; publishes the quarterly CHARGE! newsletter for members of the society.
  • Wargame Developments (WD) was founded by game designer and author Paddy Griffith in 1980, and is an international group dedicated to developing all types of wargames. It publishes a journal, The Nugget, nine times per year and holds an annual 3-day long conference – COW (The Conference of Wargamers) – every July.
  • Historical Miniatures Gaming Society (HMGS) - HMGS, Inc. is a non-profit, charitable and educational 501(c)3 organization whose purpose is to promote the study of military history through the art of tabletop miniature wargaming. HMGS holds several of the largest wargaming conventions in the United States annually.
  • Mind Sports South Africa started as the South African Wargames Union in 1984. It was the first wargaming body to have wargames recognized as a sport in the same way as which chess is so recognized. As a result, South African teams were awarded Springbok Colours (1991–1994) and Protea Colours (1995 to date).
  • The Solo Wargamers Association (SWA) founded in 1976 supports solo players in all branches of wargaming – historical, science fiction, fantasy, miniatures, board games etc. Publishes a quarterly journal Lone Warrior.
  • The British Historical Games Society (BHGS) promotes historical wargaming in Britain, holding events including tournaments periodically.
  • The War Gaming Society (WGS) was founded in May 1975. The Joaquin Valley War Gaming Association (SJVWGA), founded in 1972 by Jack Scruby, Ray Jackson and other miniature wargamers, is a subdivision of the War Gaming Society.
  • The Pike & Shot Society promotes wargaming based on the "Pike and shot" period (c. 1500–1700), publishing a journal called The Arquebusier. [2]
  • The Society of Ancients, founded in the '60s, promoting ancient wargaming and historical research through Slingshot, the society journal.
  • Warhammer Player's Society. Dedicated to all versions (Fantasy, Ancients and Science-Fiction) of Warhammer [3]
  • Society of Twentieth Century Wargamers. (SOTCW) covers all periods 1900 – present [land, sea or air] the society has a magazine, The Journal, which is produced quarterly. [4]
  • Society of Fantasy and Science Fiction Wargamers (SFSFW). For fantastical and future, including retro-future, wargames. Publishers of Ragnarok magazine. [5]
  • Naval Wargames Society. The NWS is an international society devoted to the advancement of naval wargames, publishing a quarterly journal, Battlefleet. [6]

Notable wargamers and designers

  • H.G. Wells – Known as the "Father of Miniature Wargaming" and author of the miniature wargaming classic Little Wars.[36]
  • Jack Scruby – The "Father of Modern Miniature Wargaming".[37] Popularized modern miniature wargaming and organized perhaps the first miniatures convention in 1956. Jack Scruby was also a manufacturer of military miniatures whose efforts led to a rebirth of the miniature wargaming hobby in the late 1950s.
  • Gary Gygax – Co-creator of Dungeons & Dragons and a number of miniature wargames.
  • Dave Arneson – Co-creator of Dungeons & Dragons
  • MAR Barker -Creator of Tekumel: Empire of the Petal Throne, professor, linguist, and author.
  • Peter Cushing -Actor, and star of films.
  • Duke Seifried – Sculptor of over 10,000 miniatures, one of the earliest American miniature manufacturers: Heritage, Custom Cast, Der Kreigspielers Napoleonic, and Fantastiques Fantasy Figures.
  • Bruce Rea Taylor - Designer of the Firefly, Challenger, Corps Commander and Korps Commander rules.
  • Charles Grant – Author and founder member of the UK wargaming scene in the 1960s. Helped popularize miniature wargaming.
  • Donald Featherstone – A respected military historian,[38] introduced to the hobby in 1955.[39] Since then, he was one of the most prolific authors on the subject, and very influential in the development of the hobby.
  • Fletcher Pratt – Science fiction writer (often in collaboration with L. Sprague de Camp) and originator of a popular set of rules for naval miniature wargaming.
  • Kevin Cabai-Armor Officer and wagamer- Kevin has used in many years in the Armor Branch to write a number of highly realistic and yet playable rules sets. His first Jagdpanzer- cover mechanized combat in World War II. The game was first seen at major conventions in 1985. It has been though a revised 2nd edition and is widely available. Sand Oil and Blood- was co-authored, with Marty Fenelon. It was the modern warfare version of tank combat. Already in the works to be published during Desert Shield, it was released 30 days after Desert Storm. Finally Mekong- A rule set covering Riverine Warfare in Viet Nam. Again co-authored with Marty Fenelon, it was picked up and sold by GHQ.
  • Terry Wise- Historian and writer- many Osprey publications to his credit along with the seminal "Introduction to Battlegaming" of 1969. Published rules for Ancients, Pike and Shot and American Civil wargaming that are fast, fun and easy to use.
  • Walter ("Wally") Simon – One of the original founders of the Historical Miniature Gaming Society. First President of HMGS and Organizer of the Potomac Wargamers, publisher of the PW Review.
  • Dick Bryant – Co-founder with Wally Simon of HMGS and editor since 1969 of The Courier Miniature Wargaming Magazine. His editorial in that magazine castigating GAMA for choosing cardboard counters as "The Best New Historical Miniature" started the search for an organization that supported and promulgated the hobby of Historical Miniature Wargaming that resulted in the "Meeting in Wally's Basement" that was the initialization of HMGS.
  • David Waxtel – Publisher of over 20 sets of rules, and supplement books.
  • George Gush – Noted for A Guide to Wargaming (1980) as well as the WRG Renaissance Rules
  • John Hill – Known for his classic Squad Leader and other Avalon Hill board games, also the author of the popular Johnny Reb miniatures rules.
  • Raymond ("Ray") James Jackson – Author of Classic Napoleonics, an "Old School" set of miniature wargame rules which have been in existence since 1961. Chairman and CEO of both HMGS-West and the War Gaming Society. A miniature wargamer since 1958.
  • Frank Chadwick – Author of the Command Decision and Volley & Bayonet rules, Space: 1889 and Traveller, and co-founder of Game Designers' Workshop.
  • Phil Barker – Founder of the Wargames Research Group, and inventor of the De Bellis Antiquitatis game series.
  • Arty Conliffe – Designer of Armati, Crossfire, Spearhead, Shako and Tactica rules.
  • Bob Jones – Founder of Piquet and designer of the Piquet wargame series.
  • Brigadier Peter Young, DSO, MC – Highly decorated World War II commando leader, commander of the 9th Regiment of the Arab Legion, founder of the Sealed Knot English Civil War reenactment society, Reader of Military History at Sandhurst, author of several books on military history, also author of Charge! Or How to Play Wargames and The War Game: Ten Great Battles Recreated from History.
  • Phil Dunn – Founder of the Naval Wargames Society and author of Sea Battle Games.
  • John McEwan – Creator of the first science fiction ground combat miniatures game Starguard! in 1974 along with over 200 figures and models for this game.
  • Tony Bath – Author and veteran wargamer, founding member of the Society of Ancients, best known as umpire of one of the longest running and well known of all wargames campaigns, set in the fictional land of Hyboria.
  • David Manley – Author of many sets of naval rules including Action Stations, Fire When Ready, Iron and Fire, Bulldogs Away, and Form Line of Battle, as well as numerous articles and technical papers on naval wargaming, history, and warship design.
  • Scott Mingus – founder of the international Johnny Reb Gaming Society and one of the world's most prolific authors of American Civil War scenario books.
  • Neville Dickinson – One of the original members of the UK wargaming scene and founder of Miniature Figurines, the first firm in the UK to popularize metal miniatures.
  • Larry Brom - designer of The Sword and The Flame, one of the most popular colonial era wargames.
  • Andy Chambers – Known for his work in rules design and revision for Games Workshop Inc. and Mongoose Publishing. Notable games he helped develop include Warhammer 40,000 and Starship Troopers: The Miniatures Game.
  • Bryan Ansell - Creator of Laserburn, Rules with No Name, co-creator/co-author of Warhammer, author Warhammer 40,000 and a host of other game credits. Associated primarily with Games Workshop and Citade Miniatures, also Asgard Miniatures
  • Rick Priestley – co-creator/co-author of Warhammer, author Warhammer 40,000 and a host of other game credits. Associated primarily with Games Workshop and Citadel but earlier work included co-authoring the seminal fantasy wargame rulebook Reaper.
  • Rusty Gronewold – Lead designer with Tactical Command Games, has developed many different miniature games, such as Stellar Fire, Legions Unleashed, Conflict 2000, Stellar Conflicts & Uprisings, Gunslingers & Desperados, Pirates & Buccaneers just to name a few.
  • Paddy Griffith - Military historian and founder of Wargame Developments, he devised and ran the first Megagames as well as many experimental wargames that were designed to give military historians a greater insight into how battles and campaigns were actually fought. Many of his wargames posed ethical and moral dilemmas for the players and challenged orthodox thinking.
  • Alessio Cavatore - Writer of many popular rulesets. Famous for his work with Games Workshop, Mantic and Warlord.

See also


ТузActionПостапокалиптикаАркадный автоматArcade gameДополненная реальностьАватар (картинка)Baby walkerКороткие нардыБеспедальный велосипедBaoding ballsМеч с корзинчатой гардойКоролевская битва (жанр компьютерных игр)Слон (шахматы)Card countingКарточная играКарусельКазиноКолонизаторы (настольная игра)Шахматные часыЧетыре в рядДартсИгральная костьКукольный домикДоминоEdge sortingСпиннерFirst-person (gaming)Шутер от первого лицаFortniteИграGame boyИгровой контроллерИгровой движокГеймпадGameplay of PokémonГеймерGaming houseИгровая клавиатураGoogle CardboardHalo 3: ODSTКомната смехаImmersive technologyJob SimulatorДжойстикКороль (шахматы)Конь (шахматы)Lego DuploМинифигурка ЛегоLightning McQueenОружие и доспехи в литературеList of most-played video games by player countMagic: The GatheringМассовая многопользовательская ролевая онлайн-играМатрёшкаМетро 2033Метро 2033 (игра)Mini 4WDМонополия (игра)Monopoly video gamesМногопользовательская играОригамиOVAПешкаПинболИгровой персонажPvPPlayerUnknown’s BattlegroundsДетская площадкаПокемонПокерPortalГоловоломкаФерзьЖелезнодорожный моделизмЗагадкаЛошадь-качалкаЛадья (шахматы)Кубик РубикаШутерСлот-машинаСнукерКубики сомаSpinning coneSquishiesStress ballSuper MarioSurvival horrorТанграмПлюшевый мишкаТетрисХанойская башняИгрушкаКубики (игрушка)Игрушечный поездTransformers DecepticonsИгровая приставкаВиртуальный мирWarhammer 40,000Wooden toy trainWorld of WarcraftYukikazeMiniature model (gaming)ВаргеймНастольная играМех (BattleTech)BattleTechШестиугольная карта

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Game & Play & Gamification

3d,model,playground,board games,computer,strategy,thinktank