powered by CADENAS

Social Share

Amazon

Pocketbike racing (637 views - Cars & Motorbikes & Trucks & Buse)

Pocket Bike racing, also known as Minimoto or circus racing, is a category of racing where miniature racing motorcycles (known as pocket bikes or minimoto) are raced around kart tracks. A typical minimoto is approximately one-quarter the size of a regular motorcycle, and is powered by a two-stroke internal combustion engine of between 40–50 cc producing somewhere between 2.4 and 17 hp (1.8 and 11 kW). The machines have no suspension, relying on the tires to absorb bumps and handle cornering, and weigh approximately 50 lb (23 kg). The entry-level models produce about 2.4–4.2 hp, but the more expensive racing models can have a power output of about 11–17 hp. This provides a power-to-weight ratio favorable to racing. Despite their tiny size both adults and children race them at speeds of up to 78 mph (126 km/h) in organized racing leagues. In most countries, a licence is not required to ride miniature bikes. However, they are usually not street legal and should be ridden on private land, such as car parks, gardens or on race tracks.. A notable racer who learned on a minimoto is Valentino Rossi.
Go to Article

Explanation by Hotspot Model

Youtube


    

Pocketbike racing

Pocketbike racing

Pocketbike racing

Pocket Bike racing, also known as Minimoto or circus racing, is a category of racing where miniature racing motorcycles (known as pocket bikes or minimoto) are raced around kart tracks.

A typical minimoto is approximately one-quarter the size of a regular motorcycle, and is powered by a two-stroke internal combustion engine of between 40–50 cc producing somewhere between 2.4 and 17 hp (1.8 and 11 kW). The machines have no suspension, relying on the tires to absorb bumps and handle cornering, and weigh approximately 50 lb (23 kg). The entry-level models produce about 2.4–4.2 hp, but the more expensive racing models can have a power output of about 11–17 hp. This provides a power-to-weight ratio favorable to racing. Despite their tiny size both adults and children race them at speeds of up to 78 mph (126 km/h) in organized racing leagues.

In most countries, a licence is not required to ride miniature bikes. However, they are usually not street legal and should be ridden on private land, such as car parks, gardens or on race tracks..

A notable racer who learned on a minimoto is Valentino Rossi.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks & Buse

Car, Truck,MotorBike, Bicycle, Engine, Racer, Bus