powered by CADENAS

Social Share

Amazon

Interdictor (6609 views - Transportation - Air Water Earth)

An interdictor is a type of attack aircraft that operates far behind enemy lines, with the express intent of interdicting the enemy's military targets, most notably those involved in logistics. The interdiction prevents or delays enemy forces and supplies from reaching the battlefront; the term has generally fallen from use. The strike fighter is a closely related concept, but puts more emphasis on air-to-air combat capabilities as a multirole combat aircraft. Larger versions of the interdictor concept are generally referred to as penetrators. In the post-war era, the RAF introduced interdictor variants of their English Electric Canberra jet bomber, the aircraft being available as the strategic bombing role had been taken over by the new V bombers. An early interdictor was the F-111, an aircraft able to operate at long distances from its base. The Panavia Tornado was built for a similar purpose, although operating over shorter ranges in the European theatre. The Soviet Sukhoi Su-24/Sukhoi Su-34, Chinese Xian JH-7 and the aborted British BAC TSR-2 are similar interdictor designs.
Go to Article

Explanation by Hotspot Model

Youtube


    

Interdictor

Interdictor

An interdictor is a type of attack aircraft that operates far behind enemy lines, with the express intent of interdicting the enemy's military targets, most notably those involved in logistics. The interdiction prevents or delays enemy forces and supplies from reaching the battlefront; the term has generally fallen from use. The strike fighter is a closely related concept,[citation needed] but puts more emphasis on air-to-air combat capabilities as a multirole combat aircraft. Larger versions of the interdictor concept are generally referred to as penetrators.

In the post-war era, the RAF introduced interdictor variants of their English Electric Canberra jet bomber, the aircraft being available as the strategic bombing role had been taken over by the new V bombers. An early interdictor was the F-111, an aircraft able to operate at long distances from its base. The Panavia Tornado was built for a similar purpose, although operating over shorter ranges in the European theatre. The Soviet Sukhoi Su-24/Sukhoi Su-34, Chinese Xian JH-7 and the aborted British BAC TSR-2 are similar interdictor designs.

Interdictors

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht