powered by CADENAS

Social Share

Amazon

Tandem rotors (4833 views - Transportation - Air Water Earth)

Tandem rotor helicopters have two large horizontal rotor assemblies mounted one in front of the other. Currently this configuration is mainly used for large cargo helicopters.Single rotor helicopters need a mechanism to neutralize the yawing movement produced by the single large rotor. This is commonly accomplished by a tail rotor, coaxial rotors, and the NOTAR systems. Tandem rotor helicopters, however, use counter-rotating rotors, with each cancelling out the other's torque. Therefore, all of the power from the engines can be used for lift, whereas a single rotor helicopter uses some of the engine power to counter the torque. An alternative is to mount two rotors in a coaxial configuration. The first successful tandem rotor helicopter was built by Nicolas Florine in 1927. Advantages of the tandem-rotor system are a larger centre of gravity range, and good longitudinal stability. Disadvantages of the tandem-rotor system are a complex transmission, and the need for two large rotors. The two rotors are linked by a transmission that ensures the rotors are synchronized and do not hit each other, even during an engine failure.Tandem rotor designs achieve yaw by applying opposite left and right cyclic to each rotor, effectively pulling both ends of the helicopter in opposite directions. To achieve pitch, opposite collective is applied to each rotor; decreasing the lift produced at one end, while increasing lift at the opposite end, effectively tilting the helicopter forward or back.Tandem rotor aerodynamics is a complex subject. Tandem rotor helicopters have the advantage of being able to hold more weight with shorter blades, since there are two sets. However, the rear rotor works in the aerodynamic shadow of the front rotor, which reduces its efficiency. This loss can be minimized by increasing the distance between the two rotor hubs, and by elevating one hub over the other. Tandem rotor helicopters tend to have a lower disk loading than single rotor helicopters.Tandem rotor helicopters typically require less power to hover and achieve low speed flight as compared to single rotor helicopters. Both configurations typically require the same power to achieve high speed flight.
Go to Article

Explanation by Hotspot Model

Youtube


    

Tandem rotors

Tandem rotors

Tandem rotors

Tandem rotor helicopters have two large horizontal rotor assemblies mounted one in front of the other. Currently this configuration is mainly used for large cargo helicopters.[1]

Single rotor helicopters need a mechanism to neutralize the yawing movement produced by the single large rotor. This is commonly accomplished by a tail rotor, coaxial rotors, and the NOTAR systems. Tandem rotor helicopters, however, use counter-rotating rotors, with each cancelling out the other's torque. Therefore, all of the power from the engines can be used for lift, whereas a single rotor helicopter uses some of the engine power to counter the torque.[1] An alternative is to mount two rotors in a coaxial configuration. The first successful tandem rotor helicopter was built by Nicolas Florine in 1927.

Advantages of the tandem-rotor system are a larger centre of gravity range, and good longitudinal stability. Disadvantages of the tandem-rotor system are a complex transmission,[1] and the need for two large rotors.

The two rotors are linked by a transmission that ensures the rotors are synchronized and do not hit each other, even during an engine failure.[2]

Tandem rotor designs achieve yaw by applying opposite left and right cyclic to each rotor, effectively pulling both ends of the helicopter in opposite directions. To achieve pitch, opposite collective is applied to each rotor; decreasing the lift produced at one end, while increasing lift at the opposite end, effectively tilting the helicopter forward or back.[3]

Tandem rotor aerodynamics is a complex subject.[citation needed] Tandem rotor helicopters have the advantage of being able to hold more weight with shorter blades, since there are two sets. However, the rear rotor works in the aerodynamic shadow of the front rotor, which reduces its efficiency. This loss can be minimized by increasing the distance between the two rotor hubs, and by elevating one hub over the other.[4][5] Tandem rotor helicopters tend to have a lower disk loading than single rotor helicopters.[6]

Tandem rotor helicopters typically require less power to hover and achieve low speed flight as compared to single rotor helicopters. Both configurations typically require the same power to achieve high speed flight.[7]

List of some tandem rotor helicopters


See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht