Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
An automatic door is a door that opens automatically, usually on sensing the approach of a person.
In the 1st Century AD, Greek mathematician Heron of Alexandria invented the first known automatic door. He described two different automatic door applications. The first application used heat from a fire lit by the city's temple priest. After a few hours atmospheric pressure built up in a brass vessel causing it to pump water into adjacent containers. These containers acted as weights that, through a series of ropes and pulleys, would open the temple's doors at about the time people were to arrive for prayer. Heron used a similar application to open the gates to the city.[1]
In 1931, engineers Horace H. Raymond and Sheldon S. Roby of the tool and hardware manufacturer Stanley Works designed the first model of an optical device triggering the opening of an automatic door. The invention was patented and installed in Wilcox's Pier Restaurant in West Haven, Connecticut for the benefit of waiters carrying plates of food and drink. The entire system plus installation was sold for $100.[2][3]
In 1954, Dee Horton and Lew Hewitt invented the first sliding automatic door. The automatic door used a mat actuator. In 1960, they co-founded Horton Automatics Inc and placed the first commercial automatic sliding door on the market.[4]
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art