powered by CADENAS

Social Share

Semla (7953 views - Food Drinks Beverages)

A semla, vastlakukkel, laskiaispulla or fastlagsbulle/fastelavnsbolle is a traditional sweet roll made in various forms in Sweden, Finland, Estonia, Norway, Denmark, the Faroe Islands, Iceland, Latvia, and Lithuania associated with Lent and especially Shrove Tuesday in most countries, Shrove Monday in Denmark, parts of southern Sweden and Iceland or Sunday of Fastelavn in Norway. In Sweden it is most commonly known as just “Semlor” (plural of “Semla”). In the southern parts of Sweden, as well as in Swedish-speaking Finland, it is also called “Fastlagsbullar” (plural of “Fastlagsbulle”). In Norway and Denmark it is called "Fastelavnsbolle". Semla served in a bowl of hot milk is “hetvägg”.
Go to Article

Explanation by Hotspot Model

Semla

Semla

Semla
Traditional Swedish semla
Alternative names Laskiaispulla and Lent buns
Type Sweet roll
Course Dessert
Place of origin Sweden or Finland
Region or state Nordic countries
Associated national cuisine Sweden
Invented 1500s
Serving temperature Medium
Main ingredients Wheat bread, whipped cream and almond paste
Ingredients generally used Icing sugar
Variations Hetvägg
Food energy
(per serving)
298 kcal (1248 kJ)
Nutritional value
(per serving)
Protein 6.8 g
Fat 12.7 g
Carbohydrate 38.2 g
Similar dishes Pulla and Cardamom bread
Cookbook: Semla  Media: Semla

A semla, vastlakukkel, laskiaispulla or fastlagsbulle/fastelavnsbolle is a traditional sweet roll made in various forms in Sweden,[1] Finland, Estonia, Norway, Denmark, the Faroe Islands, Iceland, Latvia, and Lithuania associated with Lent and especially Shrove Tuesday in most countries, Shrove Monday in Denmark, parts of southern Sweden and Iceland or Sunday of Fastelavn in Norway. In Sweden it is most commonly known as just “Semlor” (plural of “Semla”). In the southern parts of Sweden, as well as in Swedish-speaking Finland, it is also called “Fastlagsbullar” (plural of “Fastlagsbulle”). In Norway and Denmark it is called "Fastelavnsbolle". Semla served in a bowl of hot milk is “hetvägg”. [2]

Etymology

The name semla (plural, semlor) is a loan word from German Semmel, originally deriving from the Latin simila, meaning 'flour', itself a borrowing from Greek σεμίδαλις (semidalis), "groats", which was the name used for the finest quality wheat flour or semolina. In the southernmost part of Sweden (Scania) and by the Swedish-speaking population in Finland, they are known as fastlagsbulle. In Denmark and Norway they are known as fastelavnsbolle (fastlagen and fastelavn being the equivalent of Shrove Tuesday). In Scanian, the feast is also called fastelann. In Finnish they are known as laskiaispulla, in Latvian as vēja kūkas, and in Estonian as vastlakukkel.

Sweden/Finland

Today, the Swedish-Finnish semla [3] consists of a cardamom-spiced wheat bun which has its top cut off, and is then filled with a mix of milk and almond paste, topped with whipped cream. The cut-off top serves as a lid and is dusted with powdered sugar. Today it is often eaten on its own, with coffee or tea. Some people still eat it in a bowl of hot milk. In Finland, the bun is often filled with strawberry or raspberry jam instead of almond paste, and bakeries in Finland usually offer both versions. (Many bakeries distinguish between the two by decorating the traditional bun with almonds on top, whereas the jam-filled version has powdered sugar on top). In Finland-Swedish, semla means a plain wheat bun, used for bread and butter, and not a sweet bun. At some point Swedes grew tired of the strict observance of Lent, added cream and almond paste to the mix and started eating semla every Tuesday between Shrove Tuesday and Easter. Every year, at around the same time that the bakeries fill with semlor, the Swedish newspapers start to fill with semla taste tests. Panels of ‘experts’ dissect and inspect tables full of semlor to find the best in town. Over the years bakeries have challenged the traditional semla, hoping to create the next big buzz. In 2015, the semmelwrap took the Swedes by storm. Instead of the original semla bun, the dough is rolled out flat, filled with almond paste and whipped cream, then folded and eaten as a wrap. The pastry truly went viral in both social media and in several Swedish news feeds and it was not long before a horde of other bakeries around Sweden tried to copy the idea (hoping to beat the sales record). [4]

In Finland and Estonia the traditional dessert predates Christian influences[citation needed]. Laskiaissunnuntai and Laskiaistiistai were festivals when children and youth would go sledding or downhill sliding on a hill or a slope to determine how the crop would yield in the coming year. Those who slid the farthest were going to get the best crop. Hence the festival is named after the act of sliding or sledding downhill, laskea. Nowadays laskiainen has been integrated into Christian customs as the beginning of lent before Easter.[5]

Norway

Fastelavnsbolle consists of a cardamom-spiced wheat bun which has its top cut off, and is then filled with whipped cream, topped with jam. The cut-off top serves as a lid and is dusted with powdered sugar. The buns are served at Sunday of Fastelavn, but were previously associated with Shrove Tuesday.[6]

Denmark/Iceland

The version sold in Danish and Icelandic bakeries on or around Shrove Monday is rather different, made from puff pastry and filled with whipped cream, a bit of jam and often with icing on top. At home people may bake a version more similar to a usual wheat roll, mixing plain yeast dough with raisins, succade and sometimes candied bitter orange peel.

In Icelandic Shrove Monday is called bolludagur (bun day), named after the pastry.

History

The oldest version of the semla was a plain bread bun, eaten in a bowl of warm milk. In Swedish this is known as hetvägg, from Middle Low German hete Weggen (hot wedges) or German heisse Wecken (hot buns) and falsely interpreted as "hotwall".[7] The semla was originally eaten only on Shrove Tuesday, as the last festive food before Lent. However, with the arrival of the Protestant Reformation, the Swedes stopped observing a strict fasting for Lent. The semla in its bowl of warm milk became a traditional dessert every Tuesday between Shrove Tuesday and Easter. Today, semlor are available in shops and bakeries every day from shortly after Christmas until Easter. Each Swede consumes on average four to five bakery-produced semlor each year, in addition to any that are homemade.[8]

King Adolf Frederick of Sweden died of digestion problems on February 12, 1771 after consuming a meal consisting of lobster, caviar, sauerkraut, smoked herring and champagne, which was topped off by fourteen helpings of hetvägg (semla), the king's favorite dessert.

This was the sweet chosen to represent Finland in the Café Europe initiative of the Austrian presidency of the European Union, on Europe Day 2006.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Food Drinks Beverages

food,liquor,alcohol,drink,beverage,coke