Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution 2.5 (Unkown).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (September 2007) (Learn how and when to remove this template message) |
An arena, is a covered or not covered enclosed area, often circular or oval-shaped, designed to showcase theater, musical performances, or sporting events. The word derives from Latin harena, a particularly fine/smooth sand used to absorb blood in ancient arenas such as the Colosseum in Rome, Italy.[1] It is composed of a large open space surrounded on most or all sides by tiered seating for spectators. The key feature of an arena is that the event space is the lowest point, allowing for maximum visibility. Arenas are usually designed to accommodate a large number of spectators.
The term arena is sometimes used as a synonym for a very large venue such as Pasadena's Rose Bowl, but such a facility is typically called a stadium, especially if it does not have a roof.[citation needed] The use of one term over the other has mostly to do with the type of event. Football (be it association, rugby, or gridiron) is typically played in a stadium while basketball and ice hockey are typically played in an arena, although many of the larger arenas hold more spectators than do the stadiums of smaller colleges or high schools. There are exceptions. The home of the Duke University men's and women's basketball teams would qualify as an arena, but the facility is called Cameron Indoor Stadium. Domed stadiums, which, like arenas, are enclosed but have the larger playing surfaces and seating capacities found in stadiums, are generally not referred to as arenas in North America. There is also the sport of indoor American football (one variant of which is explicitly known as arena football), a variant of the gridiron-based game that is designed for the usual smaller playing surface of most arenas; variants of other traditionally outdoor sports, including box lacrosse and futsal/indoor soccer, also exist.
The term "arena" is also used loosely to refer to any event or type of event which either literally or metaphorically takes place in such a location, often with the specific intent of comparing an idea to a sporting event. Such examples of these would be terms such as "the arena of war" or "the arena of love" or "the political arena". In many fighting games, the stage that opponents are fought in is also called an arena.
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, BIM Object, BIM component, BIM library, BIM family, BIM catalog, GIS, Advanced Steel, AutoCAD MEP, linear, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, BIM family creation, 3D, Download, MEP BIM product library